#include <rf_common_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips if the rule involves skipping. More... | |
} | condition |
Definition at line 113 of file rf_common_cmd.h.
uint8_t rfc_radioOp_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 122 of file rf_common_cmd.h.
uint16_t rfc_radioOp_s::commandNo |
The command ID number.
Definition at line 114 of file rf_common_cmd.h.
struct { ... } rfc_radioOp_s::condition |
uint8_t rfc_radioOp_s::nSkip |
Number of skips if the rule involves skipping.
Definition at line 130 of file rf_common_cmd.h.
uint8_t rfc_radioOp_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 125 of file rf_common_cmd.h.
rfc_radioOp_t* rfc_radioOp_s::pNextOp |
Pointer to the next operation to run after this operation is done.
Definition at line 118 of file rf_common_cmd.h.
uint8_t rfc_radioOp_s::rule |
Condition for running next command: Rule for how to proceed.
Definition at line 129 of file rf_common_cmd.h.
ratmr_t rfc_radioOp_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
Definition at line 119 of file rf_common_cmd.h.
struct { ... } rfc_radioOp_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_radioOp_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
Definition at line 115 of file rf_common_cmd.h.
uint8_t rfc_radioOp_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 124 of file rf_common_cmd.h.
uint8_t rfc_radioOp_s::triggerType |
The type of trigger.
Definition at line 121 of file rf_common_cmd.h.