#include <rf_ble_cmd.h>
Data Fields | |
dataQueue_t * | pRxQ |
Pointer to receive queue. More... | |
dataQueue_t * | pTxQ |
Pointer to transmit queue. More... | |
struct { | |
uint8_t bAutoFlushIgnored:1 | |
If 1, automatically remove ignored packets from Rx queue. More... | |
uint8_t bAutoFlushCrcErr:1 | |
If 1, automatically remove packets with CRC error from Rx queue. More... | |
uint8_t bAutoFlushEmpty:1 | |
If 1, automatically remove empty packets from Rx queue. More... | |
uint8_t bIncludeLenByte:1 | |
If 1, include the received length byte in the stored packet; otherwise discard it. More... | |
uint8_t bIncludeCrc:1 | |
If 1, include the received CRC field in the stored packet; otherwise discard it. More... | |
uint8_t bAppendRssi:1 | |
If 1, append an RSSI byte to the packet in the Rx queue. More... | |
uint8_t bAppendStatus:1 | |
If 1, append a status byte to the packet in the Rx queue. More... | |
uint8_t bAppendTimestamp:1 | |
If 1, append a timestamp to the packet in the Rx queue. More... | |
} | rxConfig |
Configuration bits for the receive queue entries. More... | |
struct { | |
uint8_t lastRxSn:1 | |
The SN bit of the header of the last packet received with CRC OK. More... | |
uint8_t lastTxSn:1 | |
The SN bit of the header of the last transmitted packet. More... | |
uint8_t nextTxSn:1 | |
The SN bit of the header of the next packet to transmit. More... | |
uint8_t bFirstPkt:1 | |
For slave: 0 if a packet has been transmitted on the connection, 1 otherwise. More... | |
uint8_t bAutoEmpty:1 | |
1 if the last transmitted packet was an auto-empty packet More... | |
uint8_t bLlCtrlTx:1 | |
1 if the last transmitted packet was an LL control packet (LLID = 11) More... | |
uint8_t bLlCtrlAckRx:1 | |
1 if the last received packet was the ACK of an LL control packet More... | |
uint8_t bLlCtrlAckPending:1 | |
1 if the last successfully received packet was an LL control packet which has not yet been ACK'ed More... | |
} | seqStat |
uint8_t | maxNack |
Maximum number of NACKs received before operation ends. 0: No limit. More... | |
uint8_t | maxPkt |
Maximum number of packets transmitted in the operation before it ends. 0: No limit. More... | |
uint32_t | accessAddress |
Access address used on the connection. More... | |
uint8_t | crcInit0 |
CRC initialization value used on the connection – least significant byte. More... | |
uint8_t | crcInit1 |
CRC initialization value used on the connection – middle byte. More... | |
uint8_t | crcInit2 |
CRC initialization value used on the connection – most significant byte. More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
} | timeoutTrigger |
Trigger that defines timeout of the first receive operation. More... | |
ratmr_t | timeoutTime |
uint16_t | __dummy0 |
uint8_t | __dummy1 |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
} | endTrigger |
Trigger that causes the device to end the connection event as soon as allowed. More... | |
ratmr_t | endTime |
Definition at line 628 of file rf_ble_cmd.h.
uint16_t rfc_bleSlavePar_s::__dummy0 |
Definition at line 667 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::__dummy1 |
Definition at line 668 of file rf_ble_cmd.h.
uint32_t rfc_bleSlavePar_s::accessAddress |
Access address used on the connection.
Definition at line 653 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::bAppendRssi |
If 1, append an RSSI byte to the packet in the Rx queue.
Definition at line 637 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::bAppendStatus |
If 1, append a status byte to the packet in the Rx queue.
Definition at line 638 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::bAppendTimestamp |
If 1, append a timestamp to the packet in the Rx queue.
Definition at line 639 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::bAutoEmpty |
1 if the last transmitted packet was an auto-empty packet
Definition at line 646 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::bAutoFlushCrcErr |
If 1, automatically remove packets with CRC error from Rx queue.
Definition at line 633 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::bAutoFlushEmpty |
If 1, automatically remove empty packets from Rx queue.
Definition at line 634 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::bAutoFlushIgnored |
If 1, automatically remove ignored packets from Rx queue.
Definition at line 632 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 659 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::bFirstPkt |
For slave: 0 if a packet has been transmitted on the connection, 1 otherwise.
Definition at line 645 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::bIncludeCrc |
If 1, include the received CRC field in the stored packet; otherwise discard it.
Definition at line 636 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::bIncludeLenByte |
If 1, include the received length byte in the stored packet; otherwise discard it.
Definition at line 635 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::bLlCtrlAckPending |
1 if the last successfully received packet was an LL control packet which has not yet been ACK'ed
Definition at line 649 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::bLlCtrlAckRx |
1 if the last received packet was the ACK of an LL control packet
Definition at line 648 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::bLlCtrlTx |
1 if the last transmitted packet was an LL control packet (LLID = 11)
Definition at line 647 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::crcInit0 |
CRC initialization value used on the connection – least significant byte.
Definition at line 654 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::crcInit1 |
CRC initialization value used on the connection – middle byte.
Definition at line 655 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::crcInit2 |
CRC initialization value used on the connection – most significant byte.
Definition at line 656 of file rf_ble_cmd.h.
ratmr_t rfc_bleSlavePar_s::endTime |
Time used together with endTrigger
that causes the device to end the connection event as soon as allowed
Definition at line 677 of file rf_ble_cmd.h.
struct { ... } rfc_bleSlavePar_s::endTrigger |
Trigger that causes the device to end the connection event as soon as allowed.
uint8_t rfc_bleSlavePar_s::lastRxSn |
The SN bit of the header of the last packet received with CRC OK.
Definition at line 642 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::lastTxSn |
The SN bit of the header of the last transmitted packet.
Definition at line 643 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::maxNack |
Maximum number of NACKs received before operation ends. 0: No limit.
Definition at line 651 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::maxPkt |
Maximum number of packets transmitted in the operation before it ends. 0: No limit.
Definition at line 652 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::nextTxSn |
The SN bit of the header of the next packet to transmit.
Definition at line 644 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 662 of file rf_ble_cmd.h.
dataQueue_t* rfc_bleSlavePar_s::pRxQ |
Pointer to receive queue.
Definition at line 629 of file rf_ble_cmd.h.
dataQueue_t* rfc_bleSlavePar_s::pTxQ |
Pointer to transmit queue.
Definition at line 630 of file rf_ble_cmd.h.
struct { ... } rfc_bleSlavePar_s::rxConfig |
Configuration bits for the receive queue entries.
struct { ... } rfc_bleSlavePar_s::seqStat |
ratmr_t rfc_bleSlavePar_s::timeoutTime |
Time used together with timeoutTrigger
that defines timeout of the first receive operation
Definition at line 665 of file rf_ble_cmd.h.
struct { ... } rfc_bleSlavePar_s::timeoutTrigger |
Trigger that defines timeout of the first receive operation.
uint8_t rfc_bleSlavePar_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 661 of file rf_ble_cmd.h.
uint8_t rfc_bleSlavePar_s::triggerType |
The type of trigger.
Definition at line 658 of file rf_ble_cmd.h.