#include <rf_ble_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number. More... | |
uint16_t | status |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips if the rule involves skipping. More... | |
} | condition |
uint8_t | channel |
struct { | |
uint8_t init:7 | |
uint8_t bOverride:1 | |
} | whitening |
uint8_t * | pParams |
Pointer to command specific parameter structure. More... | |
uint8_t * | pOutput |
Pointer to command specific output structure. More... | |
Definition at line 91 of file rf_ble_cmd.h.
uint8_t rfc_bleRadioOp_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 100 of file rf_ble_cmd.h.
uint8_t rfc_bleRadioOp_s::bOverride |
0: Use default whitening for BLE advertising/data channels
1: Override whitening initialization with value of init
Definition at line 119 of file rf_ble_cmd.h.
uint8_t rfc_bleRadioOp_s::channel |
Channel to use
0–39: BLE advertising/data channel number 60–207: Custom frequency; (2300 + channel
) MHz 255: Use existing frequency Others: Reserved
Definition at line 110 of file rf_ble_cmd.h.
uint16_t rfc_bleRadioOp_s::commandNo |
The command ID number.
Definition at line 92 of file rf_ble_cmd.h.
struct { ... } rfc_bleRadioOp_s::condition |
uint8_t rfc_bleRadioOp_s::init |
If bOverride
= 1 or custom frequency is used:
0: Do not use whitening
Other value: Initialization for 7-bit LFSR whitener
Definition at line 116 of file rf_ble_cmd.h.
uint8_t rfc_bleRadioOp_s::nSkip |
Number of skips if the rule involves skipping.
Definition at line 108 of file rf_ble_cmd.h.
uint8_t rfc_bleRadioOp_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 103 of file rf_ble_cmd.h.
rfc_radioOp_t* rfc_bleRadioOp_s::pNextOp |
Pointer to the next operation to run after this operation is done.
Definition at line 96 of file rf_ble_cmd.h.
uint8_t* rfc_bleRadioOp_s::pOutput |
Pointer to command specific output structure.
Definition at line 123 of file rf_ble_cmd.h.
uint8_t* rfc_bleRadioOp_s::pParams |
Pointer to command specific parameter structure.
Definition at line 122 of file rf_ble_cmd.h.
uint8_t rfc_bleRadioOp_s::rule |
Condition for running next command: Rule for how to proceed.
Definition at line 107 of file rf_ble_cmd.h.
ratmr_t rfc_bleRadioOp_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
Definition at line 97 of file rf_ble_cmd.h.
struct { ... } rfc_bleRadioOp_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_bleRadioOp_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
Definition at line 93 of file rf_ble_cmd.h.
uint8_t rfc_bleRadioOp_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 102 of file rf_ble_cmd.h.
uint8_t rfc_bleRadioOp_s::triggerType |
The type of trigger.
Definition at line 99 of file rf_ble_cmd.h.
struct { ... } rfc_bleRadioOp_s::whitening |