#include <rf_ble_cmd.h>
Data Fields | |
dataQueue_t * | pRxQ |
Pointer to receive queue. More... | |
struct { | |
uint8_t bAutoFlushIgnored:1 | |
If 1, automatically remove ignored packets from Rx queue. More... | |
uint8_t bAutoFlushCrcErr:1 | |
If 1, automatically remove packets with CRC error from Rx queue. More... | |
uint8_t bAutoFlushEmpty:1 | |
If 1, automatically remove empty packets from Rx queue. More... | |
uint8_t bIncludeLenByte:1 | |
If 1, include the received length byte in the stored packet; otherwise discard it. More... | |
uint8_t bIncludeCrc:1 | |
If 1, include the received CRC field in the stored packet; otherwise discard it. More... | |
uint8_t bAppendRssi:1 | |
If 1, append an RSSI byte to the packet in the Rx queue. More... | |
uint8_t bAppendStatus:1 | |
If 1, append a status byte to the packet in the Rx queue. More... | |
uint8_t bAppendTimestamp:1 | |
If 1, append a timestamp to the packet in the Rx queue. More... | |
} | rxConfig |
Configuration bits for the receive queue entries. More... | |
struct { | |
uint8_t bUseWhiteList:1 | |
uint8_t bDynamicWinOffset:1 | |
1: Use dynamic WinOffset insertion More... | |
uint8_t deviceAddrType:1 | |
The type of the device address – public (0) or random (1) More... | |
uint8_t peerAddrType:1 | |
The type of the peer address – public (0) or random (1) More... | |
uint8_t bStrictLenFilter:1 | |
1: Discard messages with illegal length More... | |
} | initConfig |
uint8_t | __dummy0 |
uint8_t | connectReqLen |
Size of connect request data. More... | |
uint8_t * | pConnectReqData |
Pointer to buffer containing LLData to go in the CONNECT_REQ. More... | |
uint16_t * | pDeviceAddress |
Pointer to device address used for this device. More... | |
rfc_bleWhiteListEntry_t * | pWhiteList |
Pointer to white list or peer address. More... | |
ratmr_t | connectTime |
uint16_t | __dummy1 |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
} | timeoutTrigger |
Trigger that causes the device to stop receiving as soon as allowed. More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
} | endTrigger |
Trigger that causes the device to stop receiving as soon as allowed. More... | |
ratmr_t | timeoutTime |
ratmr_t | endTime |
Definition at line 804 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::__dummy0 |
Definition at line 826 of file rf_ble_cmd.h.
uint16_t rfc_bleInitiatorPar_s::__dummy1 |
Definition at line 834 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::bAppendRssi |
If 1, append an RSSI byte to the packet in the Rx queue.
Definition at line 812 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::bAppendStatus |
If 1, append a status byte to the packet in the Rx queue.
Definition at line 813 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::bAppendTimestamp |
If 1, append a timestamp to the packet in the Rx queue.
Definition at line 814 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::bAutoFlushCrcErr |
If 1, automatically remove packets with CRC error from Rx queue.
Definition at line 808 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::bAutoFlushEmpty |
If 1, automatically remove empty packets from Rx queue.
Definition at line 809 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::bAutoFlushIgnored |
If 1, automatically remove ignored packets from Rx queue.
Definition at line 807 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::bDynamicWinOffset |
1: Use dynamic WinOffset insertion
Definition at line 821 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 837 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::bIncludeCrc |
If 1, include the received CRC field in the stored packet; otherwise discard it.
Definition at line 811 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::bIncludeLenByte |
If 1, include the received length byte in the stored packet; otherwise discard it.
Definition at line 810 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::bStrictLenFilter |
1: Discard messages with illegal length
Definition at line 824 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::bUseWhiteList |
Initiator filter policy, cf. Volume 2, Part E, Section 7.8.10 of the Bluetooth 4.0 spec:
0: Use specific peer address
1: Use white list
Definition at line 817 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::connectReqLen |
Size of connect request data.
Definition at line 827 of file rf_ble_cmd.h.
ratmr_t rfc_bleInitiatorPar_s::connectTime |
Indication of timer value of the first possible start time of the first connection event. Set to the calculated value if a connection is made and to the next possible connection time if not.
Definition at line 831 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::deviceAddrType |
The type of the device address – public (0) or random (1)
Definition at line 822 of file rf_ble_cmd.h.
ratmr_t rfc_bleInitiatorPar_s::endTime |
Time used together with endTrigger
that causes the device to stop receiving as soon as allowed, ending with BLE_DONE_ENDED
Definition at line 853 of file rf_ble_cmd.h.
struct { ... } rfc_bleInitiatorPar_s::endTrigger |
Trigger that causes the device to stop receiving as soon as allowed.
struct { ... } rfc_bleInitiatorPar_s::initConfig |
uint8_t rfc_bleInitiatorPar_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 840 of file rf_ble_cmd.h.
uint8_t* rfc_bleInitiatorPar_s::pConnectReqData |
Pointer to buffer containing LLData to go in the CONNECT_REQ.
Definition at line 828 of file rf_ble_cmd.h.
uint16_t* rfc_bleInitiatorPar_s::pDeviceAddress |
Pointer to device address used for this device.
Definition at line 829 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::peerAddrType |
The type of the peer address – public (0) or random (1)
Definition at line 823 of file rf_ble_cmd.h.
dataQueue_t* rfc_bleInitiatorPar_s::pRxQ |
Pointer to receive queue.
Definition at line 805 of file rf_ble_cmd.h.
rfc_bleWhiteListEntry_t* rfc_bleInitiatorPar_s::pWhiteList |
Pointer to white list or peer address.
Definition at line 830 of file rf_ble_cmd.h.
struct { ... } rfc_bleInitiatorPar_s::rxConfig |
Configuration bits for the receive queue entries.
ratmr_t rfc_bleInitiatorPar_s::timeoutTime |
Time used together with timeoutTrigger
that causes the device to stop receiving as soon as allowed, ending with BLE_DONE_RXTIMEOUT
Definition at line 851 of file rf_ble_cmd.h.
struct { ... } rfc_bleInitiatorPar_s::timeoutTrigger |
Trigger that causes the device to stop receiving as soon as allowed.
uint8_t rfc_bleInitiatorPar_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 839 of file rf_ble_cmd.h.
uint8_t rfc_bleInitiatorPar_s::triggerType |
The type of trigger.
Definition at line 836 of file rf_ble_cmd.h.