#include <rf_common_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x0806. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips if the rule involves skipping. More... | |
} | condition |
struct { | |
uint16_t endianness:1 | |
0: Least significant bit first 1: Most significant bit first More... | |
uint16_t numHdrBits:6 | |
Number of bits in the header. More... | |
uint16_t bFsOff:1 | |
0: Keep frequency synth on after command 1: Turn frequency synth off after command More... | |
uint16_t bUseCrc:1 | |
0: No CRC 1: Append a CRC to the packet More... | |
uint16_t bCrcIncSw:1 | |
0: Do not include sync word in CRC calculation 1: Include sync word in CRC calculation More... | |
uint16_t bCrcIncHdr:1 | |
0: Do not include header in CRC calculation 1: Include header in CRC calculation More... | |
} | pktConfig |
uint32_t | syncWord |
Sync word to transmit. More... | |
uint8_t * | pTxPkt |
Pointer to buffer for transmitted packet. More... | |
uint16_t | pktLen |
Number of bytes in the transmitted packet. More... | |
Definition at line 354 of file rf_common_cmd.h.
uint16_t rfc_CMD_TX_s::bCrcIncHdr |
0: Do not include header in CRC calculation
1: Include header in CRC calculation
Definition at line 383 of file rf_common_cmd.h.
uint16_t rfc_CMD_TX_s::bCrcIncSw |
0: Do not include sync word in CRC calculation
1: Include sync word in CRC calculation
Definition at line 381 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 363 of file rf_common_cmd.h.
uint16_t rfc_CMD_TX_s::bFsOff |
0: Keep frequency synth on after command
1: Turn frequency synth off after command
Definition at line 377 of file rf_common_cmd.h.
uint16_t rfc_CMD_TX_s::bUseCrc |
0: No CRC
1: Append a CRC to the packet
Definition at line 379 of file rf_common_cmd.h.
uint16_t rfc_CMD_TX_s::commandNo |
The command ID number 0x0806.
Definition at line 355 of file rf_common_cmd.h.
struct { ... } rfc_CMD_TX_s::condition |
uint16_t rfc_CMD_TX_s::endianness |
0: Least significant bit first
1: Most significant bit first
Definition at line 374 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_s::nSkip |
Number of skips if the rule involves skipping.
Definition at line 371 of file rf_common_cmd.h.
uint16_t rfc_CMD_TX_s::numHdrBits |
Number of bits in the header.
Definition at line 376 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 366 of file rf_common_cmd.h.
struct { ... } rfc_CMD_TX_s::pktConfig |
uint16_t rfc_CMD_TX_s::pktLen |
Number of bytes in the transmitted packet.
Definition at line 388 of file rf_common_cmd.h.
rfc_radioOp_t* rfc_CMD_TX_s::pNextOp |
Pointer to the next operation to run after this operation is done.
Definition at line 359 of file rf_common_cmd.h.
uint8_t* rfc_CMD_TX_s::pTxPkt |
Pointer to buffer for transmitted packet.
Definition at line 387 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_s::rule |
Condition for running next command: Rule for how to proceed.
Definition at line 370 of file rf_common_cmd.h.
ratmr_t rfc_CMD_TX_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
Definition at line 360 of file rf_common_cmd.h.
struct { ... } rfc_CMD_TX_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_CMD_TX_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
Definition at line 356 of file rf_common_cmd.h.
uint32_t rfc_CMD_TX_s::syncWord |
Sync word to transmit.
Definition at line 386 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 365 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_s::triggerType |
The type of trigger.
Definition at line 362 of file rf_common_cmd.h.