CC13xx Driver Library
rfc_CMD_BLE_SCANNER_s Struct Reference

#include <rf_ble_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x1807. More...
 
uint16_t status
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips if the rule involves skipping. More...
 
condition
 
uint8_t channel
 
struct {
   uint8_t   init:7
 
   uint8_t   bOverride:1
 
whitening
 
rfc_bleScannerPar_tpParams
 Pointer to command specific parameter structure. More...
 
rfc_bleScannerOutput_tpOutput
 Pointer to command specific output structure. More...
 

Detailed Description

Definition at line 371 of file rf_ble_cmd.h.

Field Documentation

uint8_t rfc_CMD_BLE_SCANNER_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

Definition at line 380 of file rf_ble_cmd.h.

uint8_t rfc_CMD_BLE_SCANNER_s::bOverride

0: Use default whitening for BLE advertising/data channels
1: Override whitening initialization with value of init

Definition at line 399 of file rf_ble_cmd.h.

uint8_t rfc_CMD_BLE_SCANNER_s::channel

Channel to use
0–39: BLE advertising/data channel number 60–207: Custom frequency; (2300 + channel) MHz 255: Use existing frequency Others: Reserved

Definition at line 390 of file rf_ble_cmd.h.

uint16_t rfc_CMD_BLE_SCANNER_s::commandNo

The command ID number 0x1807.

Definition at line 372 of file rf_ble_cmd.h.

struct { ... } rfc_CMD_BLE_SCANNER_s::condition
uint8_t rfc_CMD_BLE_SCANNER_s::init

If bOverride = 1 or custom frequency is used:
0: Do not use whitening
Other value: Initialization for 7-bit LFSR whitener

Definition at line 396 of file rf_ble_cmd.h.

uint8_t rfc_CMD_BLE_SCANNER_s::nSkip

Number of skips if the rule involves skipping.

Definition at line 388 of file rf_ble_cmd.h.

uint8_t rfc_CMD_BLE_SCANNER_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

Definition at line 383 of file rf_ble_cmd.h.

rfc_radioOp_t* rfc_CMD_BLE_SCANNER_s::pNextOp

Pointer to the next operation to run after this operation is done.

Definition at line 376 of file rf_ble_cmd.h.

rfc_bleScannerOutput_t* rfc_CMD_BLE_SCANNER_s::pOutput

Pointer to command specific output structure.

Definition at line 403 of file rf_ble_cmd.h.

rfc_bleScannerPar_t* rfc_CMD_BLE_SCANNER_s::pParams

Pointer to command specific parameter structure.

Definition at line 402 of file rf_ble_cmd.h.

uint8_t rfc_CMD_BLE_SCANNER_s::rule

Condition for running next command: Rule for how to proceed.

Definition at line 387 of file rf_ble_cmd.h.

ratmr_t rfc_CMD_BLE_SCANNER_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

Definition at line 377 of file rf_ble_cmd.h.

struct { ... } rfc_CMD_BLE_SCANNER_s::startTrigger

Identification of the trigger that starts the operation.

uint16_t rfc_CMD_BLE_SCANNER_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

Definition at line 373 of file rf_ble_cmd.h.

uint8_t rfc_CMD_BLE_SCANNER_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

Definition at line 382 of file rf_ble_cmd.h.

uint8_t rfc_CMD_BLE_SCANNER_s::triggerType

The type of trigger.

Definition at line 379 of file rf_ble_cmd.h.

struct { ... } rfc_CMD_BLE_SCANNER_s::whitening