#include <rf_ble_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x1805. More... | |
uint16_t | status |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips if the rule involves skipping. More... | |
} | condition |
uint8_t | channel |
struct { | |
uint8_t init:7 | |
uint8_t bOverride:1 | |
} | whitening |
rfc_bleAdvPar_t * | pParams |
Pointer to command specific parameter structure. More... | |
rfc_bleAdvOutput_t * | pOutput |
Pointer to command specific output structure. More... | |
Definition at line 291 of file rf_ble_cmd.h.
uint8_t rfc_CMD_BLE_ADV_NC_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 300 of file rf_ble_cmd.h.
uint8_t rfc_CMD_BLE_ADV_NC_s::bOverride |
0: Use default whitening for BLE advertising/data channels
1: Override whitening initialization with value of init
Definition at line 319 of file rf_ble_cmd.h.
uint8_t rfc_CMD_BLE_ADV_NC_s::channel |
Channel to use
0–39: BLE advertising/data channel number 60–207: Custom frequency; (2300 + channel
) MHz 255: Use existing frequency Others: Reserved
Definition at line 310 of file rf_ble_cmd.h.
uint16_t rfc_CMD_BLE_ADV_NC_s::commandNo |
The command ID number 0x1805.
Definition at line 292 of file rf_ble_cmd.h.
struct { ... } rfc_CMD_BLE_ADV_NC_s::condition |
uint8_t rfc_CMD_BLE_ADV_NC_s::init |
If bOverride
= 1 or custom frequency is used:
0: Do not use whitening
Other value: Initialization for 7-bit LFSR whitener
Definition at line 316 of file rf_ble_cmd.h.
uint8_t rfc_CMD_BLE_ADV_NC_s::nSkip |
Number of skips if the rule involves skipping.
Definition at line 308 of file rf_ble_cmd.h.
uint8_t rfc_CMD_BLE_ADV_NC_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 303 of file rf_ble_cmd.h.
rfc_radioOp_t* rfc_CMD_BLE_ADV_NC_s::pNextOp |
Pointer to the next operation to run after this operation is done.
Definition at line 296 of file rf_ble_cmd.h.
rfc_bleAdvOutput_t* rfc_CMD_BLE_ADV_NC_s::pOutput |
Pointer to command specific output structure.
Definition at line 323 of file rf_ble_cmd.h.
rfc_bleAdvPar_t* rfc_CMD_BLE_ADV_NC_s::pParams |
Pointer to command specific parameter structure.
Definition at line 322 of file rf_ble_cmd.h.
uint8_t rfc_CMD_BLE_ADV_NC_s::rule |
Condition for running next command: Rule for how to proceed.
Definition at line 307 of file rf_ble_cmd.h.
ratmr_t rfc_CMD_BLE_ADV_NC_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
Definition at line 297 of file rf_ble_cmd.h.
struct { ... } rfc_CMD_BLE_ADV_NC_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_CMD_BLE_ADV_NC_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
Definition at line 293 of file rf_ble_cmd.h.
uint8_t rfc_CMD_BLE_ADV_NC_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 302 of file rf_ble_cmd.h.
uint8_t rfc_CMD_BLE_ADV_NC_s::triggerType |
The type of trigger.
Definition at line 299 of file rf_ble_cmd.h.
struct { ... } rfc_CMD_BLE_ADV_NC_s::whitening |