#include <rf_common_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x0005. More... | |
uint16_t | __dummy0 |
dataQueue_t * | pQueue |
Pointer to the queue structure to which the entry will be added. More... | |
uint8_t * | pEntry |
Pointer to the entry. More... | |
Definition at line 826 of file rf_common_cmd.h.
uint16_t rfc_CMD_ADD_DATA_ENTRY_s::__dummy0 |
Definition at line 828 of file rf_common_cmd.h.
uint16_t rfc_CMD_ADD_DATA_ENTRY_s::commandNo |
The command ID number 0x0005.
Definition at line 827 of file rf_common_cmd.h.
uint8_t* rfc_CMD_ADD_DATA_ENTRY_s::pEntry |
Pointer to the entry.
Definition at line 830 of file rf_common_cmd.h.
dataQueue_t* rfc_CMD_ADD_DATA_ENTRY_s::pQueue |
Pointer to the queue structure to which the entry will be added.
Definition at line 829 of file rf_common_cmd.h.