#include <driverlib/rf_mailbox.h>
Go to the source code of this file.
Macros | |
CPE interrupt definitions for BLE | |
Interrupt masks for the CPE interrupt in RDBELL. These are new names for interrupts in rf_mailbox.h, used for compartibility with previous versions with separate interrupt numbers. | |
#define | IRQN_BLE_TX_DONE IRQN_TX_DONE |
#define | IRQN_BLE_TX_ACK IRQN_TX_ACK |
#define | IRQN_BLE_TX_CTRL IRQN_TX_CTRL |
#define | IRQN_BLE_TX_CTRL_ACK IRQN_TX_CTRL_ACK |
#define | IRQN_BLE_TX_CTRL_ACK_ACK IRQN_TX_CTRL_ACK_ACK |
#define | IRQN_BLE_TX_RETRANS IRQN_TX_RETRANS |
#define | IRQN_BLE_TX_ENTRY_DONE IRQN_TX_ENTRY_DONE |
#define | IRQN_BLE_TX_BUFFER_CHANGED IRQN_TX_BUFFER_CHANGED |
#define | IRQN_BLE_RX_OK IRQN_RX_OK |
#define | IRQN_BLE_RX_NOK IRQN_RX_NOK |
#define | IRQN_BLE_RX_IGNORED IRQN_RX_IGNORED |
#define | IRQN_BLE_RX_EMPTY IRQN_RX_EMPTY |
#define | IRQN_BLE_RX_CTRL IRQN_RX_CTRL |
#define | IRQN_BLE_RX_CTRL_ACK IRQN_RX_CTRL_ACK |
#define | IRQN_BLE_RX_BUF_FULL IRQN_RX_BUF_FULL |
#define | IRQN_BLE_RX_ENTRY_DONE IRQN_RX_ENTRY_DONE |
#define | IRQ_BLE_TX_DONE (1U << IRQN_BLE_TX_DONE) |
#define | IRQ_BLE_TX_ACK (1U << IRQN_BLE_TX_ACK) |
#define | IRQ_BLE_TX_CTRL (1U << IRQN_BLE_TX_CTRL) |
#define | IRQ_BLE_TX_CTRL_ACK (1U << IRQN_BLE_TX_CTRL_ACK) |
#define | IRQ_BLE_TX_CTRL_ACK_ACK (1U << IRQN_BLE_TX_CTRL_ACK_ACK) |
#define | IRQ_BLE_TX_RETRANS (1U << IRQN_BLE_TX_RETRANS) |
#define | IRQ_BLE_TX_ENTRY_DONE (1U << IRQN_BLE_TX_ENTRY_DONE) |
#define | IRQ_BLE_TX_BUFFER_CHANGED (1U << IRQN_BLE_TX_BUFFER_CHANGED) |
#define | IRQ_BLE_RX_OK (1U << IRQN_BLE_RX_OK) |
#define | IRQ_BLE_RX_NOK (1U << IRQN_BLE_RX_NOK) |
#define | IRQ_BLE_RX_IGNORED (1U << IRQN_BLE_RX_IGNORED) |
#define | IRQ_BLE_RX_EMPTY (1U << IRQN_BLE_RX_EMPTY) |
#define | IRQ_BLE_RX_CTRL (1U << IRQN_BLE_RX_CTRL) |
#define | IRQ_BLE_RX_CTRL_ACK (1U << IRQN_BLE_RX_CTRL_ACK) |
#define | IRQ_BLE_RX_BUF_FULL (1U << IRQN_BLE_RX_BUF_FULL) |
#define | IRQ_BLE_RX_ENTRY_DONE (1U << IRQN_BLE_RX_ENTRY_DONE) |
Operation finished normally | |
#define | BLE_DONE_OK 0x1400 |
Operation ended normally. More... | |
#define | BLE_DONE_RXTIMEOUT 0x1401 |
Timeout of first Rx of slave operation or end of scan window. More... | |
#define | BLE_DONE_NOSYNC 0x1402 |
Timeout of subsequent Rx. More... | |
#define | BLE_DONE_RXERR 0x1403 |
Operation ended because of receive error (CRC or other) More... | |
#define | BLE_DONE_CONNECT 0x1404 |
CONNECT_REQ received or transmitted. More... | |
#define | BLE_DONE_MAXNACK 0x1405 |
Maximum number of retransmissions exceeded. More... | |
#define | BLE_DONE_ENDED 0x1406 |
Operation stopped after end trigger. More... | |
#define | BLE_DONE_ABORT 0x1407 |
Operation aborted by command. More... | |
#define | BLE_DONE_STOPPED 0x1408 |
Operation finished with error | |
#define | BLE_ERROR_PAR 0x1800 |
Illegal parameter. More... | |
#define | BLE_ERROR_RXBUF 0x1801 |
No available Rx buffer (Advertiser, Scanner, Initiator) More... | |
#define | BLE_ERROR_NO_SETUP 0x1802 |
Operation using Rx or Tx attemted when not in BLE mode. More... | |
#define | BLE_ERROR_NO_FS 0x1803 |
Operation using Rx or Tx attemted without frequency synth configured. More... | |
#define | BLE_ERROR_SYNTH_PROG 0x1804 |
Synthesizer programming failed to complete on time. More... | |
#define | BLE_ERROR_RXOVF 0x1805 |
Receiver overflowed during operation. More... | |
#define | BLE_ERROR_TXUNF 0x1806 |
#define BLE_DONE_ABORT 0x1407 |
Operation aborted by command.
Definition at line 92 of file rf_ble_mailbox.h.
#define BLE_DONE_CONNECT 0x1404 |
CONNECT_REQ received or transmitted.
Definition at line 89 of file rf_ble_mailbox.h.
#define BLE_DONE_ENDED 0x1406 |
Operation stopped after end trigger.
Definition at line 91 of file rf_ble_mailbox.h.
#define BLE_DONE_MAXNACK 0x1405 |
Maximum number of retransmissions exceeded.
Definition at line 90 of file rf_ble_mailbox.h.
#define BLE_DONE_NOSYNC 0x1402 |
Timeout of subsequent Rx.
Definition at line 87 of file rf_ble_mailbox.h.
#define BLE_DONE_OK 0x1400 |
Operation ended normally.
Definition at line 85 of file rf_ble_mailbox.h.
#define BLE_DONE_RXERR 0x1403 |
Operation ended because of receive error (CRC or other)
Definition at line 88 of file rf_ble_mailbox.h.
#define BLE_DONE_RXTIMEOUT 0x1401 |
Timeout of first Rx of slave operation or end of scan window.
Definition at line 86 of file rf_ble_mailbox.h.
#define BLE_DONE_STOPPED 0x1408 |
Operation stopped after stop command
Definition at line 93 of file rf_ble_mailbox.h.
#define BLE_ERROR_NO_FS 0x1803 |
Operation using Rx or Tx attemted without frequency synth configured.
Definition at line 100 of file rf_ble_mailbox.h.
#define BLE_ERROR_NO_SETUP 0x1802 |
Operation using Rx or Tx attemted when not in BLE mode.
Definition at line 99 of file rf_ble_mailbox.h.
#define BLE_ERROR_PAR 0x1800 |
Illegal parameter.
Definition at line 97 of file rf_ble_mailbox.h.
#define BLE_ERROR_RXBUF 0x1801 |
No available Rx buffer (Advertiser, Scanner, Initiator)
Definition at line 98 of file rf_ble_mailbox.h.
#define BLE_ERROR_RXOVF 0x1805 |
Receiver overflowed during operation.
Definition at line 102 of file rf_ble_mailbox.h.
#define BLE_ERROR_SYNTH_PROG 0x1804 |
Synthesizer programming failed to complete on time.
Definition at line 101 of file rf_ble_mailbox.h.
#define BLE_ERROR_TXUNF 0x1806 |
Transmitter underflowed during operation
Definition at line 103 of file rf_ble_mailbox.h.
#define IRQ_BLE_RX_BUF_FULL (1U << IRQN_BLE_RX_BUF_FULL) |
Definition at line 79 of file rf_ble_mailbox.h.
#define IRQ_BLE_RX_CTRL (1U << IRQN_BLE_RX_CTRL) |
Definition at line 77 of file rf_ble_mailbox.h.
#define IRQ_BLE_RX_CTRL_ACK (1U << IRQN_BLE_RX_CTRL_ACK) |
Definition at line 78 of file rf_ble_mailbox.h.
#define IRQ_BLE_RX_EMPTY (1U << IRQN_BLE_RX_EMPTY) |
Definition at line 76 of file rf_ble_mailbox.h.
#define IRQ_BLE_RX_ENTRY_DONE (1U << IRQN_BLE_RX_ENTRY_DONE) |
Definition at line 80 of file rf_ble_mailbox.h.
#define IRQ_BLE_RX_IGNORED (1U << IRQN_BLE_RX_IGNORED) |
Definition at line 75 of file rf_ble_mailbox.h.
#define IRQ_BLE_RX_NOK (1U << IRQN_BLE_RX_NOK) |
Definition at line 74 of file rf_ble_mailbox.h.
#define IRQ_BLE_RX_OK (1U << IRQN_BLE_RX_OK) |
Definition at line 73 of file rf_ble_mailbox.h.
#define IRQ_BLE_TX_ACK (1U << IRQN_BLE_TX_ACK) |
Definition at line 66 of file rf_ble_mailbox.h.
#define IRQ_BLE_TX_BUFFER_CHANGED (1U << IRQN_BLE_TX_BUFFER_CHANGED) |
Definition at line 72 of file rf_ble_mailbox.h.
#define IRQ_BLE_TX_CTRL (1U << IRQN_BLE_TX_CTRL) |
Definition at line 67 of file rf_ble_mailbox.h.
#define IRQ_BLE_TX_CTRL_ACK (1U << IRQN_BLE_TX_CTRL_ACK) |
Definition at line 68 of file rf_ble_mailbox.h.
#define IRQ_BLE_TX_CTRL_ACK_ACK (1U << IRQN_BLE_TX_CTRL_ACK_ACK) |
Definition at line 69 of file rf_ble_mailbox.h.
#define IRQ_BLE_TX_DONE (1U << IRQN_BLE_TX_DONE) |
Definition at line 65 of file rf_ble_mailbox.h.
#define IRQ_BLE_TX_ENTRY_DONE (1U << IRQN_BLE_TX_ENTRY_DONE) |
Definition at line 71 of file rf_ble_mailbox.h.
#define IRQ_BLE_TX_RETRANS (1U << IRQN_BLE_TX_RETRANS) |
Definition at line 70 of file rf_ble_mailbox.h.
#define IRQN_BLE_RX_BUF_FULL IRQN_RX_BUF_FULL |
Definition at line 62 of file rf_ble_mailbox.h.
#define IRQN_BLE_RX_CTRL IRQN_RX_CTRL |
Definition at line 60 of file rf_ble_mailbox.h.
#define IRQN_BLE_RX_CTRL_ACK IRQN_RX_CTRL_ACK |
Definition at line 61 of file rf_ble_mailbox.h.
#define IRQN_BLE_RX_EMPTY IRQN_RX_EMPTY |
Definition at line 59 of file rf_ble_mailbox.h.
#define IRQN_BLE_RX_ENTRY_DONE IRQN_RX_ENTRY_DONE |
Definition at line 63 of file rf_ble_mailbox.h.
#define IRQN_BLE_RX_IGNORED IRQN_RX_IGNORED |
Definition at line 58 of file rf_ble_mailbox.h.
#define IRQN_BLE_RX_NOK IRQN_RX_NOK |
Definition at line 57 of file rf_ble_mailbox.h.
#define IRQN_BLE_RX_OK IRQN_RX_OK |
Definition at line 56 of file rf_ble_mailbox.h.
#define IRQN_BLE_TX_ACK IRQN_TX_ACK |
Definition at line 49 of file rf_ble_mailbox.h.
#define IRQN_BLE_TX_BUFFER_CHANGED IRQN_TX_BUFFER_CHANGED |
Definition at line 55 of file rf_ble_mailbox.h.
#define IRQN_BLE_TX_CTRL IRQN_TX_CTRL |
Definition at line 50 of file rf_ble_mailbox.h.
#define IRQN_BLE_TX_CTRL_ACK IRQN_TX_CTRL_ACK |
Definition at line 51 of file rf_ble_mailbox.h.
#define IRQN_BLE_TX_CTRL_ACK_ACK IRQN_TX_CTRL_ACK_ACK |
Definition at line 52 of file rf_ble_mailbox.h.
#define IRQN_BLE_TX_DONE IRQN_TX_DONE |
Definition at line 48 of file rf_ble_mailbox.h.
#define IRQN_BLE_TX_ENTRY_DONE IRQN_TX_ENTRY_DONE |
Definition at line 54 of file rf_ble_mailbox.h.
#define IRQN_BLE_TX_RETRANS IRQN_TX_RETRANS |
Definition at line 53 of file rf_ble_mailbox.h.