#include <rf_common_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x0802. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips if the rule involves skipping. More... | |
} | condition |
uint8_t | mode |
The main mode to use 0x00: BLE 0x01: IEEE 802.15.4 0x02: 2 Mbps GFSK 0x05: 5 Mbps coded 8-FSK 0x06: ANT 0xFF: Keep existing mode; update overrides only Others: Reserved More... | |
uint8_t | loDivider |
LO divider setting to use. Supported values: 0 (equivalent to 2), 2, 5, 6, 10, 12, 15, and 30. Value of 0 or 2 only supported for devices that support 2.4 GHz operation. More... | |
struct { | |
uint16_t frontEndMode:3 | |
0x00: Differential mode 0x01: Single-ended mode RFP 0x02: Single-ended mode RFN 0x05 Single-ended mode RFP with external frontend control on RF pins (RFN and RXTX) 0x06 Single-ended mode RFN with external frontend control on RF pins (RFP and RXTX) Others: Reserved More... | |
uint16_t biasMode:1 | |
0: Internal bias 1: External bias More... | |
uint16_t __pad0__:6 | |
uint16_t bNoFsPowerUp:1 | |
0: Power up frequency synth 1: Do not power up frequency synth More... | |
} | config |
Configuration options. More... | |
struct { | |
uint16_t IB:6 | |
Value to write to the PA power control field at 25 °C. More... | |
uint16_t GC:2 | |
Value to write to the gain control of the 1st stage of the PA. More... | |
uint16_t boost:1 | |
Value of boost bit in synth. More... | |
uint16_t tempCoeff:7 | |
Temperature coefficient for IB. 0: No temperature compensation. More... | |
} | txPower |
Transmit power. More... | |
uint32_t * | pRegOverride |
Pointer to a list of hardware and configuration registers to override. If NULL, no override is used. More... | |
Definition at line 165 of file rf_common_cmd.h.
uint16_t rfc_CMD_RADIO_SETUP_s::__pad0__ |
Definition at line 204 of file rf_common_cmd.h.
uint8_t rfc_CMD_RADIO_SETUP_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 174 of file rf_common_cmd.h.
uint16_t rfc_CMD_RADIO_SETUP_s::biasMode |
0: Internal bias
1: External bias
Definition at line 202 of file rf_common_cmd.h.
uint16_t rfc_CMD_RADIO_SETUP_s::bNoFsPowerUp |
0: Power up frequency synth
1: Do not power up frequency synth
Definition at line 205 of file rf_common_cmd.h.
uint16_t rfc_CMD_RADIO_SETUP_s::boost |
Value of boost bit in synth.
Definition at line 211 of file rf_common_cmd.h.
uint16_t rfc_CMD_RADIO_SETUP_s::commandNo |
The command ID number 0x0802.
Definition at line 166 of file rf_common_cmd.h.
struct { ... } rfc_CMD_RADIO_SETUP_s::condition |
struct { ... } rfc_CMD_RADIO_SETUP_s::config |
Configuration options.
uint16_t rfc_CMD_RADIO_SETUP_s::frontEndMode |
0x00: Differential mode
0x01: Single-ended mode RFP
0x02: Single-ended mode RFN
0x05 Single-ended mode RFP with external frontend control on RF pins (RFN and RXTX)
0x06 Single-ended mode RFN with external frontend control on RF pins (RFP and RXTX)
Others: Reserved
Definition at line 196 of file rf_common_cmd.h.
uint16_t rfc_CMD_RADIO_SETUP_s::GC |
Value to write to the gain control of the 1st stage of the PA.
Definition at line 210 of file rf_common_cmd.h.
uint16_t rfc_CMD_RADIO_SETUP_s::IB |
Value to write to the PA power control field at 25 °C.
Definition at line 209 of file rf_common_cmd.h.
uint8_t rfc_CMD_RADIO_SETUP_s::loDivider |
LO divider setting to use. Supported values: 0 (equivalent to 2), 2, 5, 6, 10, 12, 15, and 30.
Value of 0 or 2 only supported for devices that support 2.4 GHz operation.
Definition at line 192 of file rf_common_cmd.h.
uint8_t rfc_CMD_RADIO_SETUP_s::mode |
The main mode to use
0x00: BLE
0x01: IEEE 802.15.4
0x02: 2 Mbps GFSK
0x05: 5 Mbps coded 8-FSK
0x06: ANT
0xFF: Keep existing mode; update overrides only
Others: Reserved
Definition at line 184 of file rf_common_cmd.h.
uint8_t rfc_CMD_RADIO_SETUP_s::nSkip |
Number of skips if the rule involves skipping.
Definition at line 182 of file rf_common_cmd.h.
uint8_t rfc_CMD_RADIO_SETUP_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 177 of file rf_common_cmd.h.
rfc_radioOp_t* rfc_CMD_RADIO_SETUP_s::pNextOp |
Pointer to the next operation to run after this operation is done.
Definition at line 170 of file rf_common_cmd.h.
uint32_t* rfc_CMD_RADIO_SETUP_s::pRegOverride |
Pointer to a list of hardware and configuration registers to override. If NULL, no override is used.
Definition at line 214 of file rf_common_cmd.h.
uint8_t rfc_CMD_RADIO_SETUP_s::rule |
Condition for running next command: Rule for how to proceed.
Definition at line 181 of file rf_common_cmd.h.
ratmr_t rfc_CMD_RADIO_SETUP_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
Definition at line 171 of file rf_common_cmd.h.
struct { ... } rfc_CMD_RADIO_SETUP_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_CMD_RADIO_SETUP_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
Definition at line 167 of file rf_common_cmd.h.
uint16_t rfc_CMD_RADIO_SETUP_s::tempCoeff |
Temperature coefficient for IB. 0: No temperature compensation.
Definition at line 212 of file rf_common_cmd.h.
uint8_t rfc_CMD_RADIO_SETUP_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 176 of file rf_common_cmd.h.
uint8_t rfc_CMD_RADIO_SETUP_s::triggerType |
The type of trigger.
Definition at line 173 of file rf_common_cmd.h.
struct { ... } rfc_CMD_RADIO_SETUP_s::txPower |
Transmit power.