#include <rf_prop_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x3801. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips if the rule involves skipping. More... | |
} | condition |
struct { | |
uint8_t bFsOff:1 | |
0: Keep frequency synth on after command 1: Turn frequency synth off after command More... | |
uint8_t __pad0__:2 | |
uint8_t bUseCrc:1 | |
0: Do not append CRC 1: Append CRC More... | |
uint8_t bVarLen:1 | |
0: Fixed length 1: Transmit length as first byte More... | |
} | pktConf |
uint8_t | pktLen |
Packet length. More... | |
uint32_t | syncWord |
Sync word to transmit. More... | |
uint8_t * | pPkt |
Pointer to packet. More... | |
Definition at line 120 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_TX_s::__pad0__ |
Definition at line 142 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_TX_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 129 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_TX_s::bFsOff |
0: Keep frequency synth on after command
1: Turn frequency synth off after command
Definition at line 140 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_TX_s::bUseCrc |
0: Do not append CRC
1: Append CRC
Definition at line 143 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_TX_s::bVarLen |
0: Fixed length
1: Transmit length as first byte
Definition at line 145 of file rf_prop_cmd.h.
uint16_t rfc_CMD_PROP_TX_s::commandNo |
The command ID number 0x3801.
Definition at line 121 of file rf_prop_cmd.h.
struct { ... } rfc_CMD_PROP_TX_s::condition |
uint8_t rfc_CMD_PROP_TX_s::nSkip |
Number of skips if the rule involves skipping.
Definition at line 137 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_TX_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 132 of file rf_prop_cmd.h.
struct { ... } rfc_CMD_PROP_TX_s::pktConf |
uint8_t rfc_CMD_PROP_TX_s::pktLen |
Packet length.
Definition at line 148 of file rf_prop_cmd.h.
rfc_radioOp_t* rfc_CMD_PROP_TX_s::pNextOp |
Pointer to the next operation to run after this operation is done.
Definition at line 125 of file rf_prop_cmd.h.
uint8_t* rfc_CMD_PROP_TX_s::pPkt |
Pointer to packet.
Definition at line 150 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_TX_s::rule |
Condition for running next command: Rule for how to proceed.
Definition at line 136 of file rf_prop_cmd.h.
ratmr_t rfc_CMD_PROP_TX_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
Definition at line 126 of file rf_prop_cmd.h.
struct { ... } rfc_CMD_PROP_TX_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_CMD_PROP_TX_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
Definition at line 122 of file rf_prop_cmd.h.
uint32_t rfc_CMD_PROP_TX_s::syncWord |
Sync word to transmit.
Definition at line 149 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_TX_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 131 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_TX_s::triggerType |
The type of trigger.
Definition at line 128 of file rf_prop_cmd.h.