CC13xx Driver Library
rfc.h
Go to the documentation of this file.
1 /******************************************************************************
2 * Filename: rfc.h
3 * Revised: 2015-11-17 12:03:08 +0100 (Tue, 17 Nov 2015)
4 * Revision: 45108
5 *
6 * Description: Defines and prototypes for the RF Core.
7 *
8 * Copyright (c) 2015, Texas Instruments Incorporated
9 * All rights reserved.
10 *
11 * Redistribution and use in source and binary forms, with or without
12 * modification, are permitted provided that the following conditions are met:
13 *
14 * 1) Redistributions of source code must retain the above copyright notice,
15 * this list of conditions and the following disclaimer.
16 *
17 * 2) Redistributions in binary form must reproduce the above copyright notice,
18 * this list of conditions and the following disclaimer in the documentation
19 * and/or other materials provided with the distribution.
20 *
21 * 3) Neither the name of the ORGANIZATION nor the names of its contributors may
22 * be used to endorse or promote products derived from this software without
23 * specific prior written permission.
24 *
25 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
26 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
27 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
28 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
29 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
30 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
31 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
32 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
33 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
34 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
35 * POSSIBILITY OF SUCH DAMAGE.
36 *
37 ******************************************************************************/
38 
39 //*****************************************************************************
40 //
43 //
44 //*****************************************************************************
45 
46 #ifndef __RFC_H__
47 #define __RFC_H__
48 
49 //*****************************************************************************
50 //
51 // If building with a C++ compiler, make all of the definitions in this header
52 // have a C binding.
53 //
54 //*****************************************************************************
55 #ifdef __cplusplus
56 extern "C"
57 {
58 #endif
59 
60 #include <stdbool.h>
61 #include <stdint.h>
62 #include <inc/hw_types.h>
63 #include <inc/hw_memmap.h>
64 #include <inc/hw_rfc_pwr.h>
65 #include <inc/hw_rfc_dbell.h>
66 
67 //*****************************************************************************
68 //
69 // Support for DriverLib in ROM:
70 // This section renames all functions that are not "static inline", so that
71 // calling these functions will default to implementation in flash. At the end
72 // of this file a second renaming will change the defaults to implementation in
73 // ROM for available functions.
74 //
75 // To force use of the implementation in flash, e.g. for debugging:
76 // - Globally: Define DRIVERLIB_NOROM at project level
77 // - Per function: Use prefix "NOROM_" when calling the function
78 //
79 //*****************************************************************************
80 #if !defined(DOXYGEN)
81  #define RFCCpeIntGetAndClear NOROM_RFCCpeIntGetAndClear
82  #define RFCDoorbellSendTo NOROM_RFCDoorbellSendTo
83 #endif
84 
85 //*****************************************************************************
86 //
87 // API Functions and prototypes
88 //
89 //*****************************************************************************
90 
91 //*****************************************************************************
92 //
100 //
101 //*****************************************************************************
102 __STATIC_INLINE void
104 {
105  //
106  // Enable all clocks
107  //
108  HWREG(RFC_PWR_NONBUF_BASE + RFC_PWR_O_PWMCLKEN) =
120 }
121 
122 //*****************************************************************************
123 //
135 //
136 //*****************************************************************************
137 __STATIC_INLINE void
139 {
140  //
141  // Disable all clocks
142  //
143  HWREG(RFC_PWR_NONBUF_BASE + RFC_PWR_O_PWMCLKEN) = 0x0;
144 }
145 
146 //*****************************************************************************
147 //
149 //
150 //*****************************************************************************
151 __STATIC_INLINE void
152 RFCCpe0IntEnable(uint32_t ui32Mask)
153 {
154  //
155  // Multiplex RF Core interrupts to CPE0 IRQ.
156  //
157  HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFCPEISL) &= ~ui32Mask;
158 
159  do
160  {
161  //
162  // Clear any pending interrupts.
163  //
164  HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFCPEIFG) = 0x0;
165  }while(HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFCPEIFG) != 0x0);
166 
167  //
168  // Enable the masked interrupts
169  //
170  HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFCPEIEN) |= ui32Mask;
171 }
172 
173 
174 //*****************************************************************************
175 //
177 //
178 //*****************************************************************************
179 __STATIC_INLINE void
180 RFCCpe1IntEnable(uint32_t ui32Mask)
181 {
182  //
183  // Multiplex RF Core interrupts to CPE1 IRQ.
184  //
185  HWREG( RFC_DBELL_BASE + RFC_DBELL_O_RFCPEISL) |= ui32Mask;
186 
187  do
188  {
189  //
190  // Clear any pending interrupts.
191  //
192  HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFCPEIFG) = 0x0;
193  }while(HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFCPEIFG) != 0x0);
194 
195  //
196  // Enable the masked interrupts
197  //
198  HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFCPEIEN) |= ui32Mask;
199 }
200 
201 
202 //*****************************************************************************
203 //
206 //
207 //*****************************************************************************
208 __STATIC_INLINE void
209 RFCHwIntEnable(uint32_t ui32Mask)
210 {
211  //
212  // Clear any pending interrupts.
213  //
214  HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFHWIFG) = 0x0;
215 
216  //
217  // Enable the masked interrupts
218  //
219  HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFHWIEN) |= ui32Mask;
220 }
221 
222 
223 //*****************************************************************************
224 //
226 //
227 //*****************************************************************************
228 __STATIC_INLINE void
229 RFCCpeIntDisable(uint32_t ui32Mask)
230 {
231  //
232  // Disable the masked interrupts
233  //
234  HWREG( RFC_DBELL_BASE + RFC_DBELL_O_RFCPEIEN ) &= ~ui32Mask;
235 
236  do
237  {
238  //
239  // Clear any pending interrupts.
240  //
241  HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFCPEIFG) = 0x0;
242  }while(HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFCPEIFG) != 0x0);
243 }
244 
245 
246 //*****************************************************************************
247 //
249 //
250 //*****************************************************************************
251 __STATIC_INLINE void
252 RFCHwIntDisable(uint32_t ui32Mask)
253 {
254  //
255  // Disable the masked interrupts
256  //
257  HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFHWIEN) &= ~ui32Mask;
258 
259  //
260  // Clear any pending interrupts.
261  //
262  HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFHWIFG) = 0x0;
263 }
264 
265 
266 //*****************************************************************************
267 //
269 //
270 //*****************************************************************************
271 extern uint32_t RFCCpeIntGetAndClear(void);
272 
273 
274 //*****************************************************************************
275 //
277 //
278 //*****************************************************************************
279 __STATIC_INLINE void
280 RFCCpeIntClear(uint32_t ui32Mask)
281 {
282  do
283  {
284  //
285  // Clear interrupts that may now be pending
286  //
287  HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFCPEIFG) &= ~ui32Mask;
288  }while(HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFCPEIFG) != ~ui32Mask);
289 }
290 
291 
292 //*****************************************************************************
293 //
295 //
296 //*****************************************************************************
297 __STATIC_INLINE void
298 RFCHwIntClear(uint32_t ui32Mask)
299 {
300  //
301  // Clear pending interrupts.
302  //
303  HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFHWIFG) &= ~ui32Mask;
304 }
305 
306 
307 //*****************************************************************************
308 //
310 //
311 //*****************************************************************************
312 __STATIC_INLINE void
314 {
315  //
316  // Clear any pending interrupts.
317  //
318  HWREG(RFC_DBELL_BASE + RFC_DBELL_O_RFACKIFG) = 0x0;
319 }
320 
321 
322 //*****************************************************************************
323 //
325 //
326 //*****************************************************************************
327 extern uint32_t RFCDoorbellSendTo(uint32_t pOp);
328 
329 
330 //*****************************************************************************
331 //
332 // Support for DriverLib in ROM:
333 // Redirect to implementation in ROM when available.
334 //
335 //*****************************************************************************
336 #if !defined(DRIVERLIB_NOROM) && !defined(DOXYGEN)
337  #include <driverlib/rom.h>
338  #ifdef ROM_RFCCpeIntGetAndClear
339  #undef RFCCpeIntGetAndClear
340  #define RFCCpeIntGetAndClear ROM_RFCCpeIntGetAndClear
341  #endif
342  #ifdef ROM_RFCDoorbellSendTo
343  #undef RFCDoorbellSendTo
344  #define RFCDoorbellSendTo ROM_RFCDoorbellSendTo
345  #endif
346 #endif
347 
348 //*****************************************************************************
349 //
350 // Mark the end of the C bindings section for C++ compilers.
351 //
352 //*****************************************************************************
353 #ifdef __cplusplus
354 }
355 #endif
356 
357 #endif // __RFC_H__
358 
359 //*****************************************************************************
360 //
363 //
364 //*****************************************************************************
static void RFCHwIntDisable(uint32_t ui32Mask)
Disable HW interrupt.
Definition: rfc.h:252
static void RFCCpe1IntEnable(uint32_t ui32Mask)
Enable CPE1 interrupt.
Definition: rfc.h:180
static void RFCCpeIntDisable(uint32_t ui32Mask)
Disable CPE interrupt.
Definition: rfc.h:229
static void RFCCpeIntClear(uint32_t ui32Mask)
Clear interrupt flags.
Definition: rfc.h:280
static void RFCCpe0IntEnable(uint32_t ui32Mask)
Enable CPE0 interrupt.
Definition: rfc.h:152
static void RFCAckIntClear(void)
Clear interrupt flags.
Definition: rfc.h:313
uint32_t RFCCpeIntGetAndClear(void)
Get and clear CPE interrupt flags.
Definition: rfc.c:47
static void RFCClockDisable(void)
Disable the RF core clocks.
Definition: rfc.h:138
uint32_t RFCDoorbellSendTo(uint32_t pOp)
Send command to doorbell and wait for ack.
Definition: rfc.c:65
static void RFCHwIntEnable(uint32_t ui32Mask)
Definition: rfc.h:209
static void RFCHwIntClear(uint32_t ui32Mask)
Clear interrupt flags.
Definition: rfc.h:298
static void RFCClockEnable(void)
Enable the RF core clocks.
Definition: rfc.h:103