![]() |
![]() |
Functions | |
int | Raw6Output (HANDLE hSock, UINT8 *buf, INT32 size, INT32 *pRetSize) |
void | Raw6Input (PBM_Pkt *pPkt, IPV6HDR *ptr_ipv6hdr, UINT8 Protocol) |
void Raw6Input | ( | PBM_Pkt * | pPkt, | |
IPV6HDR * | ptr_ipv6hdr, | |||
UINT8 | Protocol | |||
) |
Description
The function is called when a RAW packet is received over the IPv6 Network.
[in] | pPkt | The packet received. |
[in] | ptr_ipv6hdr | The IPv6 Header of the received packet. |
[in] | Protocol | The Layer4 Protocol received. This is not necessarily the same as the Next Header in the IPv6 header. |
Not | Applicable. |
int Raw6Output | ( | HANDLE | hSock, | |
UINT8 * | buf, | |||
INT32 | size, | |||
INT32 * | pRetSize | |||
) |
Description
The function is called to transmit a RAW packet over an IPv6 network.
[in] | hSock | Socket handle using which the packet is sent out. |
[in] | buf | Data Buffer which is to be sent out. |
[in] | size | Length of the data buffer to be sent out. |
[out] | pRetSize | Actual Length of data sent out. |
Success | - 0 Error - Non Zero |