module ti.sysbios.knl.Event

Event Manager

SYS/BIOS events are a means of communication between Tasks and other threads such as Hwis, Swis, and other Tasks, or between Tasks and other SYS/BIOS objects. Other SYS/BIOS objects include semaphores, mailboxes, message queues, etc. Only tasks can wait for events; whereas tasks, Hwis, Swis, or SYS/BIOS objects can post them. [ more ... ]
C synopsis target-domain sourced in ti/sysbios/knl/Event.xdc
#include <ti/sysbios/knl/Event.h>
Functions
Void
Void
Void
UInt 
Void
UInt 
Event_pend// Wait for events defined in 'and' OR 'or' masks(Event_Handle handle, UInt andMask, UInt orMask, UInt32 timeout);
Void 
Functions common to all target instances
Functions common to all target modules
Defines
#define
#define
Event_Id_01//  (UInt)0x2
#define
Event_Id_02//  (UInt)0x4
#define
Event_Id_03//  (UInt)0x8
#define
Event_Id_04//  (UInt)0x10
#define
Event_Id_05//  (UInt)0x20
#define
Event_Id_06//  (UInt)0x40
#define
Event_Id_07//  (UInt)0x80
#define
Event_Id_08//  (UInt)0x100
#define
Event_Id_09//  (UInt)0x200
#define
Event_Id_10//  (UInt)0x400
#define
Event_Id_11//  (UInt)0x800
#define
Event_Id_12//  (UInt)0x1000
#define
Event_Id_13//  (UInt)0x2000
#define
Event_Id_14//  (UInt)0x4000
#define
Event_Id_15//  (UInt)0x8000
#define
Event_Id_16//  (UInt)0x10000
#define
Event_Id_17//  (UInt)0x20000
#define
Event_Id_18//  (UInt)0x40000
#define
Event_Id_19//  (UInt)0x80000
#define
Event_Id_20//  (UInt)0x100000
#define
Event_Id_21//  (UInt)0x200000
#define
Event_Id_22//  (UInt)0x400000
#define
Event_Id_23//  (UInt)0x800000
#define
Event_Id_24//  (UInt)0x1000000
#define
Event_Id_25//  (UInt)0x2000000
#define
Event_Id_26//  (UInt)0x4000000
#define
Event_Id_27//  (UInt)0x8000000
#define
Event_Id_28//  (UInt)0x10000000
#define
Event_Id_29//  (UInt)0x20000000
#define
Event_Id_30//  (UInt)0x40000000
#define
Event_Id_31//  (UInt)0x80000000
#define
Typedefs
typedef Event_Object *
typedef struct
typedef struct
typedef struct
Constants
extern const Assert_Id 
extern const Assert_Id 
extern const Assert_Id 
extern const Assert_Id 
extern const Assert_Id 
extern const Log_Event 
extern const Log_Event 
 
DETAILS
SYS/BIOS events are a means of communication between Tasks and other threads such as Hwis, Swis, and other Tasks, or between Tasks and other SYS/BIOS objects. Other SYS/BIOS objects include semaphores, mailboxes, message queues, etc. Only tasks can wait for events; whereas tasks, Hwis, Swis, or SYS/BIOS objects can post them.
In order for a task to be notified of an event from a SYS/BIOS object an event object must first be registered with that object. Separate APIs are provided (in their respective modules) for each of the SYS/BIOS object types that support this feature.
Events are synchronous in nature, meaning that a receiving task will block or pend while waiting for the events to occur. When the desired events are received, the pending task continues its execution, as it would after a call to Semaphore_pend(), for example.
Tasks can also wait on events that are not linked to other SYS/BIOS objects. These events are explicitly posted from other threads such as tasks, Swis, or Hwis. A task does not register to receive these events; the sending thread simply posts its event(s) to the event object the task is pending on. This scenario is similar to having an ISR post a semaphore.
A task can wait on events from multiple resources and/or threads; thus, it can be waiting for a semaphore to be posted and for a message to arrive in a message queue or an ISR thread to signal that an event has occurred.
Events are binary. Events become available (posted) on each Event_post() of the eventId and become non-available (consumed) on each qualifying Event_pend() mask.
Unlike Semaphores, only a single task can pend on an Event object.
pend is used to wait for events. The andMask & orMask determine which event(s) must occur before returning from pend. The timeout parameter allows the task to wait until a timeout, wait indefinitely, or not wait at all. A return value of zero indicates that a timeout has occurred. A non-zero return value is the set of events that were active at the time the task was unblocked.
The andMask defines a set of events that must ALL occur to allow pend to return.
The orMask defines a set of events that will cause pend to return if ANY of them occur.
All active events present in the orMask are consumed (ie removed from the event object) upon return from pend. Only when all events present in the andMask are active are they consumed on return from pend.
pend returns immediately if the andMask OR orMask conditions are true upon entry.
post is used to signal events. If a task is waiting for the event and all of the event conditions are met, post unblocks the task. If no task is waiting, post simply registers the event with the event object and returns.
The maximum number of eventIds supported is target specific and depends on the number of bits in a UInt data type. For 6x and ARM devices the maximum number of eventIds is therefore 32. For 28x and MSP430 devices, the maximum number of eventIds is 16.

Calling Context

Function Hwi Swi Task Main Startup
create N N Y Y N
Params_init Y Y Y Y Y
construct N N Y Y N
delete N N Y Y N
destruct N N Y Y N
getPostedEvents Y Y Y Y Y
pend N* N* Y N* N
post Y Y Y Y N
Definitions: (N* means OK to call iff the timeout parameter is set to '0'.)
  • Hwi: API is callable from a Hwi thread.
  • Swi: API is callable from a Swi thread.
  • Task: API is callable from a Task thread.
  • Main: API is callable during any of these phases:
    • In your module startup after this module is started (e.g. Event_Module_startupDone() returns TRUE).
    • During xdc.runtime.Startup.lastFxns.
    • During main().
    • During BIOS.startupFxns.
  • Startup: API is callable during any of these phases:
    • During xdc.runtime.Startup.firstFxns.
    • In your module startup before this module is started (e.g. Event_Module_startupDone() returns FALSE).
 
const Event_Id_00

Pre-defined Event Ids

C synopsis target-domain
#define Event_Id_00 (UInt)0x1
 
DETAILS
Event_Ids are provided to simplify the specification of andMasks and orMasks arguments to Event_pend().
Since each Event_Id is a bitmask composed of only a single bit, a group of Event_Ids within an andMask or orMask can be indicated by simply adding them together. For instance, to indicate that a task is to be awakened only when both Event_Id_00 and Event_Id_01 have been posted, the andMask for Event_pend() would be constructed as below:
  Event_pend(event, Event_Id_00+EventId_01, Event_Id_NONE,
             BIOS_WAIT_FOREVER);
As shown above, Event_Id_NONE is to be used as an empty (NULL) andMask or orMask.
NOTE
For targets where a UInt is 32 bits in length, Event_Id_00 thru Event_Id_31 can be used.
For targets where a UInt is 16 bits in length, Event_Id_00 thru Event_Id_15 can be used.
 
const Event_Id_01
C synopsis target-domain
#define Event_Id_01 (UInt)0x2
 
SEE
 
const Event_Id_02
C synopsis target-domain
#define Event_Id_02 (UInt)0x4
 
SEE
 
const Event_Id_03
C synopsis target-domain
#define Event_Id_03 (UInt)0x8
 
SEE
 
const Event_Id_04
C synopsis target-domain
#define Event_Id_04 (UInt)0x10
 
SEE
 
const Event_Id_05
C synopsis target-domain
#define Event_Id_05 (UInt)0x20
 
SEE
 
const Event_Id_06
C synopsis target-domain
#define Event_Id_06 (UInt)0x40
 
SEE
 
const Event_Id_07
C synopsis target-domain
#define Event_Id_07 (UInt)0x80
 
SEE
 
const Event_Id_08
C synopsis target-domain
#define Event_Id_08 (UInt)0x100
 
SEE
 
const Event_Id_09
C synopsis target-domain
#define Event_Id_09 (UInt)0x200
 
SEE
 
const Event_Id_10
C synopsis target-domain
#define Event_Id_10 (UInt)0x400
 
SEE
 
const Event_Id_11
C synopsis target-domain
#define Event_Id_11 (UInt)0x800
 
SEE
 
const Event_Id_12
C synopsis target-domain
#define Event_Id_12 (UInt)0x1000
 
SEE
 
const Event_Id_13
C synopsis target-domain
#define Event_Id_13 (UInt)0x2000
 
SEE
 
const Event_Id_14
C synopsis target-domain
#define Event_Id_14 (UInt)0x4000
 
SEE
 
const Event_Id_15
C synopsis target-domain
#define Event_Id_15 (UInt)0x8000
 
SEE
 
const Event_Id_16
C synopsis target-domain
#define Event_Id_16 (UInt)0x10000
 
SEE
 
const Event_Id_17
C synopsis target-domain
#define Event_Id_17 (UInt)0x20000
 
SEE
 
const Event_Id_18
C synopsis target-domain
#define Event_Id_18 (UInt)0x40000
 
SEE
 
const Event_Id_19
C synopsis target-domain
#define Event_Id_19 (UInt)0x80000
 
SEE
 
const Event_Id_20
C synopsis target-domain
#define Event_Id_20 (UInt)0x100000
 
SEE
 
const Event_Id_21
C synopsis target-domain
#define Event_Id_21 (UInt)0x200000
 
SEE
 
const Event_Id_22
C synopsis target-domain
#define Event_Id_22 (UInt)0x400000
 
SEE
 
const Event_Id_23
C synopsis target-domain
#define Event_Id_23 (UInt)0x800000
 
SEE
 
const Event_Id_24
C synopsis target-domain
#define Event_Id_24 (UInt)0x1000000
 
SEE
 
const Event_Id_25
C synopsis target-domain
#define Event_Id_25 (UInt)0x2000000
 
SEE
 
const Event_Id_26
C synopsis target-domain
#define Event_Id_26 (UInt)0x4000000
 
SEE
 
const Event_Id_27
C synopsis target-domain
#define Event_Id_27 (UInt)0x8000000
 
SEE
 
const Event_Id_28
C synopsis target-domain
#define Event_Id_28 (UInt)0x10000000
 
SEE
 
const Event_Id_29
C synopsis target-domain
#define Event_Id_29 (UInt)0x20000000
 
SEE
 
const Event_Id_30
C synopsis target-domain
#define Event_Id_30 (UInt)0x40000000
 
SEE
 
const Event_Id_31
C synopsis target-domain
#define Event_Id_31 (UInt)0x80000000
 
SEE
 
const Event_Id_NONE
C synopsis target-domain
#define Event_Id_NONE (UInt)0
 
SEE
 
config Event_A_badContext  // module-wide

Asserted when pend is called with non-zero timeout from other than a Task context

C synopsis target-domain
extern const Assert_Id Event_A_badContext;
 
 
config Event_A_eventInUse  // module-wide

Asserted when pend is called by multiple tasks on the same Event object

C synopsis target-domain
extern const Assert_Id Event_A_eventInUse;
 
 
config Event_A_nullEventId  // module-wide

Asserted when post is called with eventId == 0

C synopsis target-domain
extern const Assert_Id Event_A_nullEventId;
 
 
config Event_A_nullEventMasks  // module-wide

Asserted when pend is called with andMask and orMask == 0

C synopsis target-domain
extern const Assert_Id Event_A_nullEventMasks;
 
 
config Event_A_pendTaskDisabled  // module-wide

Asserted in Event_pend()

C synopsis target-domain
extern const Assert_Id Event_A_pendTaskDisabled;
 
DETAILS
Assert raised if Event_pend() is called with the Task or Swi scheduler disabled.
 
config Event_LM_pend  // module-wide

Logged on calls to Event_pend()

C synopsis target-domain
extern const Log_Event Event_LM_pend;
 
 
config Event_LM_post  // module-wide

Logged on calls to Event_post()

C synopsis target-domain
extern const Log_Event Event_LM_post;
 
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId Event_Module_id();
// Get this module's unique id
 
Bool Event_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle Event_Module_heap();
// The heap from which this module allocates memory
 
Bool Event_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 Event_Module_getMask();
// Returns the diagnostics mask for this module
 
Void Event_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types

C synopsis target-domain
typedef struct Event_Object Event_Object;
// Opaque internal representation of an instance object
 
typedef Event_Object *Event_Handle;
// Client reference to an instance object
 
typedef struct Event_Struct Event_Struct;
// Opaque client structure large enough to hold an instance object
 
Event_Handle Event_handle(Event_Struct *structP);
// Convert this instance structure pointer into an instance handle
 
Event_Struct *Event_struct(Event_Handle handle);
// Convert this instance handle into an instance structure pointer
Instance Config Parameters

C synopsis target-domain
typedef struct Event_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
} Event_Params;
 
Void Event_Params_init(Event_Params *params);
// Initialize this config-params structure with supplier-specified defaults before instance creation
Runtime Instance Creation

C synopsis target-domain
Event_Handle Event_create(const Event_Params *params, Error_Block *eb);
// Allocate and initialize a new instance object and return its handle
 
Void Event_construct(Event_Struct *structP, const Event_Params *params);
// Initialize a new instance object inside the provided structure
ARGUMENTS
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
This function creates a new Event object.
Instance Deletion

C synopsis target-domain
Void Event_delete(Event_Handle *handleP);
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void Event_destruct(Event_Struct *structP);
// Finalize the instance object inside the provided structure
 
Event_getPostedEvents()  // instance

Returns the set of events that have not been consumed by a task (ie those events that have not fully satisfied any pend() conditions). No events are consumed!

C synopsis target-domain
UInt Event_getPostedEvents(Event_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created Event instance object
RETURNS
All un-consumed events posted to the event.
 
Event_pend()  // instance

Wait for events defined in 'and' OR 'or' masks

C synopsis target-domain
UInt Event_pend(Event_Handle handle, UInt andMask, UInt orMask, UInt32 timeout);
 
ARGUMENTS
handle — handle of a previously-created Event instance object
andMask — return from pend() when ALL of these events have occurred
orMask — return from pend() when ANY of these events have occurred
timeout — return from pend() after this many system time units
RETURNS
All consumed events or zero if timeout.
DETAILS
pend() is used to wait for events. The andMask and orMask determine which event(s) must occur before returning from pend(). The timeout parameter allows the task to wait until a timeout, wait indefinitely, or not wait at all. A return value of zero indicates that a timeout has occurred. A non-zero return value is the set of events that were active at the time the task was unblocked.
The andMask defines a set of events that must ALL occur to allow pend() to return.
The orMask defines a set of events that will cause pend() to return if ANY of them occur.
All active events present in the orMask are consumed (i.e. removed from the event object) upon return from pend(). Only when all events present in the andMask are active are they consumed on return from pend().
The pend conditions are satisfied when either ALL of the events in the andMask occur or ANY of the events in the orMask occur.
A timeout value of BIOS_WAIT_FOREVER causes the task to wait indefinitely for matching events to be posted.
A timeout value of BIOS_NO_WAIT causes Event_pend to return immediately.
 
Event_post()  // instance

Post event(s) to an event object

C synopsis target-domain
Void Event_post(Event_Handle handle, UInt eventMask);
 
ARGUMENTS
handle — handle of a previously-created Event instance object
eventMask — mask of eventIds to post (must be non-zero)
DETAILS
Event_post() is used to signal events. If a task is waiting for the event and the event conditions are met, post() unblocks the task. If no tasks are waiting, post() simply registers the event with the event object and returns.
Instance Built-Ins

C synopsis target-domain
Int Event_Object_count();
// The number of statically-created instance objects
 
Event_Handle Event_Object_get(Event_Object *array, Int i);
// The handle of the i-th statically-created instance object (array == NULL)
 
Event_Handle Event_Object_first();
// The handle of the first dynamically-created instance object, or NULL
 
Event_Handle Event_Object_next(Event_Handle handle);
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle Event_Object_heap();
// The heap used to allocate dynamically-created instance objects
 
Types_Label *Event_Handle_label(Event_Handle handle, Types_Label *buf);
// The label associated with this instance object
 
String Event_Handle_name(Event_Handle handle);
// The name of this instance object
 
Configuration settings sourced in ti/sysbios/knl/Event.xdc
var Event = xdc.useModule('ti.sysbios.knl.Event');
module-wide constants & types
    const Event.Id_01//  = 0x2;
    const Event.Id_02//  = 0x4;
    const Event.Id_03//  = 0x8;
    const Event.Id_04//  = 0x10;
    const Event.Id_05//  = 0x20;
    const Event.Id_06//  = 0x40;
    const Event.Id_07//  = 0x80;
    const Event.Id_08//  = 0x100;
    const Event.Id_09//  = 0x200;
    const Event.Id_10//  = 0x400;
    const Event.Id_11//  = 0x800;
    const Event.Id_12//  = 0x1000;
    const Event.Id_13//  = 0x2000;
    const Event.Id_14//  = 0x4000;
    const Event.Id_15//  = 0x8000;
    const Event.Id_16//  = 0x10000;
    const Event.Id_17//  = 0x20000;
    const Event.Id_18//  = 0x40000;
    const Event.Id_19//  = 0x80000;
    const Event.Id_20//  = 0x100000;
    const Event.Id_21//  = 0x200000;
    const Event.Id_22//  = 0x400000;
    const Event.Id_23//  = 0x800000;
    const Event.Id_24//  = 0x1000000;
    const Event.Id_25//  = 0x2000000;
    const Event.Id_26//  = 0x4000000;
    const Event.Id_27//  = 0x8000000;
    const Event.Id_28//  = 0x10000000;
    const Event.Id_29//  = 0x20000000;
    const Event.Id_30//  = 0x40000000;
    const Event.Id_31//  = 0x80000000;
    const Event.Id_NONE//  = 0;
module-wide config parameters
        msg: "A_badContext: bad calling context. Must be called from a Task."
    };
        msg: "A_eventInUse: Event object already in use."
    };
        msg: "A_nullEventId: posted eventId is null."
    };
        msg: "A_nullEventMasks: orMask and andMask are null."
    };
        msg: "A_pendTaskDisabled: Cannot call Event_pend() while the Task or Swi scheduler is disabled."
    };
        mask: Diags.USER1 | Diags.USER2,
        msg: "LM_pend: event: 0x%x, currEvents: 0x%x, andMask: 0x%x, orMask: 0x%x, timeout: %d"
    };
        mask: Diags.USER1 | Diags.USER2,
        msg: "LM_post: event: 0x%x, currEvents: 0x%x, eventId: 0x%x"
    };
 
per-instance config parameters
    var params = new Event.Params// Instance config-params object;
per-instance creation
    var inst = Event.create// Create an instance-object(params);
 
 
const Event.Id_00

Pre-defined Event Ids

Configuration settings
const Event.Id_00 = 0x1;
 
DETAILS
Event_Ids are provided to simplify the specification of andMasks and orMasks arguments to Event_pend().
Since each Event_Id is a bitmask composed of only a single bit, a group of Event_Ids within an andMask or orMask can be indicated by simply adding them together. For instance, to indicate that a task is to be awakened only when both Event_Id_00 and Event_Id_01 have been posted, the andMask for Event_pend() would be constructed as below:
  Event_pend(event, Event_Id_00+EventId_01, Event_Id_NONE,
             BIOS_WAIT_FOREVER);
As shown above, Event_Id_NONE is to be used as an empty (NULL) andMask or orMask.
NOTE
For targets where a UInt is 32 bits in length, Event_Id_00 thru Event_Id_31 can be used.
For targets where a UInt is 16 bits in length, Event_Id_00 thru Event_Id_15 can be used.
C SYNOPSIS
 
const Event.Id_01
Configuration settings
const Event.Id_01 = 0x2;
 
SEE
C SYNOPSIS
 
const Event.Id_02
Configuration settings
const Event.Id_02 = 0x4;
 
SEE
C SYNOPSIS
 
const Event.Id_03
Configuration settings
const Event.Id_03 = 0x8;
 
SEE
C SYNOPSIS
 
const Event.Id_04
Configuration settings
const Event.Id_04 = 0x10;
 
SEE
C SYNOPSIS
 
const Event.Id_05
Configuration settings
const Event.Id_05 = 0x20;
 
SEE
C SYNOPSIS
 
const Event.Id_06
Configuration settings
const Event.Id_06 = 0x40;
 
SEE
C SYNOPSIS
 
const Event.Id_07
Configuration settings
const Event.Id_07 = 0x80;
 
SEE
C SYNOPSIS
 
const Event.Id_08
Configuration settings
const Event.Id_08 = 0x100;
 
SEE
C SYNOPSIS
 
const Event.Id_09
Configuration settings
const Event.Id_09 = 0x200;
 
SEE
C SYNOPSIS
 
const Event.Id_10
Configuration settings
const Event.Id_10 = 0x400;
 
SEE
C SYNOPSIS
 
const Event.Id_11
Configuration settings
const Event.Id_11 = 0x800;
 
SEE
C SYNOPSIS
 
const Event.Id_12
Configuration settings
const Event.Id_12 = 0x1000;
 
SEE
C SYNOPSIS
 
const Event.Id_13
Configuration settings
const Event.Id_13 = 0x2000;
 
SEE
C SYNOPSIS
 
const Event.Id_14
Configuration settings
const Event.Id_14 = 0x4000;
 
SEE
C SYNOPSIS
 
const Event.Id_15
Configuration settings
const Event.Id_15 = 0x8000;
 
SEE
C SYNOPSIS
 
const Event.Id_16
Configuration settings
const Event.Id_16 = 0x10000;
 
SEE
C SYNOPSIS
 
const Event.Id_17
Configuration settings
const Event.Id_17 = 0x20000;
 
SEE
C SYNOPSIS
 
const Event.Id_18
Configuration settings
const Event.Id_18 = 0x40000;
 
SEE
C SYNOPSIS
 
const Event.Id_19
Configuration settings
const Event.Id_19 = 0x80000;
 
SEE
C SYNOPSIS
 
const Event.Id_20
Configuration settings
const Event.Id_20 = 0x100000;
 
SEE
C SYNOPSIS
 
const Event.Id_21
Configuration settings
const Event.Id_21 = 0x200000;
 
SEE
C SYNOPSIS
 
const Event.Id_22
Configuration settings
const Event.Id_22 = 0x400000;
 
SEE
C SYNOPSIS
 
const Event.Id_23
Configuration settings
const Event.Id_23 = 0x800000;
 
SEE
C SYNOPSIS
 
const Event.Id_24
Configuration settings
const Event.Id_24 = 0x1000000;
 
SEE
C SYNOPSIS
 
const Event.Id_25
Configuration settings
const Event.Id_25 = 0x2000000;
 
SEE
C SYNOPSIS
 
const Event.Id_26
Configuration settings
const Event.Id_26 = 0x4000000;
 
SEE
C SYNOPSIS
 
const Event.Id_27
Configuration settings
const Event.Id_27 = 0x8000000;
 
SEE
C SYNOPSIS
 
const Event.Id_28
Configuration settings
const Event.Id_28 = 0x10000000;
 
SEE
C SYNOPSIS
 
const Event.Id_29
Configuration settings
const Event.Id_29 = 0x20000000;
 
SEE
C SYNOPSIS
 
const Event.Id_30
Configuration settings
const Event.Id_30 = 0x40000000;
 
SEE
C SYNOPSIS
 
const Event.Id_31
Configuration settings
const Event.Id_31 = 0x80000000;
 
SEE
C SYNOPSIS
 
const Event.Id_NONE
Configuration settings
const Event.Id_NONE = 0;
 
SEE
C SYNOPSIS
 
config Event.A_badContext  // module-wide

Asserted when pend is called with non-zero timeout from other than a Task context

Configuration settings
Event.A_badContext = Assert.Desc {
    msg: "A_badContext: bad calling context. Must be called from a Task."
};
 
C SYNOPSIS
 
config Event.A_eventInUse  // module-wide

Asserted when pend is called by multiple tasks on the same Event object

Configuration settings
Event.A_eventInUse = Assert.Desc {
    msg: "A_eventInUse: Event object already in use."
};
 
C SYNOPSIS
 
config Event.A_nullEventId  // module-wide

Asserted when post is called with eventId == 0

Configuration settings
Event.A_nullEventId = Assert.Desc {
    msg: "A_nullEventId: posted eventId is null."
};
 
C SYNOPSIS
 
config Event.A_nullEventMasks  // module-wide

Asserted when pend is called with andMask and orMask == 0

Configuration settings
Event.A_nullEventMasks = Assert.Desc {
    msg: "A_nullEventMasks: orMask and andMask are null."
};
 
C SYNOPSIS
 
config Event.A_pendTaskDisabled  // module-wide

Asserted in Event_pend()

Configuration settings
Event.A_pendTaskDisabled = Assert.Desc {
    msg: "A_pendTaskDisabled: Cannot call Event_pend() while the Task or Swi scheduler is disabled."
};
 
DETAILS
Assert raised if Event_pend() is called with the Task or Swi scheduler disabled.
C SYNOPSIS
 
config Event.LM_pend  // module-wide

Logged on calls to Event_pend()

Configuration settings
Event.LM_pend = Log.EventDesc {
    mask: Diags.USER1 | Diags.USER2,
    msg: "LM_pend: event: 0x%x, currEvents: 0x%x, andMask: 0x%x, orMask: 0x%x, timeout: %d"
};
 
C SYNOPSIS
 
config Event.LM_post  // module-wide

Logged on calls to Event_post()

Configuration settings
Event.LM_post = Log.EventDesc {
    mask: Diags.USER1 | Diags.USER2,
    msg: "LM_post: event: 0x%x, currEvents: 0x%x, eventId: 0x%x"
};
 
C SYNOPSIS
 
metaonly config Event.common$  // module-wide

Common module configuration parameters

Configuration settings
Event.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
Instance Config Parameters

Configuration settings
var params = new Event.Params;
// Instance config-params object
Static Instance Creation

Configuration settings
var params = new Event.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = Event.create(params);
// Create an instance-object
ARGUMENTS
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
This function creates a new Event object.
generated on Tue, 13 Oct 2015 04:13:15 GMT