#include <driverlib/vims.h>
Go to the source code of this file.
Functions | |
void | VIMSConfigure (uint32_t ui32Base, bool bRoundRobin, bool bPrefetch) |
Configures the VIMS. More... | |
void | VIMSModeSet (uint32_t ui32Base, uint32_t ui32Mode) |
Set the operational mode of the VIMS. More... | |
uint32_t | VIMSModeGet (uint32_t ui32Base) |
Get the current operational mode of the VIMS. More... | |
void | VIMSModeSafeSet (uint32_t ui32Base, uint32_t ui32NewMode, bool blocking) |
Set the operational mode of the VIMS in a safe sequence. More... | |