#include <driverlib/timer.h>
Go to the source code of this file.
Functions | |
static uint32_t | TimerIntNumberGet (uint32_t ui32Base) |
Gets the timer interrupt number. More... | |
void | TimerConfigure (uint32_t ui32Base, uint32_t ui32Config) |
Configures the timer(s) More... | |
void | TimerLevelControl (uint32_t ui32Base, uint32_t ui32Timer, bool bInvert) |
Controls the output level. More... | |
void | TimerStallControl (uint32_t ui32Base, uint32_t ui32Timer, bool bStall) |
Controls the stall handling. More... | |
void | TimerWaitOnTriggerControl (uint32_t ui32Base, uint32_t ui32Timer, bool bWait) |
Controls the wait on trigger handling. More... | |
void | TimerIntRegister (uint32_t ui32Base, uint32_t ui32Timer, void(*pfnHandler)(void)) |
Registers an interrupt handler for the timer interrupt. More... | |
void | TimerIntUnregister (uint32_t ui32Base, uint32_t ui32Timer) |
Unregisters an interrupt handler for the timer interrupt. More... | |
void | TimerMatchUpdateMode (uint32_t ui32Base, uint32_t ui32Timer, uint32_t ui32Mode) |
Sets the Match Register Update mode. More... | |
void | TimerIntervalLoadMode (uint32_t ui32Base, uint32_t ui32Timer, uint32_t ui32Mode) |
Sets the Interval Load mode. More... | |
|
static |
Gets the timer interrupt number.
Given a timer base address, this function returns the corresponding interrupt number.
ui32Base | is the base address of the timer module. |
ui32Base
is invalid. Definition at line 79 of file timer.c.
Referenced by TimerIntRegister(), and TimerIntUnregister().