Go to the source code of this file.
Functions | |
uint32_t | FlashsafeSizeGet (void) |
Get the size of the flash. More... | |
uint32_t | FlashsafeSectorSizeGet (void) |
Get size of a flash sector in no of bytes. More... | |
uint32_t | FlashsafePowerModeSet (uint32_t ui32PowerMode, uint32_t ui32BankGracePeriode, uint32_t ui32PumpGracePeriode) |
Set power mode. More... | |
uint32_t | FlashsafePowerModeGet (void) |
Get current configured power mode. More... | |
uint32_t | FlashsafeProtectionSet (uint32_t ui32SectorAddress, uint32_t ui32ProtectMode) |
Set sector protection. More... | |
uint32_t | FlashsafeProtectionGet (uint32_t ui32SectorAddress) |
Get sector protection. More... | |
uint32_t | FlashsafeProtectionSave (uint32_t ui32SectorAddress) |
Save sector protection to make it permanent. More... | |
uint32_t | FlashsafeCheckFsmForError (void) |
Checks if the Flashsafe state machine has detected an error. More... | |
uint32_t | FlashsafeCheckFsmForReady (void) |
Checks if the Flash state machine is ready. More... | |
uint32_t | FlashsafeIntRegister (void(*pfnHandler)(void)) |
Registers an interrupt handler for the flash interrupt. More... | |
uint32_t | FlashsafeIntUnregister (void) |
Unregisters the interrupt handler for the flash interrupt. More... | |
uint32_t | FlashsafeIntEnable (uint32_t ui32IntFlags) |
Enables flash controller interrupt sources. More... | |
uint32_t | FlashsafeIntDisable (uint32_t ui32IntFlags) |
Disables individual flash controller interrupt sources. More... | |
uint32_t | FlashsafeIntStatus (void) |
Gets the current interrupt status. More... | |
uint32_t | FlashsafeIntClear (uint32_t ui32IntFlags) |
Clears flash controller interrupt source. More... | |
uint32_t | FlashsafeSectorErase (uint32_t ui32SectorAddress) |
Erase a flash sector. More... | |
uint32_t | FlashsafeProgram (uint8_t *pui8DataBuffer, uint32_t ui32Address, uint32_t ui32Count) |
Programs unprotected main bank flash sectors. More... | |
uint32_t | FlashsafeDisableSectorsForWrite (void) |
Disables all sectors for erase and programming on the active bank. More... | |