SSI0

Instance: SSI0
Component: SSI
Base address: 0x40000000


Synchronous Serial Interface with master and slave capabilities

TOP:SSI0 Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

CR0

RW

32

0x0000 0000

0x0000 0000

0x4000 0000

CR1

RW

32

0x0000 0000

0x0000 0004

0x4000 0004

DR

RW

32

0x0000 XXXX

0x0000 0008

0x4000 0008

SR

RO

32

0x0000 0003

0x0000 000C

0x4000 000C

CPSR

RW

32

0x0000 0000

0x0000 0010

0x4000 0010

IMSC

RW

32

0x0000 0000

0x0000 0014

0x4000 0014

RIS

RO

32

0x0000 0008

0x0000 0018

0x4000 0018

MIS

RO

32

0x0000 0000

0x0000 001C

0x4000 001C

ICR

WO

32

0x0000 0000

0x0000 0020

0x4000 0020

DMACR

RW

32

0x0000 0000

0x0000 0024

0x4000 0024

TOP:SSI0 Register Descriptions

TOP:SSI0:CR0

Address Offset 0x0000 0000
Physical Address 0x4000 0000 Instance 0x4000 0000
Description Control 0
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:8 SCR Serial clock rate:
This is used to generate the transmit and receive bit rate of the SSI. The bit rate is
(SSI's clock frequency)/((SCR+1)*CPSR.CPSDVSR).
SCR is a value from 0-255.
RW 0x00
7 SPH CLKOUT phase (Motorola SPI frame format only)
This bit selects the clock edge that captures data and enables it to change state. It
has the most impact on the first bit transmitted by either permitting or not permitting a clock transition before the first data capture edge.
Value ENUM Name Description
0x0 1ST_CLK_EDGE Data is captured on the first clock edge transition.
0x1 2ND_CLK_EDGE Data is captured on the second clock edge transition.
RW 0
6 SPO CLKOUT polarity (Motorola SPI frame format only)
Value ENUM Name Description
0x0 LOW SSI produces a steady state LOW value on the
CLKOUT pin when data is not being transferred.
0x1 HIGH SSI produces a steady state HIGH value on the CLKOUT pin when data is not being transferred.
RW 0
5:4 FRF Frame format.
The supported frame formats are Motorola SPI, TI synchronous serial and National Microwire.
Value 0'b11 is reserved and shall not be used.
Value ENUM Name Description
0x0 MOTOROLA_SPI Motorola SPI frame format
0x1 TI_SYNC_SERIAL TI synchronous serial frame format
0x2 NATIONAL_MICROWIRE National Microwire frame format
RW 0b00
3:0 DSS Data Size Select.
Values 0b0000, 0b0001, 0b0010 and 0b0011 are reserved and shall not be used.
Value ENUM Name Description
0x3 4_BIT 4-bit data
0x4 5_BIT 5-bit data
0x5 6_BIT 6-bit data
0x6 7_BIT 7-bit data
0x7 8_BIT 8-bit data
0x8 9_BIT 9-bit data
0x9 10_BIT 10-bit data
0xA 11_BIT 11-bit data
0xB 12_BIT 12-bit data
0xC 13_BIT 13-bit data
0xD 14_BIT 14-bit data
0xE 15_BIT 15-bit data
0xF 16_BIT 16-bit data
RW 0x0

TOP:SSI0:CR1

Address Offset 0x0000 0004
Physical Address 0x4000 0004 Instance 0x4000 0004
Description Control 1
Type RW
Bits Field Name Description Type Reset
31:4 RESERVED Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x000 0000
3 SOD Slave-mode output disabled
This bit is relevant only in the slave mode, MS=1. In multiple-slave systems, it is possible for an SSI master to broadcast a message to all slaves in the system while ensuring that only one slave drives data onto its serial output line. In such systems the RXD lines from multiple slaves could be tied together. To operate in such systems, this bitfield can be set if the SSI slave is not supposed to drive the TXD line:

0: SSI can drive the TXD output in slave mode.
1: SSI cannot drive the TXD output in slave mode.
RW 0
2 MS Master or slave mode select. This bit can be modified only when SSI is disabled, SSE=0.
Value ENUM Name Description
0x0 MASTER Device configured as master
0x1 SLAVE Device configured as slave
RW 0
1 SSE Synchronous serial interface enable.
Value ENUM Name Description
0x0 SSI_DISABLED Operation disabled
0x1 SSI_ENABLED Operation enabled
RW 0
0 LBM Loop back mode:

0: Normal serial port operation enabled.
1: Output of transmit serial shifter is connected to input of receive serial shifter internally.
RW 0

TOP:SSI0:DR

Address Offset 0x0000 0008
Physical Address 0x4000 0008 Instance 0x4000 0008
Description Data
16-bits wide data register:
When read, the entry in the receive FIFO, pointed to by the current FIFO read pointer, is accessed. As data values are removed by the receive logic from the incoming data frame, they are placed into the entry in the receive FIFO, pointed to by the current FIFO write pointer.
When written, the entry in the transmit FIFO, pointed to by the write pointer, is written to. Data values are removed from the transmit FIFO one value at a time by the transmit logic. It is loaded into the transmit serial shifter, then serially shifted out onto the TXD output pin at the programmed bit rate.
When a data size of less than 16 bits is selected, the user must right-justify data written to the transmit FIFO. The transmit logic ignores the unused bits. Received data less than 16 bits is automatically right-justified in the receive buffer.
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 DATA Transmit/receive data
The values read from this field or written to this field must be right-justified when SSI is programmed for a data size that is less than 16 bits (CR0.DSS != 0b1111). Unused bits at the top are ignored by transmit logic. The receive logic automatically right-justifies.
RW 0xXXXX

TOP:SSI0:SR

Address Offset 0x0000 000C
Physical Address 0x4000 000C Instance 0x4000 000C
Description Status
Type RO
Bits Field Name Description Type Reset
31:5 RESERVED Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000
4 BSY Serial interface busy:

0: SSI is idle
1: SSI is currently transmitting and/or receiving a frame or the transmit FIFO is not empty.
RO 0
3 RFF Receive FIFO full:

0: Receive FIFO is not full.
1: Receive FIFO is full.
RO 0
2 RNE Receive FIFO not empty

0: Receive FIFO is empty.
1: Receive FIFO is not empty.
RO 0
1 TNF Transmit FIFO not full:

0: Transmit FIFO is full.
1: Transmit FIFO is not full.
RO 1
0 TFE Transmit FIFO empty:

0: Transmit FIFO is not empty.
1: Transmit FIFO is empty.
RO 1

TOP:SSI0:CPSR

Address Offset 0x0000 0010
Physical Address 0x4000 0010 Instance 0x4000 0010
Description Clock Prescale
Type RW
Bits Field Name Description Type Reset
31:8 RESERVED Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x00 0000
7:0 CPSDVSR Clock prescale divisor:
This field specifies the division factor by which the input system clock to SSI must be internally divided before further use.
The value programmed into this field must be an even non-zero number (2-254). The least significant bit of the programmed number is hard-coded to zero. If an odd number is written to this register, data read back from
this register has the least significant bit as zero.
RW 0x00

TOP:SSI0:IMSC

Address Offset 0x0000 0014
Physical Address 0x4000 0014 Instance 0x4000 0014
Description Interrupt Mask Set and Clear
Type RW
Bits Field Name Description Type Reset
31:4 RESERVED Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x000 0000
3 TXIM Transmit FIFO interrupt mask:
A read returns the current mask for transmit FIFO interrupt. On a write of 1, the mask for transmit FIFO interrupt is set which means the interrupt state will be reflected in MIS.TXMIS. A write of 0 clears the mask which means MIS.TXMIS will not reflect the interrupt.
RW 0
2 RXIM Receive FIFO interrupt mask:
A read returns the current mask for receive FIFO interrupt. On a write of 1, the mask for receive FIFO interrupt is set which means the interrupt state will be reflected in MIS.RXMIS. A write of 0 clears the mask which means MIS.RXMIS will not reflect the interrupt.
RW 0
1 RTIM Receive timeout interrupt mask:
A read returns the current mask for receive timeout interrupt. On a write of 1, the mask for receive timeout interrupt is set which means the interrupt state will be reflected in MIS.RTMIS. A write of 0 clears the mask which means MIS.RTMIS will not reflect the interrupt.
RW 0
0 RORIM Receive overrun interrupt mask:
A read returns the current mask for receive overrun interrupt. On a write of 1, the mask for receive overrun interrupt is set which means the interrupt state will be reflected in MIS.RORMIS. A write of 0 clears the mask which means MIS.RORMIS will not reflect the interrupt.
RW 0

TOP:SSI0:RIS

Address Offset 0x0000 0018
Physical Address 0x4000 0018 Instance 0x4000 0018
Description Raw Interrupt Status
Type RO
Bits Field Name Description Type Reset
31:4 RESERVED Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x000 0000
3 TXRIS Raw transmit FIFO interrupt status:
The transmit interrupt is asserted when there are four or fewer valid entries in the transmit FIFO. The transmit interrupt is not qualified with the SSI enable signal. Therefore one of the following ways can be used:
- data can be written to the transmit FIFO prior to enabling the SSI and the
interrupts.
- SSI and interrupts can be enabled so that data can be written to the transmit FIFO by an interrupt service routine.
RO 1
2 RXRIS Raw interrupt state of receive FIFO interrupt:
The receive interrupt is asserted when there are four or more valid entries in the receive FIFO.
RO 0
1 RTRIS Raw interrupt state of receive timeout interrupt:
The receive timeout interrupt is asserted when the receive FIFO is not empty and SSI has remained idle for a fixed 32 bit period. This mechanism can be used to notify the user that data is still present in the receive FIFO and requires servicing. This interrupt is deasserted if the receive FIFO becomes empty by subsequent reads, or if new data is received on RXD.
It can also be cleared by writing to ICR.RTIC.
RO 0
0 RORRIS Raw interrupt state of receive overrun interrupt:
The receive overrun interrupt is asserted when the FIFO is already full and an additional data frame is received, causing an overrun of the FIFO. Data is over-written in the
receive shift register, but not the FIFO so the FIFO contents stay valid.
It can also be cleared by writing to ICR.RORIC.
RO 0

TOP:SSI0:MIS

Address Offset 0x0000 001C
Physical Address 0x4000 001C Instance 0x4000 001C
Description Masked Interrupt Status
Type RO
Bits Field Name Description Type Reset
31:4 RESERVED Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x000 0000
3 TXMIS Masked interrupt state of transmit FIFO interrupt:
This field returns the masked interrupt state of transmit FIFO interrupt which is the AND product of raw interrupt state RIS.TXRIS and the mask setting IMSC.TXIM.
RO 0
2 RXMIS Masked interrupt state of receive FIFO interrupt:
This field returns the masked interrupt state of receive FIFO interrupt which is the AND product of raw interrupt state RIS.RXRIS and the mask setting IMSC.RXIM.
RO 0
1 RTMIS Masked interrupt state of receive timeout interrupt:
This field returns the masked interrupt state of receive timeout interrupt which is the AND product of raw interrupt state RIS.RTRIS and the mask setting IMSC.RTIM.
RO 0
0 RORMIS Masked interrupt state of receive overrun interrupt:
This field returns the masked interrupt state of receive overrun interrupt which is the AND product of raw interrupt state RIS.RORRIS and the mask setting IMSC.RORIM.
RO 0

TOP:SSI0:ICR

Address Offset 0x0000 0020
Physical Address 0x4000 0020 Instance 0x4000 0020
Description Interrupt Clear
On a write of 1, the corresponding interrupt is cleared. A write of 0 has no effect.
Type WO
Bits Field Name Description Type Reset
31:2 RESERVED Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. WO 0b00 0000 0000 0000 0000 0000 0000 0000
1 RTIC Clear the receive timeout interrupt:
Writing 1 to this field clears the timeout interrupt (RIS.RTRIS). Writing 0 has no effect.
WO 0
0 RORIC Clear the receive overrun interrupt:
Writing 1 to this field clears the overrun error interrupt (RIS.RORRIS). Writing 0 has no effect.
WO 0

TOP:SSI0:DMACR

Address Offset 0x0000 0024
Physical Address 0x4000 0024 Instance 0x4000 0024
Description DMA Control
Type RW
Bits Field Name Description Type Reset
31:2 RESERVED Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000 0000 0000 0000
1 TXDMAE Transmit DMA enable. If this bit is set to 1, DMA for the transmit FIFO is enabled. RW 0
0 RXDMAE Receive DMA enable. If this bit is set to 1, DMA for the receive FIFO is enabled. RW 0