AUX_TDCIF

Instance: AUX_TDCIF
Component: AUX_TDC
Base address: 0x400C4000


AUX Time To Digital Converter

TOP:AUX_TDCIF Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

CTL

RW

32

0x0000 0000

0x0000 0000

0x400C 4000

STAT

RO

32

0b0000 0000 0000 000X XXXX XXX0 0000 0110

0x0000 0004

0x400C 4004

RESULT

RO

32

0x0000 0002

0x0000 0008

0x400C 4008

SATCFG

RW

32

0x0000 000F

0x0000 000C

0x400C 400C

TRIGSRC

RW

32

0x0000 0000

0x0000 0010

0x400C 4010

TRIGCNT

RW

32

0x0000 0000

0x0000 0014

0x400C 4014

TRIGCNTLOAD

RW

32

0x0000 0000

0x0000 0018

0x400C 4018

TRIGCNTCFG

RW

32

0x0000 0000

0x0000 001C

0x400C 401C

PRECTL

RW

32

0x0000 001F

0x0000 0020

0x400C 4020

PRECNT

RW

32

0x0000 0000

0x0000 0024

0x400C 4024

TOP:AUX_TDCIF Register Descriptions

TOP:AUX_TDCIF:CTL

Address Offset 0x0000 0000
Physical Address 0x400C 4000 Instance 0x400C 4000
Description Control
Type RW
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000 0000 0000 0000
1:0 CMD TDC command strobes
Value ENUM Name Description
0x0 CLR_RESULT This command clears STAT.SAT, STAT.DONE and results. Note: This is not needed as prerequisite for a measurement. Reliable clear is only guaranteed from IDLE state
0x1 RUN_SYNC_START This command makes the TDC FSM start counting synchronously to the first rising edge that follows a required falling edge of the start event. This guarantees an edge triggered start and is recommended for frequency measurements. A falling edge of the start event may be missed if the command is issued close to it in time, but the TDC will catch later falling edges and guarantee that a measurement starts synchronously to the rising edge of the start event
0x2 RUN This command makes the TDC FSM start and stop counting asynchronously. TDC measurement may start immediately if start is high and hence it may not give precise edge to edge measurements. Only recommended when start pulse is guaranteed to arrive at least 7 clock periods after the command
0x3 ABORT This command forces the TDC back to IDLE state
WO 0b00

TOP:AUX_TDCIF:STAT

Address Offset 0x0000 0004
Physical Address 0x400C 4004 Instance 0x400C 4004
Description Status
Type RO
Bits Field Name Description Type Reset
31:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0000 0000 0000 000X XXXX XXX0
7 SAT Saturation flag for TDC measurement

0: Conversion has not saturated
1: Conversion stopped due to saturation

This field is cleared when starting new measurement or setting CTL.CMD to CLR_RESULT
RO 0
6 DONE Measurement complete flag

0: Measurement not yet complete
1: Measurement complete

This field is cleared when starting new measurement or setting CTL.CMD to CLR_RESULT
RO 0
5:0 STATE TDC internal state machine status
Value ENUM Name Description
0x0 WAIT_START Current state is TDC_STATE_WAIT_START
0x4 WAIT_START_STOP_CNT_EN Current state is TDC_STATE_WAIT_STARTSTOPCNTEN
0x6 IDLE Current state is TDC_STATE_IDLE
0x7 CLR_CNT Current state is TDC_STATE_CLRCNT
0x8 WAIT_STOP Current state is TDC_STATE_WAIT_STOP
0xC WAIT_STOP_CNTDWN Current state is TDC_STATE_WAIT_STOPCNTDOWN
0xE GET_RESULT Current state is TDC_STATE_GETRESULTS
0xF POR Current state is TDC_STATE_POR
0x16 WAIT_CLR_CNT_DONE Current state is TDC_STATE_WAIT_CLRCNT_DONE
0x1E START_FALL Current state is TDC_WAIT_STARTFALL
0x2E FORCE_STOP Current state is TDC_FORCESTOP
RO 0b00 0110

TOP:AUX_TDCIF:RESULT

Address Offset 0x0000 0008
Physical Address 0x400C 4008 Instance 0x400C 4008
Description Result

Result of last TDC conversion
Type RO
Bits Field Name Description Type Reset
31:25 RESERVED25 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
24:0 VALUE Result of the TDC conversion. The result is in clock edges of the clock selected in DDI_0_OSC:CTL0.ACLK_TDC_SRC_SEL. Both rising and falling edges are counted.

When saturating the result is slightly higher than the saturation limit, since it takes a non-zero time to stop the measurement. The highest saturation limit is 24 bits (see SATCFG.LIMIT) so maximum value of VALUE is hence slightly above 2^24.
RO 0b0 0000 0000 0000 0000 0000 0010

TOP:AUX_TDCIF:SATCFG

Address Offset 0x0000 000C
Physical Address 0x400C 400C Instance 0x400C 400C
Description Saturation Configuration
Type RW
Bits Field Name Description Type Reset
31:4 RESERVED4 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x000 0000
3:0 LIMIT Select when the TDC times out. Values not enumerated are not supported
Value ENUM Name Description
0x3 R12 Result bit 12 : TDC saturates and stops when RESULT.VALUE[12] is set. The flag STAT.SAT is set when the timer saturates.
0x4 R13 Result bit 13 : TDC saturates and stops when RESULT.VALUE[13] is set. The flag STAT.SAT is set when the timer saturates.
0x5 R14 Result bit 14 : TDC saturates and stops when RESULT.VALUE[14] is set. The flag STAT.SAT is set when the timer saturates.
0x6 R15 Result bit 15 : TDC saturates and stops when RESULT.VALUE[15] is set. The flag STAT.SAT is set when the timer saturates.
0x7 R16 Result bit 16 : TDC saturates and stops when RESULT.VALUE[16] is set. The flag STAT.SAT is set when the timer saturates.
0x8 R17 Result bit 17 : TDC saturates and stops when RESULT.VALUE[17] is set. The flag STAT.SAT is set when the timer saturates.
0x9 R18 Result bit 18 : TDC saturates and stops when RESULT.VALUE[18] is set. The flag STAT.SAT is set when the timer saturates.
0xA R19 Result bit 19 : TDC saturates and stops when RESULT.VALUE[19] is set. The flag STAT.SAT is set when the timer saturates.
0xB R20 Result bit 20 : TDC saturates and stops when RESULT.VALUE[20] is set. The flag STAT.SAT is set when the timer saturates.
0xC R21 Result bit 21 : TDC saturates and stops when RESULT.VALUE[21] is set. The flag STAT.SAT is set when the timer saturates.
0xD R22 Result bit 22 : TDC saturates and stops when RESULT.VALUE[22] is set. The flag STAT.SAT is set when the timer saturates.
0xE R23 Result bit 23 : TDC saturates and stops when RESULT.VALUE[23] is set. The flag STAT.SAT is set when the timer saturates.
0xF R24 Result bit 24 : TDC saturates and stops when RESULT.VALUE[24] is set. The flag STAT.SAT is set when the timer saturates.
RW 0xF

TOP:AUX_TDCIF:TRIGSRC

Address Offset 0x0000 0010
Physical Address 0x400C 4010 Instance 0x400C 4010
Description Trigger Source

TDC start/stop trigger source selection
Type RW
Bits Field Name Description Type Reset
31:14 RESERVED14 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000
13 STOP_POL Polarity of stop signal. Note! Must not be changed if STAT.STATE is not IDLE
Value ENUM Name Description
0x0 HIGH TDC stops when high level is detected
0x1 LOW TDC stops when low level is detected
RW 0
12:8 STOP_SRC Selects the asynchronous stop signal Note! Must not be changed if STAT.STATE is not IDLE
Value ENUM Name Description
0x0 AON_RTC_CH2 Selects AON_RTC_CH2
0x1 AUX_COMPA Selects AUX_COMPA
0x2 AUX_COMPB Selects AUX_COMPB
0x3 ISRC_RESET Selects ISRC_RESET
0x4 TIMER0_EV Selects TIMER0_EV
0x5 TIMER1_EV Selects TIMER1_EV
0x6 SMPH_AUTOTAKE_DONE Selects SMPH_AUTOTAKE_DONE
0x7 ADC_DONE Selects ADC_DONE
0x8 ADC_FIFO_ALMOST_FULL Selects ADC_FIFO_ALMOST_FULL
0x9 OBSMUX0 Selects OBSMUX0
0xA OBSMUX1 Selects OBSMUX1
0xB AON_SW Selects AON_SW
0xC AON_PROG_WU Selects AON_PROG_WU
0xD AUXIO0 Selects AUXIO0
0xE AUXIO1 Selects AUXIO1
0xF AUXIO2 Selects AUXIO2
0x10 AUXIO3 Selects AUXIO3
0x11 AUXIO4 Selects AUXIO4
0x12 AUXIO5 Selects AUXIO5
0x13 AUXIO6 Selects AUXIO6
0x14 AUXIO7 Selects AUXIO7
0x15 AUXIO8 Selects AUXIO8
0x16 AUXIO9 Selects AUXIO9
0x17 AUXIO10 Selects AUXIO10
0x18 AUXIO11 Selects AUXIO11
0x19 AUXIO12 Selects AUXIO12
0x1A AUXIO13 Selects AUXIO13
0x1B AUXIO14 Selects AUXIO14
0x1C AUXIO15 Selects AUXIO15
0x1D ACLK_REF Selects ACLK_REF
0x1E MCU_EV Selects MCU_EV
0x1F TDC_PRE Selects TDC_PRE
RW 0b0 0000
7:6 RESERVED6 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00
5 START_POL Polarity of start signal. Note! Must not be changed if STAT.STATE is not IDLE
Value ENUM Name Description
0x0 HIGH TDC starts when high level is detected
0x1 LOW TDC starts when low level is detected
RW 0
4:0 START_SRC Selects the asynchronous start signal Note! Must not be changed if STAT.STATE is not IDLE
Value ENUM Name Description
0x0 AON_RTC_CH2 Selects AON_RTC_CH2
0x1 AUX_COMPA Selects AUX_COMPA
0x2 AUX_COMPB Selects AUX_COMPB
0x3 ISRC_RESET Selects ISRC_RESET
0x4 TIMER0_EV Selects TIMER0_EV
0x5 TIMER1_EV Selects TIMER1_EV
0x6 SMPH_AUTOTAKE_DONE Selects SMPH_AUTOTAKE_DONE
0x7 ADC_DONE Selects ADC_DONE
0x8 ADC_FIFO_ALMOST_FULL Selects ADC_FIFO_ALMOST_FULL
0x9 OBSMUX0 Selects OBSMUX0
0xA OBSMUX1 Selects OBSMUX1
0xB AON_SW Selects AON_SW
0xC AON_PROG_WU Selects AON_PROG_WU
0xD AUXIO0 Selects AUXIO0
0xE AUXIO1 Selects AUXIO1
0xF AUXIO2 Selects AUXIO2
0x10 AUXIO3 Selects AUXIO3
0x11 AUXIO4 Selects AUXIO4
0x12 AUXIO5 Selects AUXIO5
0x13 AUXIO6 Selects AUXIO6
0x14 AUXIO7 Selects AUXIO7
0x15 AUXIO8 Selects AUXIO8
0x16 AUXIO9 Selects AUXIO9
0x17 AUXIO10 Selects AUXIO10
0x18 AUXIO11 Selects AUXIO11
0x19 AUXIO12 Selects AUXIO12
0x1A AUXIO13 Selects AUXIO13
0x1B AUXIO14 Selects AUXIO14
0x1C AUXIO15 Selects AUXIO15
0x1D ACLK_REF Selects ACLK_REF
0x1E MCU_EV Selects MCU_EV
0x1F TDC_PRE Selects TDC_PRE
RW 0b0 0000

TOP:AUX_TDCIF:TRIGCNT

Address Offset 0x0000 0014
Physical Address 0x400C 4014 Instance 0x400C 4014
Description Trigger Counter

Stop counter status/control of TDC
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 CNT Remaining number of stop events that will be ignored. Writing to this register updates the value. The CNT will be loaded with the value of TRIGCNTLOAD.CNT at the start of every measurement.

When the stop counter is enabled the first CNT-1 stop events is ignored after which the TDC will stop measurement on event number CNT

Note! Must not be changed if STAT.STATE is not IDLE
RW 0x0000

TOP:AUX_TDCIF:TRIGCNTLOAD

Address Offset 0x0000 0018
Physical Address 0x400C 4018 Instance 0x400C 4018
Description Trigger Counter Load

Stop counter control of TDC
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 CNT Selects the number of stop events that will be ignored by the TDC. This can be used to measure multiple periods of a clock signal. The value written to this field is loaded into the stop counter at the start of each measurement.

Note! Both values 0 and 1 will make the TDC stop on the first event after the start event

Note! Must not be changed if STAT.STATE is not IDLE
RW 0x0000

TOP:AUX_TDCIF:TRIGCNTCFG

Address Offset 0x0000 001C
Physical Address 0x400C 401C Instance 0x400C 401C
Description Trigger Counter Configuration
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 EN Stop counter enable

0: Stop counter is disabled
1: Stop counter is enabled
RW 0

TOP:AUX_TDCIF:PRECTL

Address Offset 0x0000 0020
Physical Address 0x400C 4020 Instance 0x400C 4020
Description Prescaler Control

The prescaler can be used to count events that are faster than the AUX clock speed. It can be used standalone or as a start/stop source for the TDC by configuring TRIGSRC.START_SRC and TRIGSRC.STOP_SRC to TDC_PRE. When counting fast signals with the TDC that are faster than 1/10th of the clock frequency of AUX it is recommended to use the prescaler.
Type RW
Bits Field Name Description Type Reset
31:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x00 0000
7 RESET_N Prescaler reset control

0: Prescaler is held in reset
1: Prescaler is not held in reset
RW 0
6 RATIO Prescaler ratio. This controls how often an event is generated on the TDC_PRE line. After the prescaler is reset the event output TDC_PRE is 0.
Value ENUM Name Description
0x0 DIV16 Prescaler divides by 16. A rising edge on the output is generated for every 16 rising edges of the input (the output toggles on every 8th rising edge of the input).
0x1 DIV64 Prescaler divides by 64. A rising edge on the output is generated for every 64 rising edges of the input (the output toggles on every 32th rising edge of the input). .
RW 0
5 RESERVED5 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0
4:0 SRC Selects event for prescaler to use as input
Note! Only change when prescaler is in reset
Value ENUM Name Description
0x0 AON_RTC_CH2 0
0x1 AUX_COMPA 0
0x2 AUX_COMPB 0
0x3 ISRC_RESET 0
0x4 TIMER0_EV 0
0x5 TIMER1_EV 0
0x6 SMPH_AUTOTAKE_DONE 0
0x7 ADC_DONE 0
0x8 ADC_FIFO_ALMOST_FULL 0
0x9 OBSMUX0 0
0xA OBSMUX1 0
0xB AON_SW 0
0xC AON_PROG_WU 0
0xD AUXIO0 0
0xE AUXIO1 0
0xF AUXIO2 0
0x10 AUXIO3 0
0x11 AUXIO4 0
0x12 AUXIO5 0
0x13 AUXIO6 0
0x14 AUXIO7 0
0x15 AUXIO8 0
0x16 AUXIO9 0
0x17 AUXIO10 0
0x18 AUXIO11 0
0x19 AUXIO12 0
0x1A AUXIO13 0
0x1B AUXIO14 0
0x1C AUXIO15 0
0x1D ACLK_REF 0
0x1E MCU_EV 0
0x1F ADC_IRQ 0
RW 0b1 1111

TOP:AUX_TDCIF:PRECNT

Address Offset 0x0000 0024
Physical Address 0x400C 4024 Instance 0x400C 4024
Description Prescaler Counter

Value of prescaler counter
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 CNT Writing to this register will latch the contents of the 16 bit prescaler counter (The value written is don't care).

Reading will return the latched value.
RW 0x0000