#include <rf_common_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x0808. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips if the rule involves skipping. More... | |
} | condition |
struct { | |
uint8_t bUseCw:1 | |
0: Send modulated signal 1: Send continuous wave More... | |
uint8_t bFsOff:1 | |
0: Keep frequency synth on after command 1: Turn frequency synth off after command More... | |
uint8_t whitenMode:2 | |
0: No whitening 1: Default whitening 2: PRBS-15 3: PRBS-32 More... | |
} | config |
uint8_t | __dummy0 |
uint16_t | txWord |
Value to send to the modem before whitening. More... | |
uint8_t | __dummy1 |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | endTrigger |
Trigger classifier for ending the operation. More... | |
uint32_t | syncWord |
Sync word to use for transmitter. More... | |
ratmr_t | endTime |
Time to end the operation. More... | |
Definition at line 444 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_TEST_s::__dummy0 |
Definition at line 473 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_TEST_s::__dummy1 |
Definition at line 475 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_TEST_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 453 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_TEST_s::bFsOff |
0: Keep frequency synth on after command
1: Turn frequency synth off after command
Definition at line 466 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_TEST_s::bUseCw |
0: Send modulated signal
1: Send continuous wave
Definition at line 464 of file rf_common_cmd.h.
uint16_t rfc_CMD_TX_TEST_s::commandNo |
The command ID number 0x0808.
Definition at line 445 of file rf_common_cmd.h.
struct { ... } rfc_CMD_TX_TEST_s::condition |
struct { ... } rfc_CMD_TX_TEST_s::config |
ratmr_t rfc_CMD_TX_TEST_s::endTime |
Time to end the operation.
Definition at line 485 of file rf_common_cmd.h.
struct { ... } rfc_CMD_TX_TEST_s::endTrigger |
Trigger classifier for ending the operation.
uint8_t rfc_CMD_TX_TEST_s::nSkip |
Number of skips if the rule involves skipping.
Definition at line 461 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_TEST_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 456 of file rf_common_cmd.h.
rfc_radioOp_t* rfc_CMD_TX_TEST_s::pNextOp |
Pointer to the next operation to run after this operation is done.
Definition at line 449 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_TEST_s::rule |
Condition for running next command: Rule for how to proceed.
Definition at line 460 of file rf_common_cmd.h.
ratmr_t rfc_CMD_TX_TEST_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
Definition at line 450 of file rf_common_cmd.h.
struct { ... } rfc_CMD_TX_TEST_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_CMD_TX_TEST_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
Definition at line 446 of file rf_common_cmd.h.
uint32_t rfc_CMD_TX_TEST_s::syncWord |
Sync word to use for transmitter.
Definition at line 484 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_TEST_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 455 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_TEST_s::triggerType |
The type of trigger.
Definition at line 452 of file rf_common_cmd.h.
uint16_t rfc_CMD_TX_TEST_s::txWord |
Value to send to the modem before whitening.
Definition at line 474 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_TEST_s::whitenMode |
0: No whitening
1: Default whitening
2: PRBS-15
3: PRBS-32
Definition at line 468 of file rf_common_cmd.h.