#include <rf_common_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x0809. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips if the rule involves skipping. More... | |
} | condition |
uint16_t | __dummy0 |
ratmr_t | rat0 |
The returned RAT timer value corresponding to the value the RAT would have had when the RTC was zero. More... | |
Definition at line 493 of file rf_common_cmd.h.
uint16_t rfc_CMD_SYNC_STOP_RAT_s::__dummy0 |
Definition at line 512 of file rf_common_cmd.h.
uint8_t rfc_CMD_SYNC_STOP_RAT_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 502 of file rf_common_cmd.h.
uint16_t rfc_CMD_SYNC_STOP_RAT_s::commandNo |
The command ID number 0x0809.
Definition at line 494 of file rf_common_cmd.h.
struct { ... } rfc_CMD_SYNC_STOP_RAT_s::condition |
uint8_t rfc_CMD_SYNC_STOP_RAT_s::nSkip |
Number of skips if the rule involves skipping.
Definition at line 510 of file rf_common_cmd.h.
uint8_t rfc_CMD_SYNC_STOP_RAT_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 505 of file rf_common_cmd.h.
rfc_radioOp_t* rfc_CMD_SYNC_STOP_RAT_s::pNextOp |
Pointer to the next operation to run after this operation is done.
Definition at line 498 of file rf_common_cmd.h.
ratmr_t rfc_CMD_SYNC_STOP_RAT_s::rat0 |
The returned RAT timer value corresponding to the value the RAT would have had when the RTC was zero.
Definition at line 513 of file rf_common_cmd.h.
uint8_t rfc_CMD_SYNC_STOP_RAT_s::rule |
Condition for running next command: Rule for how to proceed.
Definition at line 509 of file rf_common_cmd.h.
ratmr_t rfc_CMD_SYNC_STOP_RAT_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
Definition at line 499 of file rf_common_cmd.h.
struct { ... } rfc_CMD_SYNC_STOP_RAT_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_CMD_SYNC_STOP_RAT_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
Definition at line 495 of file rf_common_cmd.h.
uint8_t rfc_CMD_SYNC_STOP_RAT_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 504 of file rf_common_cmd.h.
uint8_t rfc_CMD_SYNC_STOP_RAT_s::triggerType |
The type of trigger.
Definition at line 501 of file rf_common_cmd.h.