#include <rf_common_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x0006. More... | |
uint16_t | __dummy0 |
dataQueue_t * | pQueue |
Pointer to the queue structure from which the entry will be removed. More... | |
uint8_t * | pEntry |
Pointer to the entry that was removed. More... | |
Definition at line 828 of file rf_common_cmd.h.
uint16_t rfc_CMD_REMOVE_DATA_ENTRY_s::__dummy0 |
Definition at line 830 of file rf_common_cmd.h.
uint16_t rfc_CMD_REMOVE_DATA_ENTRY_s::commandNo |
The command ID number 0x0006.
Definition at line 829 of file rf_common_cmd.h.
uint8_t* rfc_CMD_REMOVE_DATA_ENTRY_s::pEntry |
Pointer to the entry that was removed.
Definition at line 832 of file rf_common_cmd.h.
dataQueue_t* rfc_CMD_REMOVE_DATA_ENTRY_s::pQueue |
Pointer to the queue structure from which the entry will be removed.
Definition at line 831 of file rf_common_cmd.h.