63 #ifndef ti_drivers_watchdog_WatchdogMSP432__include
64 #define ti_drivers_watchdog_WatchdogMSP432__include
uint8_t clockSource
Definition: WatchdogMSP432.h:103
struct WatchdogMSP432_Object WatchdogMSP432_Object
Watchdog Object for MSP432.
uint8_t intPriority
Definition: WatchdogMSP432.h:102
bool isOpen
Definition: WatchdogMSP432.h:115
HwiP_Handle hwiHandle
Definition: WatchdogMSP432.h:114
Watchdog hardware attributes for MSP432 These fields are used by driverlib APIs and therefore must be...
Definition: WatchdogMSP432.h:99
Watchdog driver interface.
uint8_t clockDivider
Definition: WatchdogMSP432.h:104
const Watchdog_FxnTable WatchdogMSP432_fxnTable
Watchdog function table for MSP432.
uint32_t baseAddr
Definition: WatchdogMSP432.h:100
uint8_t intNum
Definition: WatchdogMSP432.h:101
Watchdog_ResetMode resetMode
Definition: WatchdogMSP432.h:113
The definition of a Watchdog function table that contains the required set of functions to control a ...
Definition: Watchdog.h:275
void * HwiP_Handle
Opaque client reference to an instance of a HwiP.
Definition: HwiP.h:66
Watchdog_ResetMode
Watchdog reset mode settings.
Definition: Watchdog.h:197
Hardware Interrupt module for the RTOS Porting Interface.
struct WatchdogMSP432_HWAttrs WatchdogMSP432_HWAttrs
Watchdog hardware attributes for MSP432 These fields are used by driverlib APIs and therefore must be...
Watchdog Object for MSP432.
Definition: WatchdogMSP432.h:112