47 #ifndef ti_drivers_uart_UARTTivaDMA__include
48 #define ti_drivers_uart_UARTTivaDMA__include
58 #include <ti/sysbios/knl/Semaphore.h>
59 #define ti_sysbios_family_arm_m3_Hwi__nolocalnames
60 #include <ti/sysbios/family/arm/m3/Hwi.h>
147 ti_sysbios_family_arm_m3_Hwi_Struct
hwi;
153 #undef ti_sysbios_family_arm_m3_Hwi__nolocalnames
uint32_t txChannelIndex
Definition: UARTTivaDMA.h:114
size_t writeCount
Definition: UARTTivaDMA.h:138
Semaphore_Struct writeSem
Definition: UARTTivaDMA.h:148
struct UARTTivaDMA_Object UARTTivaDMA_Object
UARTTivaDMA Object.
UARTTivaDMA Object.
Definition: UARTTivaDMA.h:122
struct UARTTivaDMA_HWAttrs UARTTivaDMA_HWAttrs
UARTTivaDMA Hardware attributes.
UART_Callback readCallback
Definition: UARTTivaDMA.h:129
Semaphore_Struct readSem
Definition: UARTTivaDMA.h:149
The definition of a UART function table that contains the required set of functions to control a spec...
Definition: UART.h:497
unsigned int baseAddr
Definition: UARTTivaDMA.h:106
bool opened
Definition: UARTTivaDMA.h:124
unsigned int intPriority
Definition: UARTTivaDMA.h:110
UART_Mode
UART mode settings.
Definition: UART.h:291
unsigned int readTimeout
Definition: UARTTivaDMA.h:127
UART_DataMode
UART data mode settings.
Definition: UART.h:339
UART_ReturnMode
UART return mode settings.
Definition: UART.h:324
UART_Mode writeMode
Definition: UARTTivaDMA.h:126
size_t writeSize
Definition: UARTTivaDMA.h:139
UART_Echo
UART echo settings.
Definition: UART.h:357
void * readBuf
Definition: UARTTivaDMA.h:142
UART_DataMode writeDataMode
Definition: UARTTivaDMA.h:133
UARTTivaDMA Hardware attributes.
Definition: UARTTivaDMA.h:104
ti_sysbios_family_arm_m3_Hwi_Struct hwi
Definition: UARTTivaDMA.h:147
unsigned int intNum
Definition: UARTTivaDMA.h:108
UART_Echo readEcho
Definition: UARTTivaDMA.h:134
struct UARTTivaDMA_Object * UARTTivaDMA_Handle
UART_Callback writeCallback
Definition: UARTTivaDMA.h:130
const void * writeBuf
Definition: UARTTivaDMA.h:137
UART_ReturnMode readReturnMode
Definition: UARTTivaDMA.h:131
UART_DataMode readDataMode
Definition: UARTTivaDMA.h:132
void(* UART_Callback)(UART_Handle, void *buf, size_t count)
The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The cal...
Definition: UART.h:284
unsigned int writeTimeout
Definition: UARTTivaDMA.h:128
size_t readCount
Definition: UARTTivaDMA.h:143
uint32_t rxChannelIndex
Definition: UARTTivaDMA.h:112
size_t readSize
Definition: UARTTivaDMA.h:144
const UART_FxnTable UARTTivaDMA_fxnTable
UART_Mode readMode
Definition: UARTTivaDMA.h:125