50 #ifndef ti_drivers_sdspi_SDSPITiva__include
51 #define ti_drivers_sdspi_SDSPITiva__include
60 #include <ti/sysbios/fatfs/ff.h>
61 #include <ti/sysbios/fatfs/diskio.h>
Definition: SDSPITiva.h:82
uint32_t driveNumber
Definition: SDSPITiva.h:161
DSTATUS diskState
Definition: SDSPITiva.h:162
SDSPITiva Object.
Definition: SDSPITiva.h:160
SDSPIBaseAddrType baseAddr
Definition: SDSPITiva.h:132
SDSPITiva Hardware attributes.
Definition: SDSPITiva.h:130
uint32_t portCS
Definition: SDSPITiva.h:150
The definition of a SDSPI function table that contains the required set of functions to control a spe...
Definition: SDSPI.h:222
const SDSPI_FxnTable SDSPITiva_fxnTable
struct SDSPITiva_Object * SDSPITiva_Handle
unsigned long SDSPIBaseAddrType
Definition: SDSPITiva.h:68
SDSPITiva_CardType cardType
Definition: SDSPITiva.h:163
Definition: SDSPITiva.h:79
struct SDSPITiva_Object SDSPITiva_Object
SDSPITiva Object.
uint32_t portMOSI
Definition: SDSPITiva.h:145
FATFS filesystem
Definition: SDSPITiva.h:165
uint32_t portSCK
Definition: SDSPITiva.h:135
struct SDSPITiva_HWAttrs SDSPITiva_HWAttrs
uint32_t pinMOSI
Definition: SDSPITiva.h:147
unsigned long SDSPIDataType
Definition: SDSPITiva.h:69
Definition: SDSPITiva.h:80
Definition: SDSPITiva.h:81
uint32_t portMISO
Definition: SDSPITiva.h:140
SDSPITiva_CardType
SD Card type inserted.
Definition: SDSPITiva.h:78
uint32_t pinCS
Definition: SDSPITiva.h:152
uint32_t pinSCK
Definition: SDSPITiva.h:137
uint32_t pinMISO
Definition: SDSPITiva.h:142
uint32_t bitRate
Definition: SDSPITiva.h:164