50 #ifndef ti_drivers_sdspi_SDSPIEUSCIB__include
51 #define ti_drivers_sdspi_SDSPIEUSCIB__include
66 #include <ti/sysbios/fatfs/ff.h>
67 #include <ti/sysbios/fatfs/diskio.h>
uint32_t pinCS
Definition: SDSPIEUSCIB.h:155
const SDSPI_FxnTable SDSPIEUSCIB_fxnTable
struct SDSPIEUSCIB_Object SDSPIEUSCIB_Object
SDSPIEUSCIB Object.
FATFS filesystem
Definition: SDSPIEUSCIB.h:168
SDSPIEUSCIB Object.
Definition: SDSPIEUSCIB.h:163
uint8_t portMOSI
Definition: SDSPIEUSCIB.h:150
struct SDSPIEUSCIB_HWAttrsV1 SDSPIEUSCIB_HWAttrsV1
uint8_t portCS
Definition: SDSPIEUSCIB.h:154
Definition: SDSPIEUSCIB.h:78
uint8_t portMISO
Definition: SDSPIEUSCIB.h:146
The definition of a SDSPI function table that contains the required set of functions to control a spe...
Definition: SDSPI.h:222
SDSPIEUSCIB_CardType
SD Card type inserted.
Definition: SDSPIEUSCIB.h:75
uint32_t pinMOSI
Definition: SDSPIEUSCIB.h:151
uint8_t pinMISOModeFunction
Definition: SDSPIEUSCIB.h:148
Definition: SDSPIEUSCIB.h:79
uint32_t bitRate
Definition: SDSPIEUSCIB.h:167
uint32_t pinMISO
Definition: SDSPIEUSCIB.h:147
uint32_t baseAddr
Definition: SDSPIEUSCIB.h:139
Definition: SDSPIEUSCIB.h:77
uint8_t pinMOSIModeFunction
Definition: SDSPIEUSCIB.h:152
uint8_t clockSource
Definition: SDSPIEUSCIB.h:140
struct SDSPIEUSCIB_Object * SDSPIEUSCIB_Handle
uint8_t portSCK
Definition: SDSPIEUSCIB.h:142
SDSPIEUSCIB_CardType cardType
Definition: SDSPIEUSCIB.h:166
SDSPIEUSCIB Hardware attributes.
Definition: SDSPIEUSCIB.h:138
uint8_t pinSCKModeFunction
Definition: SDSPIEUSCIB.h:144
uint32_t pinSCK
Definition: SDSPIEUSCIB.h:143
uint16_t driveNumber
Definition: SDSPIEUSCIB.h:164
Definition: SDSPIEUSCIB.h:76
DSTATUS diskState
Definition: SDSPIEUSCIB.h:165