90 #ifndef ti_driver_pwm_PWMTimerMSP432__include
91 #define ti_driver_pwm_PWMTimerMSP432__include
100 #define PWMTimerMSP432_NUM_TIMERS 4
103 #define PWMTimerMSP432_CHANGE_PERIOD PWM_CMD_RESERVED + 0
bool isOpen
Definition: PWMTimerMSP432.h:151
uint8_t cyclesPerMicroSec
Definition: PWMTimerMSP432.h:138
PWMTimerMSP432 Hardware attributes.
Definition: PWMTimerMSP432.h:125
struct PWMTimerMSP432_Object PWMTimerMSP432_Object
PWMTimerMSP432 Object.
PWMTimerMSP432_Status.
Definition: PWMTimerMSP432.h:135
uint8_t dutyMode
Definition: PWMTimerMSP432.h:150
const PWM_FxnTable PWMTimerMSP432_fxnTable
struct PWMTimerMSP432_HWAttrs PWMTimerMSP432_HWAttrs
PWMTimerMSP432 Hardware attributes.
uint8_t pwmCompareOutputBit
Definition: PWMTimerMSP432.h:149
PWMTimerMSP432 Object.
Definition: PWMTimerMSP432.h:147
The definition of a PWM function table that contains the required set of functions to control a speci...
Definition: PWM.h:327
uint16_t period
Definition: PWMTimerMSP432.h:136
uint8_t prescalar
Definition: PWMTimerMSP432.h:137
PWMTimerMSP432_Status * pwmTimerStatus
Definition: PWMTimerMSP432.h:148
uint32_t baseAddr
Definition: PWMTimerMSP432.h:126
uint8_t activeOutputsMask
Definition: PWMTimerMSP432.h:139
struct PWMTimerMSP432_Status PWMTimerMSP432_Status
PWMTimerMSP432_Status.
uint8_t compareRegister
Definition: PWMTimerMSP432.h:127