77 #ifndef ti_driver_pwm_PWMTimerCC3200__include
78 #define ti_driver_pwm_PWMTimerCC3200__include
87 #define PWMTimerCC3200_CHANGE_PERIOD PWM_CMD_RESERVED + 0
struct PWMTimerCC3200_Object PWMTimerCC3200_Object
PWMTimerCC3200 Object.
uint8_t dutyMode
Definition: PWMTimerCC3200.h:128
uint32_t baseAddr
Definition: PWMTimerCC3200.h:116
PWMTimerCC3200 Hardware attributes.
Definition: PWMTimerCC3200.h:115
uint8_t cyclesPerMicroSec
Definition: PWMTimerCC3200.h:129
PWMTimerCC3200 Object.
Definition: PWMTimerCC3200.h:125
uint16_t timer
Definition: PWMTimerCC3200.h:117
The definition of a PWM function table that contains the required set of functions to control a speci...
Definition: PWM.h:327
uint32_t duty
Definition: PWMTimerCC3200.h:127
uint32_t period
Definition: PWMTimerCC3200.h:126
const PWM_FxnTable PWMTimerCC3200_fxnTable
struct PWMTimerCC3200_HWAttrs PWMTimerCC3200_HWAttrs
PWMTimerCC3200 Hardware attributes.