287 #ifndef ti_drivers_i2c_I2CCC26XX__include
288 #define ti_drivers_i2c_I2CCC26XX__include
298 #include <ti/sysbios/family/arm/cc26xx/Power.h>
300 #define ti_sysbios_family_arm_m3_Hwi__nolocalnames
301 #include <ti/sysbios/family/arm/m3/Hwi.h>
302 #include <ti/sysbios/knl/Semaphore.h>
424 ti_sysbios_family_arm_m3_Hwi_Struct
hwi;
451 #undef ti_sysbios_family_arm_m3_Hwi__nolocalnames
Semaphore_Struct transferComplete
Definition: I2CCC26XX.h:426
I2CBaseAddrType baseAddr
Definition: I2CCC26XX.h:386
I2C_CallbackFxn transferCallbackFxn
Definition: I2CCC26XX.h:419
uint8_t pinSDA
Definition: I2CCC26XX.h:334
struct I2CCC26XX_HWAttrs I2CCC26XX_HWAttrs
I2CCC26XX Hardware attributes.
uint8_t * writeBufIdx
Definition: I2CCC26XX.h:434
bool isOpen
Definition: I2CCC26XX.h:447
I2CCC26XX Hardware attributes.
Definition: I2CCC26XX.h:384
Definition: I2CCC26XX.h:346
struct I2CCC26XX_I2CPinCfg I2CCC26XX_I2CPinCfg
I2CCC26XX Pin Configuration.
void(* I2C_CallbackFxn)(I2C_Handle, I2C_Transaction *, bool)
I2C callback function.
Definition: I2C.h:248
uint8_t intPriority
I2C Peripheral's interrupt priority.
Definition: I2CCC26XX.h:404
I2CCC26XX_Mode
I2CCC26XX mode.
Definition: I2CCC26XX.h:344
unsigned long powerMngrId
Definition: I2CCC26XX.h:388
I2CCC26XX Pin Configuration.
Definition: I2CCC26XX.h:333
Definition: I2CCC26XX.h:348
uint32_t bitRate
Definition: I2CCC26XX.h:421
I2C_Transaction * currentTransaction
Definition: I2CCC26XX.h:433
I2C_TransferMode transferMode
Definition: I2CCC26XX.h:418
Definition: I2CCC26XX.h:345
Power_NotifyObj i2cPostObj
Definition: I2CCC26XX.h:445
I2C_TransferMode
I2C transfer mode.
Definition: I2C.h:230
PIN_State pinState
Definition: I2CCC26XX.h:429
The definition of a I2C function table that contains the required set of functions to control a speci...
Definition: I2C.h:328
PIN_Handle hPin
Definition: I2CCC26XX.h:430
Device-specific pin & GPIO driver for CC26xx family [def].
Semaphore_Struct mutex
Definition: I2CCC26XX.h:425
Definition: I2CCC26XX.h:347
struct I2CCC26XX_Object I2CCC26XX_Object
I2CCC26XX Object.
Power notify object structure.
Definition: Power.h:112
uint8_t * readBufIdx
Definition: I2CCC26XX.h:436
const I2C_FxnTable I2CCC26XX_fxnTable
underlying data structure for type PIN_State
Definition: PIN.h:686
int intNum
Definition: I2CCC26XX.h:390
I2C_Transaction * tailPtr
Definition: I2CCC26XX.h:441
I2C_Transaction * headPtr
Definition: I2CCC26XX.h:440
uint8_t pinSCL
Definition: I2CCC26XX.h:335
volatile I2CCC26XX_Mode mode
Definition: I2CCC26XX.h:420
I2CCC26XX Object.
Definition: I2CCC26XX.h:416
unsigned int writeCountIdx
Definition: I2CCC26XX.h:435
ti_sysbios_family_arm_m3_Hwi_Struct hwi
Definition: I2CCC26XX.h:424
I2C transaction.
Definition: I2C.h:210
unsigned long I2CDataType
Definition: I2CCC26XX.h:307
uint8_t sdaPin
Definition: I2CCC26XX.h:406
unsigned long I2CBaseAddrType
Definition: I2CCC26XX.h:305
void * i2cPostFxn
Definition: I2CCC26XX.h:444
uint8_t sclPin
Definition: I2CCC26XX.h:408
unsigned int readCountIdx
Definition: I2CCC26XX.h:437