46 #ifndef ti_drivers_Camera_CameraCC3200DMA__include
47 #define ti_drivers_Camera_CameraCC3200DMA__include
60 #define CameraCC3200DMA_DMA_TRANSFER_SIZE 64
uint32_t intNum
Definition: CameraCC3200DMA.h:100
The definition of a Camera function table that contains the required set of functions to control a sp...
Definition: Camera.h:380
void(* Camera_Callback)(Camera_Handle, void *buf, size_t bufferLength)
The definition of a callback function used by the Camera driver when used in Camera_MODE_CALLBACK.
Definition: Camera.h:187
unsigned long channelIndex
Definition: CameraCC3200DMA.h:104
SemaphoreP_Handle captureSem
Definition: CameraCC3200DMA.h:129
HwiP_Handle hwiHandle
Definition: CameraCC3200DMA.h:130
void * SemaphoreP_Handle
Opaque client reference to an instance of a SemaphoreP.
Definition: SemaphoreP.h:96
Semaphore module for the RTOS Porting Interface.
uint32_t captureTimeout
Definition: CameraCC3200DMA.h:119
bool inUse
Definition: CameraCC3200DMA.h:126
bool opened
Definition: CameraCC3200DMA.h:114
uint32_t baseAddr
Definition: CameraCC3200DMA.h:98
size_t bufferlength
Definition: CameraCC3200DMA.h:121
struct CameraCC3200DMA_Object * CameraCC3200DMA_Handle
CameraCC3200DMA Object.
Definition: CameraCC3200DMA.h:112
const Camera_FxnTable CameraCC3200DMA_fxnTable
void * captureBuf
Definition: CameraCC3200DMA.h:120
Camera_Callback captureCallback
Definition: CameraCC3200DMA.h:118
Camera_CaptureMode
Camera capture mode settings.
Definition: Camera.h:196
bool cameraDMA_PingPongMode
Definition: CameraCC3200DMA.h:124
uint32_t intPriority
Definition: CameraCC3200DMA.h:102
void * HwiP_Handle
Opaque client reference to an instance of a HwiP.
Definition: HwiP.h:66
Camera_CaptureMode operationMode
Definition: CameraCC3200DMA.h:115
size_t frameLength
Definition: CameraCC3200DMA.h:122
struct CameraCC3200DMA_HWAttrs CameraCC3200DMA_HWAttrs
CameraCC3200DMA Hardware attributes.
size_t cameraDMAxIntrRcvd
Definition: CameraCC3200DMA.h:125
Hardware Interrupt module for the RTOS Porting Interface.
struct CameraCC3200DMA_Object CameraCC3200DMA_Object
CameraCC3200DMA Object.
CameraCC3200DMA Hardware attributes.
Definition: CameraCC3200DMA.h:96