Main Page
Data Structures
Files
Data Structures
Data Fields
SOCK6PCB Struct Reference
The structure describes the IPv6 Socket Protocol specific properties.
More...
#include <sockif.h>
Data Fields
IP6N
IPAddrLocal
Local IPv6 Address.
UINT16
PortLocal
Local IP Port.
IP6N
IPAddrForeign
Foreign host's IPv6 Address.
UINT16
PortForeign
Foreign IP Port.
UINT32
State
Socket state (protocol dependent).
Detailed Description
The structure describes the IPv6 Socket Protocol specific properties.
The documentation for this struct was generated from the following file:
inc/stack/inc/sockif.h
Copyright 2009, Texas Instruments Incorporated