![]() |
![]() |
Functions | |
int | RawEthTxPacket (HANDLE hRawEthSock, char *pBuffer, int len) |
int | RawEthTxPacketNC (HANDLE hRawEthSock, char *pBuffer, int len, HANDLE hPkt) |
int | RawEthRxPacket (PBM_Handle hPkt) |
int RawEthRxPacket | ( | PBM_Handle | hPkt | ) |
Description
This routine is the API interface routine which is called by the NIMU layer when the ethernet type doesnt match any of the well know standard ethernet types. This function checks if a raw ethernet socket object exists for the ethernet type in the packet and if so enqueus in the socket buffer for the application to receive.
[in] | hPkt | Handle to the packet which is to be passed up the NDK stack. |
-1 | - Error | |
0 | - Success |
int RawEthTxPacket | ( | HANDLE | hRawEthSock, | |
char * | pBuffer, | |||
int | len | |||
) |
Description
The function is the interface routine which is called to send a packet via a raw ethernet socket object.
[in] | hRawEthSock | Handle to the Raw ethernet socket. |
[in] | pBuffer | Handle to the data buffer that needs to be sent |
[in] | len | length of the data |
0 | - Successfully sent out the packet. ENOBUFS - Error allocating memory for the packet. Packet not sent out. |
int RawEthTxPacketNC | ( | HANDLE | hRawEthSock, | |
char * | pBuffer, | |||
int | len, | |||
HANDLE | hPkt | |||
) |
Description
The function is the interface routine which is called to send a packet without any copy via a raw ethernet socket object.
[in] | hRawEthSock | Handle to the Raw ethernet socket. |
[in] | pBuffer | Handle to the data buffer that needs to be sent |
[in] | len | length of the data |
[in] | hPkt | Handle to the packet that needs to be sent |
0 | - Successfully sent out the packet. EINVAL - Bad Packet / Buffer handles, packet not sent out. |