![]() |
![]() |
Data Structures | |
struct | JUMBO_MEMORYBLOCK |
This structure defines the Jumbo memory block structure. More... | |
struct | JUMBO_PITENTRY |
This structure defines the Page Information entry. More... | |
Functions | |
int | _jumbo_mmInit () |
void * | jumbo_mmAlloc (uint Size) |
void | jumbo_mmFree (void *p) |
void | _jumbo_mmCheck (uint CallMode, int(*pPrn)(const char *,...)) |
void _jumbo_mmCheck | ( | uint | CallMode, | |
int(*)(const char *,...) | pPrn | |||
) |
Description
This function iterates through the PIT table and dumps the current memory usage stats according to the arguments specified.
[in] | CallMode | This argument specifies the type of stats / operation that needs to be performed by this function. The 3 supported call modes are: MMCHECK_MAP : Map out allocated memory, but don't dump ID's MMCHECK_DUMP : Dump allocated block ID's MMCHECK_SHUTDOWN : Dump allocated block's & free |
[in] | pPrn | Callback function pointer to be notified. |
None. |
int _jumbo_mmInit | ( | ) |
Description
This function initializes the jumbo frame memory system.
[in] | None |
Always | returns 1 to indicate success. |
void* jumbo_mmAlloc | ( | uint | Size | ) |
Description
This function allocates the required memory size from jumbo memory area.
[in] | Size | Page Index in the Page Info Table. |
Returns | the pointer to allocated memory block. |
void jumbo_mmFree | ( | void * | p | ) |
Description
This function frees the memory pointed to by the arguments to it.
[in] | p | Pointer to the memory block that is to be freed. |
None. |