![]() |
![]() |
Data Structures | |
struct | IPV6_DEV_RECORD |
The structure describes the IPv6 Device Record. More... | |
struct | IPV6STATS |
The structure describes the IPv6 Statistics Block. More... | |
Functions | |
_extern void | IPv6ParseExtnHeaders (PBM_Pkt *pPkt, IPV6HDR *ptr_ipv6hdr) |
_extern int | IPv6ParseFragHdr (PBM_Pkt *pPkt, IPV6HDR *ptr_ipv6hdr) |
_extern void | IPv6RxPacket (PBM_Pkt *pPkt) |
_extern HANDLE | IPv6GetRoute (IP6N DstIP) |
_extern int | IPv6TxPacket (PBM_Pkt *pPkt, UINT32 Flags) |
_extern int | IPv6InterfaceDeInit (UINT16 dev_index) |
_extern int | IPv6AddAddress (UINT16 dev_index, IP6N Address, UINT16 NetBits, UINT32 VLT, UINT32 PLT, UINT8 IsAny) |
_extern int | IPv6DelAddress (UINT16 dev_index, IP6N Address) |
_extern void | IPv6GetSubnetMaskFromBits (IP6N *SubnetMask, UINT16 bits) |
_extern void | IPv6DisplayIPAddress (IP6N address) |
_extern int | IPv6StringToIPAddress (char *StringIP, IP6N *address) |
_extern UINT16 | IPv6CompareAddress (IP6N addr1, IP6N addr2) |
_extern UINT16 | IPv6IsMulticast (IP6N address) |
_extern UINT16 | IPv6IsLinkLocal (IP6N address) |
_extern UINT16 | IPv6Layer4ComputeChecksum (UINT8 *ptr_l4Hdr, PSEUDOV6 *ptr_pseudoHdr) |
_extern int IPv6AddAddress | ( | UINT16 | dev_index, | |
IP6N | Address, | |||
UINT16 | NetBits, | |||
UINT32 | ValidLifetime, | |||
UINT32 | PrefLifetime, | |||
UINT8 | IsAnycast | |||
) |
Description
This function is used to add an IPv6 address to an interface. This function should not be used to add Link Local Addresses to the interface. Link Local Addresses are automatically added to the interface when the IPv6 stack is initialized on it.
[in] | dev_index | The device index on which the IPv6 address needs to be added. |
[in] | Address | The IPv6 Address which needs to be added. |
[in] | NetBits | The number of bits which make the Subnet-Mask. |
[in] | ValidLifetime | The Valid Lifetime of the address. Set to INFINITE_LT if the address is permanent |
[in] | PrefLifetime | The Preferred Lifetime of the address. Set to INFINITE_LT if the address is permanent. |
[in] | IsAnycast | Flag which indicates if the address to be added is ANYCAST or UNICAST. Set to 1 for ANYCAST. |
0 | - Success | |
<0 | - Error |
_extern UINT16 IPv6CompareAddress | ( | IP6N | addr1, | |
IP6N | addr2 | |||
) |
Description
Utility Function used to compare the 2 IPv6 Addresses.
This is for *internal* NDK Stack Usage.
[in] | addr1 | The first IPv6 Address which is to be compared. |
[in] | addr2 | The second IPv6 Address which is to be compared. |
1 | - The IP Addresses match | |
0 | - The IP Addresses do not match |
_extern int IPv6DelAddress | ( | UINT16 | dev_index, | |
IP6N | Address | |||
) |
Description
This function is used to delete an IPv6 address from an interface This function should not be used to delete Link Local Addresses from the interface. Link Local Addresses are automatically deleted from the interface when the IPv6 stack is de-initialized on it.
[in] | dev_index | The device index on which the IPv6 address needs to be deleted. |
[in] | Address | The IPv6 Address which needs to be deleted. |
0 | - Success | |
<0 | - Error |
_extern void IPv6DisplayIPAddress | ( | IP6N | address | ) |
Description
Utility Function which prints the IPv6 address. The IP address passed has to be specified in network order (IP6N).
[in] | address | IPv6 Address to be displayed. |
Not | Applicable. |
_extern HANDLE IPv6GetRoute | ( | IP6N | DstIP | ) |
Description
The function is used to get an IPv6 route matching the destination IP Address. The function increments the reference counter for the ROUTE6 object.
This is for *internal* NDK Stack Usage.
[in] | DstIP | IPv6 Destination IP address we are trying to find a route for. |
Success | - Handle of the Route6 object to be used. | |
Error | - 0 |
_extern void IPv6GetSubnetMaskFromBits | ( | IP6N * | SubnetMask, | |
UINT16 | bits | |||
) |
Description
Utility Function which gets the subnet mask given the number of bits.
For example: Subnet Mask = 0xFFFF:: if the bits is 16
This is for *internal* NDK Stack Usage.
[out] | SubnetMask | Pointer to the computed subnet mask in network order. |
[in] | bits | Number of bits in the subnet mask |
Not | Applicable. |
_extern int IPv6InterfaceDeInit | ( | UINT16 | dev_index | ) |
Description
This function is used to deinitialize the IPv6 stack on the the specific device name. The function is available to System Developers and should only be called from within kernel mode.
[in] | dev_index | The device index on which the IPv6 stack is to be deinitialized. |
0 | - Success | |
<0 | - Error |
_extern UINT16 IPv6IsLinkLocal | ( | IP6N | address | ) |
Description
Utility Function which determines if the IPv6 Address specified is a Link Local address or not?
This is for *internal* NDK Stack Usage.
[in] | address | IPv6 Address which needs to be verfied. |
1 | - The address passed is Link Local | |
0 | - The address passed is NOT Link Local |
_extern UINT16 IPv6IsMulticast | ( | IP6N | address | ) |
Description
Utility Function which determines if the IPv6 Address specified is a Multicast address or not?
This is for *internal* NDK Stack Usage.
[in] | address | IPv6 Address which needs to be verfied. |
1 | - The address passed is MULTICAST | |
0 | - The address passed is NOT Multicast |
_extern UINT16 IPv6Layer4ComputeChecksum | ( | UINT8 * | ptr_l4Hdr, | |
PSEUDOV6 * | ptr_pseudoHdr | |||
) |
Description
The function does the Layer4 Checksum computation.
[in] | ptr_l4Hdr | Pointer to the Layer4 Header. This could be TCP, UDP or ICMPv6. |
[in] | ptr_pseudoHdr | Pointer to the Pseudo Header. |
Returns | the computed checksum. |
_extern void IPv6ParseExtnHeaders | ( | PBM_Pkt * | pPkt, | |
IPV6HDR * | ptr_ipv6hdr | |||
) |
Description
The function handles all IPV6 extension headers.
[in] | pPkt | Pointer to the entire IPv6 Packet. |
[in] | ptr_ipv6hdr | Pointer to the IPv6 Header. |
None |
_extern int IPv6ParseFragHdr | ( | PBM_Pkt * | pPkt, | |
IPV6HDR * | ptr_ipv6hdr | |||
) |
Description
The function handles all packets with fragmentation header.
[in] | pPkt | Pointer to the entire IPv6 Packet. |
[in] | ptr_ipv6hdr | Pointer to the IPv6 Header. |
-1 | - Error in processing the packet. Packet has been cleaned up. | |
1 | - Packet has been successfully processed by fragmentation module. Its been absorbed by this module for reassembly. Ignore this packet. This packet is now a responsibility of the fragmentation layer for further processing. |
_extern void IPv6RxPacket | ( | PBM_Pkt * | pPkt | ) |
Description
This function is used to process an IPv6 packet received on the network.
This is for *internal* NDK Stack Usage.
[in] | pPkt | Pointer to the IPv6 packet. |
Not | Applicable. |
_extern int IPv6StringToIPAddress | ( | char * | StringIP, | |
IP6N * | address | |||
) |
Description
Utility Function which converts an IPv6 Address from CHAR Format to IP6N
[in] | StringIP | The IPv6 Address in String Format |
[out] | address | The IPv6 Address in IP6N format. |
0 | - Success | |
-1 | - Error |
_extern int IPv6TxPacket | ( | PBM_Pkt * | pPkt, | |
UINT32 | Flags | |||
) |
Description
The function is used to transmit an IPv6 packet.
This is for *internal* NDK Stack Usage.
[in] | pPkt | Pointer to the IPv6 packet which needs to be transmitted |
[in] | Flags | Flags which need to be worked out. (Placeholder) |
Success | - 0 | |
Error | - <0 |