![]() |
![]() |
Data Structures | |
struct | DREC |
The structure describes the Daemon Entry. More... | |
struct | _child |
The structure describes the data instance for daemon child task. More... | |
Typedefs | |
typedef _child | CHILD |
The structure describes the data instance for daemon child task. | |
Functions | |
HANDLE | DaemonNew (uint Type, IPN LocalAddress, uint LocalPort, int(*pCb)(SOCKET, UINT32), uint Priority, uint StackSize, UINT32 Argument, uint MaxSpawn) |
void | DaemonFree (HANDLE hEntry) |
HANDLE | Daemon6New (uint Type, IP6N LocalAddress, uint LocalPort, int(*pCb)(SOCKET, UINT32), uint Priority, uint StackSize, UINT32 Argument, uint MaxSpawn) |
void | Daemon6Free (HANDLE hEntry) |
void Daemon6Free | ( | HANDLE | hEntry | ) |
Description
The function is to used cleanup a previously created V6 daemon.
[in] | hEntry | This is the handle to the daemon which was previously created using Daemon6New |
Not | Applicable. |
HANDLE Daemon6New | ( | uint | Type, | |
IP6N | LocalAddress, | |||
uint | LocalPort, | |||
int(*)(SOCKET, UINT32) | pCb, | |||
uint | Priority, | |||
uint | StackSize, | |||
UINT32 | Argument, | |||
uint | MaxSpawn | |||
) |
Description
The function creates a V6 Daemon.
[in] | Type | This is the type of socket being opened through the daemon. In the case of IPv6 the following types are supported
|
[in] | LocalAddress | This is the Local Address to which the socket will be bound to. In most cases this is typically passed as IPV6_UNSPECIFIED_ADDRESS |
[in] | LocalPort | This is the Local Port to serve (cannot be NULL) |
[in] | pCb | Call back function which is to be invoked. |
[in] | Priority | Priority of new task to create for callback function |
[in] | StackSize | Stack size of new task to create for callback function |
[in] | Argument | Argument (besides socket) to pass to callback function |
[in] | MaxSpawn | Maximum number of callback function instances (must be 1 for UDP) |
Success | - Handle to the spawned Daemon. | |
Error | - 0 |
void DaemonFree | ( | HANDLE | hEntry | ) |
Description
The function is to used cleanup a previously created V4 daemon.
[in] | hEntry | This is the handle to the daemon which was previously created using DaemonNew |
Not | Applicable. |
HANDLE DaemonNew | ( | uint | Type, | |
IPN | LocalAddress, | |||
uint | LocalPort, | |||
int(*)(SOCKET, UINT32) | pCb, | |||
uint | Priority, | |||
uint | StackSize, | |||
UINT32 | Argument, | |||
uint | MaxSpawn | |||
) |
Description
The function creates a V4 Daemon.
[in] | Type | This is the type of socket being opened through the daemon. In the case of IPv4 all socket types are supported i.e. SOCK_STREAM, SOCK_STREAMNC and SOCK_DGRAM. |
[in] | LocalAddress | This is the Local Address to which the socket will be bound to. In most cases this is typically passed as NULL. |
[in] | LocalPort | This is the Local Port to serve (cannot be NULL) |
[in] | pCb | Call back function which is to be invoked. |
[in] | Priority | Priority of new task to create for callback function |
[in] | StackSize | Stack size of new task to create for callback function |
[in] | Argument | Argument (besides socket) to pass to callback function |
[in] | MaxSpawn | Maximum number of callback function instances (must be 1 for UDP) |
Success | - Handle to the spawned Daemon. | |
Error | - 0 |