#include <stdbool.h>
#include <stdint.h>
#include <inc/hw_types.h>
#include <inc/hw_memmap.h>
#include <inc/hw_vims.h>
#include <driverlib/debug.h>
Go to the source code of this file.
Macros | |
#define | VIMS_MODE_CHANGING 0x4 |
#define | VIMS_MODE_DISABLED 0x0 |
#define | VIMS_MODE_ENABLED 0x1 |
#define | VIMS_MODE_SPLIT 0x2 |
#define | VIMS_MODE_OFF 0x3 |
Functions | |
void | VIMSConfigure (uint32_t ui32Base, bool bRoundRobin, bool bPrefetch) |
Configures the VIMS. More... | |
void | VIMSModeSet (uint32_t ui32Base, uint32_t ui32Mode) |
Set the operational mode of the VIMS. More... | |
uint32_t | VIMSModeGet (uint32_t ui32Base) |
Get the current operational mode of the VIMS. More... | |
void | VIMSModeSetBlocking (uint32_t ui32Mode) |
Set the operational mode of the VIMS in a safe sequence (blocking). More... | |
static void | VIMSLineBufDisable (uint32_t ui32Base) |
Disable VIMS linebuffers. More... | |
static void | VIMSLineBufEnable (uint32_t ui32Base) |
Enable VIMS linebuffers. More... | |