CC26xx Driver Library
udma.h
Go to the documentation of this file.
1 /******************************************************************************
2 * Filename: udma.h
3 * Revised: 2015-08-03 10:40:26 +0200 (Mon, 03 Aug 2015)
4 * Revision: 44307
5 *
6 * Description: Defines and prototypes for the uDMA controller.
7 *
8 * Copyright (c) 2015, Texas Instruments Incorporated
9 * All rights reserved.
10 *
11 * Redistribution and use in source and binary forms, with or without
12 * modification, are permitted provided that the following conditions are met:
13 *
14 * 1) Redistributions of source code must retain the above copyright notice,
15 * this list of conditions and the following disclaimer.
16 *
17 * 2) Redistributions in binary form must reproduce the above copyright notice,
18 * this list of conditions and the following disclaimer in the documentation
19 * and/or other materials provided with the distribution.
20 *
21 * 3) Neither the name of the ORGANIZATION nor the names of its contributors may
22 * be used to endorse or promote products derived from this software without
23 * specific prior written permission.
24 *
25 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
26 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
27 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
28 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
29 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
30 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
31 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
32 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
33 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
34 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
35 * POSSIBILITY OF SUCH DAMAGE.
36 *
37 ******************************************************************************/
38 
39 //*****************************************************************************
40 //
45 //
46 //*****************************************************************************
47 
48 #ifndef __UDMA_H__
49 #define __UDMA_H__
50 
51 //*****************************************************************************
52 //
53 // If building with a C++ compiler, make all of the definitions in this header
54 // have a C binding.
55 //
56 //*****************************************************************************
57 #ifdef __cplusplus
58 extern "C"
59 {
60 #endif
61 
62 #include <stdbool.h>
63 #include <stdint.h>
64 #include <inc/hw_types.h>
65 #include <inc/hw_ints.h>
66 #include <inc/hw_memmap.h>
67 #include <inc/hw_udma.h>
68 #include <driverlib/debug.h>
69 #include <driverlib/interrupt.h>
70 
71 //*****************************************************************************
72 //
73 // Support for DriverLib in ROM:
74 // This section renames all functions that are not "static inline", so that
75 // calling these functions will default to implementation in flash. At the end
76 // of this file a second renaming will change the defaults to implementation in
77 // ROM for available functions.
78 //
79 // To force use of the implementation in flash, e.g. for debugging:
80 // - Globally: Define DRIVERLIB_NOROM at project level
81 // - Per function: Use prefix "NOROM_" when calling the function
82 //
83 //*****************************************************************************
84 #if !defined(DOXYGEN)
85  #define uDMAChannelAttributeEnable NOROM_uDMAChannelAttributeEnable
86  #define uDMAChannelAttributeDisable NOROM_uDMAChannelAttributeDisable
87  #define uDMAChannelAttributeGet NOROM_uDMAChannelAttributeGet
88  #define uDMAChannelControlSet NOROM_uDMAChannelControlSet
89  #define uDMAChannelTransferSet NOROM_uDMAChannelTransferSet
90  #define uDMAChannelScatterGatherSet NOROM_uDMAChannelScatterGatherSet
91  #define uDMAChannelSizeGet NOROM_uDMAChannelSizeGet
92  #define uDMAChannelModeGet NOROM_uDMAChannelModeGet
93 #endif
94 
95 //*****************************************************************************
96 //
101 //
102 //*****************************************************************************
103 typedef struct
104 {
105  volatile void *pvSrcEndAddr;
106  volatile void *pvDstEndAddr;
107  volatile uint32_t ui32Control;
108  volatile uint32_t ui32Spare;
109 }
111 
112 //*****************************************************************************
113 //
127 
139 //
179 //*****************************************************************************
180 #define uDMATaskStructEntry(ui32TransferCount, \
181  ui32ItemSize, \
182  ui32SrcIncrement, \
183  pvSrcAddr, \
184  ui32DstIncrement, \
185  pvDstAddr, \
186  ui32ArbSize, \
187  ui32Mode) \
188  { \
189  (((ui32SrcIncrement) == UDMA_SRC_INC_NONE) ? (pvSrcAddr) : \
190  ((void *)(&((uint8_t *)(pvSrcAddr))[((ui32TransferCount) << \
191  ((ui32SrcIncrement) >> 26)) - 1]))), \
192  (((ui32DstIncrement) == UDMA_DST_INC_NONE) ? (pvDstAddr) : \
193  ((void *)(&((uint8_t *)(pvDstAddr))[((ui32TransferCount) << \
194  ((ui32DstIncrement) >> 30)) - 1]))), \
195  (ui32SrcIncrement) | (ui32DstIncrement) | (ui32ItemSize) | \
196  (ui32ArbSize) | (((ui32TransferCount) - 1) << 4) | \
197  ((((ui32Mode) == UDMA_MODE_MEM_SCATTER_GATHER) || \
198  ((ui32Mode) == UDMA_MODE_PER_SCATTER_GATHER)) ? \
199  (ui32Mode) | UDMA_MODE_ALT_SELECT : (ui32Mode)), 0 \
200  }
201 
202 //*****************************************************************************
203 //
204 // The hardware configured number of uDMA channels.
205 //
206 //*****************************************************************************
207 #define UDMA_NUM_CHANNELS 21
208 
209 //*****************************************************************************
210 //
211 // The level of priority for the uDMA channels
212 //
213 //*****************************************************************************
214 #define UDMA_PRIORITY_LOW 0x00000000
215 #define UDMA_PRIORITY_HIGH 0x00000001
216 
217 //*****************************************************************************
218 //
219 // Flags that can be passed to uDMAChannelAttributeEnable(),
220 // uDMAChannelAttributeDisable(), and returned from uDMAChannelAttributeGet().
221 //
222 //*****************************************************************************
223 #define UDMA_ATTR_USEBURST 0x00000001
224 #define UDMA_ATTR_ALTSELECT 0x00000002
225 #define UDMA_ATTR_HIGH_PRIORITY 0x00000004
226 #define UDMA_ATTR_REQMASK 0x00000008
227 #define UDMA_ATTR_ALL 0x0000000F
228 
229 //*****************************************************************************
230 //
231 // DMA control modes that can be passed to uDMAChannelModeSet() and returned
232 // uDMAChannelModeGet().
233 //
234 //*****************************************************************************
235 #define UDMA_MODE_STOP 0x00000000
236 #define UDMA_MODE_BASIC 0x00000001
237 #define UDMA_MODE_AUTO 0x00000002
238 #define UDMA_MODE_PINGPONG 0x00000003
239 #define UDMA_MODE_MEM_SCATTER_GATHER \
240  0x00000004
241 #define UDMA_MODE_PER_SCATTER_GATHER \
242  0x00000006
243 #define UDMA_MODE_M 0x00000007 // uDMA Transfer Mode
244 #define UDMA_MODE_ALT_SELECT 0x00000001
245 
246 //*****************************************************************************
247 //
248 // Channel configuration values that can be passed to uDMAControlSet().
249 //
250 //*****************************************************************************
251 #define UDMA_DST_INC_8 0x00000000
252 #define UDMA_DST_INC_16 0x40000000
253 #define UDMA_DST_INC_32 0x80000000
254 #define UDMA_DST_INC_NONE 0xC0000000
255 #define UDMA_DST_INC_M 0xC0000000 // Destination Address Increment
256 #define UDMA_DST_INC_S 30
257 #define UDMA_SRC_INC_8 0x00000000
258 #define UDMA_SRC_INC_16 0x04000000
259 #define UDMA_SRC_INC_32 0x08000000
260 #define UDMA_SRC_INC_NONE 0x0c000000
261 #define UDMA_SRC_INC_M 0x0C000000 // Source Address Increment
262 #define UDMA_SRC_INC_S 26
263 #define UDMA_SIZE_8 0x00000000
264 #define UDMA_SIZE_16 0x11000000
265 #define UDMA_SIZE_32 0x22000000
266 #define UDMA_SIZE_M 0x33000000 // Data Size
267 #define UDMA_SIZE_S 24
268 #define UDMA_ARB_1 0x00000000
269 #define UDMA_ARB_2 0x00004000
270 #define UDMA_ARB_4 0x00008000
271 #define UDMA_ARB_8 0x0000c000
272 #define UDMA_ARB_16 0x00010000
273 #define UDMA_ARB_32 0x00014000
274 #define UDMA_ARB_64 0x00018000
275 #define UDMA_ARB_128 0x0001c000
276 #define UDMA_ARB_256 0x00020000
277 #define UDMA_ARB_512 0x00024000
278 #define UDMA_ARB_1024 0x00028000
279 #define UDMA_ARB_M 0x0003C000 // Arbitration Size
280 #define UDMA_ARB_S 14
281 #define UDMA_NEXT_USEBURST 0x00000008
282 #define UDMA_XFER_SIZE_MAX 1024
283 #define UDMA_XFER_SIZE_M 0x00003FF0 // Transfer size
284 #define UDMA_XFER_SIZE_S 4
285 
286 //*****************************************************************************
287 //
288 // Channel numbers to be passed to API functions that require a channel number
289 // ID.
290 //
291 //*****************************************************************************
292 #define UDMA_CHAN_SW_EVT0 0 // Software Event Channel 0
293 #define UDMA_CHAN_UART0_RX 1 // UART0 RX Data
294 #define UDMA_CHAN_UART0_TX 2 // UART0 RX Data
295 #define UDMA_CHAN_SSI0_RX 3 // SSI0 RX Data
296 #define UDMA_CHAN_SSI0_TX 4 // SSI0 RX Data
297 #define UDMA_CHAN_SPIS_RX 5 // SPIS RX Data
298 #define UDMA_CHAN_SPIS_TX 6 // SPIS RX Data
299 #define UDMA_CHAN_AUX_ADC 7 // AUX ADC event
300 #define UDMA_CHAN_AUX_SW 8 // AUX Software event
301 #define UDMA_CHAN_TIMER0_A 9 // Timer0 A event
302 #define UDMA_CHAN_TIMER0_B 10 // Timer0 B event
303 #define UDMA_CHAN_TIMER1_A 11
304 #define UDMA_CHAN_TIMER1_B 12
305 #define UDMA_CHAN_AON_PROG2 13
306 #define UDMA_CHAN_DMA_PROG 14
307 #define UDMA_CHAN_AON_RTC 15
308 #define UDMA_CHAN_SSI1_RX 16
309 #define UDMA_CHAN_SSI1_TX 17
310 #define UDMA_CHAN_SW_EVT1 18
311 #define UDMA_CHAN_SW_EVT2 19
312 #define UDMA_CHAN_SW_EVT3 20
313 
314 //*****************************************************************************
315 //
316 // Flags to be OR'd with the channel ID to indicate if the primary or alternate
317 // control structure should be used.
318 //
319 //*****************************************************************************
320 #define UDMA_PRI_SELECT 0x00000000
321 #define UDMA_ALT_SELECT 0x00000020
322 
323 //*****************************************************************************
324 //
325 // API Functions and prototypes
326 //
327 //*****************************************************************************
328 
329 #ifdef DRIVERLIB_DEBUG
330 //*****************************************************************************
331 //
342 //
343 //*****************************************************************************
344 static bool
345 uDMABaseValid(uint32_t ui32Base)
346 {
347  return(ui32Base == UDMA0_BASE);
348 }
349 #endif
350 
351 //*****************************************************************************
352 //
361 //
362 //*****************************************************************************
363 __STATIC_INLINE void
364 uDMAEnable(uint32_t ui32Base)
365 {
366  //
367  // Check the arguments.
368  //
369  ASSERT(uDMABaseValid(ui32Base));
370 
371  //
372  // Set the master enable bit in the config register.
373  //
374  HWREG(ui32Base + UDMA_O_CFG) = UDMA_CFG_MASTERENABLE;
375 }
376 
377 //*****************************************************************************
378 //
387 //
388 //*****************************************************************************
389 __STATIC_INLINE void
390 uDMADisable(uint32_t ui32Base)
391 {
392  //
393  // Check the arguments.
394  //
395  ASSERT(uDMABaseValid(ui32Base));
396 
397  //
398  // Clear the master enable bit in the config register.
399  //
400  HWREG(ui32Base + UDMA_O_CFG) = 0;
401 }
402 
403 //*****************************************************************************
404 //
414 //
415 //*****************************************************************************
416 __STATIC_INLINE uint32_t
417 uDMAErrorStatusGet(uint32_t ui32Base)
418 {
419  //
420  // Check the arguments.
421  //
422  ASSERT(uDMABaseValid(ui32Base));
423 
424  //
425  // Return the uDMA error status.
426  //
427  return(HWREG(ui32Base + UDMA_O_ERROR));
428 }
429 
430 //*****************************************************************************
431 //
440 //
441 //*****************************************************************************
442 __STATIC_INLINE void
443 uDMAErrorStatusClear(uint32_t ui32Base)
444 {
445  //
446  // Check the arguments.
447  //
448  ASSERT(uDMABaseValid(ui32Base));
449 
450  //
451  // Clear the uDMA error interrupt.
452  //
453  HWREG(ui32Base + UDMA_O_ERROR) = UDMA_ERROR_STATUS;
454 }
455 
456 //*****************************************************************************
457 //
472 //
473 //*****************************************************************************
474 __STATIC_INLINE void
475 uDMAChannelEnable(uint32_t ui32Base, uint32_t ui32ChannelNum)
476 {
477  //
478  // Check the arguments.
479  //
480  ASSERT(uDMABaseValid(ui32Base));
481  ASSERT(ui32ChannelNum < UDMA_NUM_CHANNELS);
482 
483  //
484  // Set the bit for this channel in the enable set register.
485  //
486  HWREG(ui32Base + UDMA_O_SETCHANNELEN) = 1 << ui32ChannelNum;
487 }
488 
489 //*****************************************************************************
490 //
501 //
502 //*****************************************************************************
503 __STATIC_INLINE void
504 uDMAChannelDisable(uint32_t ui32Base, uint32_t ui32ChannelNum)
505 {
506  //
507  // Check the arguments.
508  //
509  ASSERT(uDMABaseValid(ui32Base));
510  ASSERT(ui32ChannelNum < UDMA_NUM_CHANNELS);
511 
512  //
513  // Set the bit for this channel in the enable clear register.
514  //
515  HWREG(ui32Base + UDMA_O_CLEARCHANNELEN) = 1 << ui32ChannelNum;
516 }
517 
518 //*****************************************************************************
519 //
532 //
533 //*****************************************************************************
534 __STATIC_INLINE bool
535 uDMAChannelIsEnabled(uint32_t ui32Base, uint32_t ui32ChannelNum)
536 {
537  //
538  // Check the arguments.
539  //
540  ASSERT(uDMABaseValid(ui32Base));
541  ASSERT(ui32ChannelNum < UDMA_NUM_CHANNELS);
542 
543  //
544  // AND the specified channel bit with the enable register, and return the
545  // result.
546  //
547  return((HWREG(ui32Base + UDMA_O_SETCHANNELEN) & (1 << ui32ChannelNum)) ?
548  true : false);
549 }
550 
551 //*****************************************************************************
552 //
577 //
578 //*****************************************************************************
579 __STATIC_INLINE void
580 uDMAControlBaseSet(uint32_t ui32Base, void *pControlTable)
581 {
582  //
583  // Check the arguments.
584  //
585  ASSERT(uDMABaseValid(ui32Base));
586  ASSERT(((uint32_t)pControlTable & ~0x3FF) ==
587  (uint32_t)pControlTable);
588  ASSERT((uint32_t)pControlTable >= SRAM_BASE);
589 
590  //
591  // Program the base address into the register.
592  //
593  HWREG(ui32Base + UDMA_O_CTRL) = (uint32_t)pControlTable;
594 }
595 
596 //*****************************************************************************
597 //
607 //
608 //*****************************************************************************
609 __STATIC_INLINE void *
610 uDMAControlBaseGet(uint32_t ui32Base)
611 {
612  //
613  // Check the arguments.
614  //
615 
616  ASSERT(uDMABaseValid(ui32Base));
617  //
618  // Read the current value of the control base register, and return it to
619  // the caller.
620  //
621  return((void *)HWREG(ui32Base + UDMA_O_CTRL));
622 }
623 
624 //*****************************************************************************
625 //
635 //
636 //*****************************************************************************
637 __STATIC_INLINE void *
638 uDMAControlAlternateBaseGet(uint32_t ui32Base)
639 {
640  //
641  // Check the arguments.
642  //
643  ASSERT(uDMABaseValid(ui32Base));
644 
645  //
646  // Read the current value of the control base register, and return it to
647  // the caller.
648  //
649  return((void *)HWREG(ui32Base + UDMA_O_ALTCTRL));
650 }
651 
652 //*****************************************************************************
653 //
671 //
672 //*****************************************************************************
673 __STATIC_INLINE void
674 uDMAChannelRequest(uint32_t ui32Base, uint32_t ui32ChannelNum)
675 {
676  //
677  // Check the arguments.
678  //
679  ASSERT(uDMABaseValid(ui32Base));
680  ASSERT(ui32ChannelNum < UDMA_NUM_CHANNELS);
681 
682  //
683  // Set the bit for this channel in the software uDMA request register.
684  //
685  HWREG(ui32Base + UDMA_O_SOFTREQ) = 1 << ui32ChannelNum;
686 }
687 
688 //*****************************************************************************
689 //
706 //
707 //*****************************************************************************
708 extern void uDMAChannelAttributeEnable(uint32_t ui32Base,
709  uint32_t ui32ChannelNum,
710  uint32_t ui32Attr);
711 
712 //*****************************************************************************
713 //
730 //
731 //*****************************************************************************
732 extern void uDMAChannelAttributeDisable(uint32_t ui32Base,
733  uint32_t ui32ChannelNum,
734  uint32_t ui32Attr);
735 
736 //*****************************************************************************
737 //
754 //
755 //*****************************************************************************
756 extern uint32_t uDMAChannelAttributeGet(uint32_t ui32Base,
757  uint32_t ui32ChannelNum);
758 
759 //*****************************************************************************
760 //
799 //
800 //*****************************************************************************
801 extern void uDMAChannelControlSet(uint32_t ui32Base,
802  uint32_t ui32ChannelStructIndex,
803  uint32_t ui32Control);
804 
805 //*****************************************************************************
806 //
863 //
864 //*****************************************************************************
865 extern void uDMAChannelTransferSet(uint32_t ui32Base,
866  uint32_t ui32ChannelStructIndex,
867  uint32_t ui32Mode, void *pvSrcAddr,
868  void *pvDstAddr, uint32_t ui32TransferSize);
869 
870 //*****************************************************************************
871 //
896 //
897 //*****************************************************************************
898 extern void uDMAChannelScatterGatherSet(uint32_t ui32Base,
899  uint32_t ui32ChannelNum,
900  uint32_t ui32TaskCount,
901  void *pvTaskList,
902  uint32_t ui32IsPeriphSG);
903 
904 //*****************************************************************************
905 //
920 //
921 //*****************************************************************************
922 extern uint32_t uDMAChannelSizeGet(uint32_t ui32Base,
923  uint32_t ui32ChannelStructIndex);
924 
925 //*****************************************************************************
926 //
946 //
947 //*****************************************************************************
948 extern uint32_t uDMAChannelModeGet(uint32_t ui32Base,
949  uint32_t ui32ChannelStructIndex);
950 
951 //*****************************************************************************
952 //
976 //
977 //*****************************************************************************
978 __STATIC_INLINE void
979 uDMAIntRegister(uint32_t ui32Base, uint32_t ui32IntChannel,
980  void (*pfnHandler)(void))
981 {
982  //
983  // Check the arguments.
984  //
985  ASSERT(uDMABaseValid(ui32Base));
986  ASSERT(pfnHandler);
987  ASSERT((ui32IntChannel == INT_UDMA) || (ui32IntChannel == INT_UDMAERR));
988 
989  //
990  // Register the interrupt handler.
991  //
992  IntRegister(ui32IntChannel, pfnHandler);
993 
994  //
995  // Enable the memory management fault.
996  //
997  IntEnable(ui32IntChannel);
998 }
999 
1000 //*****************************************************************************
1001 //
1018 //
1019 //*****************************************************************************
1020 __STATIC_INLINE void
1021 uDMAIntUnregister(uint32_t ui32Base, uint32_t ui32IntChannel)
1022 {
1023  //
1024  // Check the arguments.
1025  //
1026  ASSERT(uDMABaseValid(ui32Base));
1027  ASSERT((ui32IntChannel == INT_UDMA) || (ui32IntChannel == INT_UDMAERR));
1028 
1029  //
1030  // Disable the interrupt.
1031  //
1032  IntDisable(ui32IntChannel);
1033 
1034  //
1035  // Unregister the interrupt handler.
1036  //
1037  IntUnregister(ui32IntChannel);
1038 }
1039 
1040 //*****************************************************************************
1041 //
1053 //
1054 //*****************************************************************************
1055 __STATIC_INLINE void
1056 uDMAIntClear(uint32_t ui32Base, uint32_t ui32ChanMask)
1057 {
1058  //
1059  // Check the arguments.
1060  //
1061  ASSERT(uDMABaseValid(ui32Base));
1062 
1063  //
1064  // Clear the requested bits in the uDMA interrupt status register.
1065  //
1066  HWREG(ui32Base + UDMA_O_REQDONE) = ui32ChanMask;
1067 }
1068 
1069 //*****************************************************************************
1070 //
1080 //
1081 //*****************************************************************************
1082 __STATIC_INLINE uint32_t
1083 uDMAIntStatus(uint32_t ui32Base)
1084 {
1085  //
1086  // Check the arguments.
1087  //
1088  ASSERT(uDMABaseValid(ui32Base));
1089 
1090  //
1091  // Return the uDMA interrupt status register.
1092  //
1093  return (HWREG(ui32Base + UDMA_O_REQDONE));
1094 }
1095 
1096 //*****************************************************************************
1097 //
1112 //
1113 //*****************************************************************************
1114 __STATIC_INLINE void
1115 uDMAIntSwEventEnable(uint32_t ui32Base, uint32_t ui32IntChannel)
1116 {
1117  //
1118  // Check the arguments.
1119  //
1120  ASSERT(uDMABaseValid(ui32Base));
1121  ASSERT(ui32IntChannel < UDMA_NUM_CHANNELS);
1122 
1123  //
1124  // Enable the channel.
1125  //
1126  HWREGBITW(ui32Base + UDMA_O_DONEMASK, ui32IntChannel) = 1;
1127 }
1128 
1129 //*****************************************************************************
1130 //
1143 //
1144 //*****************************************************************************
1145 __STATIC_INLINE void
1146 uDMAIntSwEventDisable(uint32_t ui32Base, uint32_t ui32IntChannel)
1147 {
1148  //
1149  // Check the arguments.
1150  //
1151  ASSERT(uDMABaseValid(ui32Base));
1152  ASSERT(ui32IntChannel < UDMA_NUM_CHANNELS);
1153 
1154  //
1155  // Disable the SW channel.
1156  //
1157  HWREGBITW(ui32Base + UDMA_O_DONEMASK, ui32IntChannel) = 0;
1158 }
1159 
1160 //*****************************************************************************
1161 //
1169 //
1170 //*****************************************************************************
1171 __STATIC_INLINE uint32_t
1172 uDMAGetStatus(uint32_t ui32Base)
1173 {
1174  //
1175  // Check the arguments.
1176  //
1177  ASSERT(uDMABaseValid(ui32Base));
1178 
1179  //
1180  // Read and return the status register.
1181  //
1182  return HWREG(ui32Base + UDMA_O_STATUS);
1183 }
1184 
1185 //*****************************************************************************
1186 //
1196 //
1197 //*****************************************************************************
1198 __STATIC_INLINE void
1199 uDMAChannelPrioritySet(uint32_t ui32Base, uint32_t ui32ChannelNum)
1200 {
1201  //
1202  // Check the arguments.
1203  //
1204  ASSERT(uDMABaseValid(ui32Base));
1205  ASSERT(ui32ChannelNum < UDMA_NUM_CHANNELS);
1206 
1207  //
1208  // Set the channel priority to high.
1209  //
1210  HWREG(ui32Base + UDMA_O_SETCHNLPRIORITY) = 1 << ui32ChannelNum;
1211 }
1212 
1213 //*****************************************************************************
1214 //
1223 //
1224 //*****************************************************************************
1225 __STATIC_INLINE bool
1226 uDMAChannelPriorityGet(uint32_t ui32Base, uint32_t ui32ChannelNum)
1227 {
1228  //
1229  // Check the arguments.
1230  //
1231  ASSERT(uDMABaseValid(ui32Base));
1232  ASSERT(ui32ChannelNum < UDMA_NUM_CHANNELS);
1233 
1234  //
1235  // Return the channel priority.
1236  //
1237  return(HWREG(ui32Base + UDMA_O_SETCHNLPRIORITY) & (1 << ui32ChannelNum) ?
1239 }
1240 
1241 //*****************************************************************************
1242 //
1252 //
1253 //*****************************************************************************
1254 __STATIC_INLINE void
1255 uDMAChannelPriorityClear(uint32_t ui32Base, uint32_t ui32ChannelNum)
1256 {
1257  //
1258  // Check the arguments.
1259  //
1260  ASSERT(uDMABaseValid(ui32Base));
1261  ASSERT(ui32ChannelNum < UDMA_NUM_CHANNELS);
1262 
1263  //
1264  // Clear the channel priority.
1265  //
1266  HWREG(ui32Base + UDMA_O_CLEARCHNLPRIORITY) = 1 << ui32ChannelNum;
1267 }
1268 
1269 //*****************************************************************************
1270 //
1271 // Support for DriverLib in ROM:
1272 // Redirect to implementation in ROM when available.
1273 //
1274 //*****************************************************************************
1275 #if !defined(DRIVERLIB_NOROM) && !defined(DOXYGEN)
1276  #include <driverlib/rom.h>
1277  #ifdef ROM_uDMAChannelAttributeEnable
1278  #undef uDMAChannelAttributeEnable
1279  #define uDMAChannelAttributeEnable ROM_uDMAChannelAttributeEnable
1280  #endif
1281  #ifdef ROM_uDMAChannelAttributeDisable
1282  #undef uDMAChannelAttributeDisable
1283  #define uDMAChannelAttributeDisable ROM_uDMAChannelAttributeDisable
1284  #endif
1285  #ifdef ROM_uDMAChannelAttributeGet
1286  #undef uDMAChannelAttributeGet
1287  #define uDMAChannelAttributeGet ROM_uDMAChannelAttributeGet
1288  #endif
1289  #ifdef ROM_uDMAChannelControlSet
1290  #undef uDMAChannelControlSet
1291  #define uDMAChannelControlSet ROM_uDMAChannelControlSet
1292  #endif
1293  #ifdef ROM_uDMAChannelTransferSet
1294  #undef uDMAChannelTransferSet
1295  #define uDMAChannelTransferSet ROM_uDMAChannelTransferSet
1296  #endif
1297  #ifdef ROM_uDMAChannelScatterGatherSet
1298  #undef uDMAChannelScatterGatherSet
1299  #define uDMAChannelScatterGatherSet ROM_uDMAChannelScatterGatherSet
1300  #endif
1301  #ifdef ROM_uDMAChannelSizeGet
1302  #undef uDMAChannelSizeGet
1303  #define uDMAChannelSizeGet ROM_uDMAChannelSizeGet
1304  #endif
1305  #ifdef ROM_uDMAChannelModeGet
1306  #undef uDMAChannelModeGet
1307  #define uDMAChannelModeGet ROM_uDMAChannelModeGet
1308  #endif
1309 #endif
1310 
1311 //*****************************************************************************
1312 //
1313 // Mark the end of the C bindings section for C++ compilers.
1314 //
1315 //*****************************************************************************
1316 #ifdef __cplusplus
1317 }
1318 #endif
1319 
1320 #endif // __UDMA_H__
1321 
1322 //*****************************************************************************
1323 //
1327 //
1328 //*****************************************************************************
#define UDMA_NUM_CHANNELS
Definition: udma.h:207
uint32_t uDMAChannelModeGet(uint32_t ui32Base, uint32_t ui32ChannelStructIndex)
Gets the transfer mode for a uDMA channel control structure.
Definition: udma.c:514
volatile void * pvSrcEndAddr
The ending source address of the data transfer.
Definition: udma.h:105
static void uDMAIntUnregister(uint32_t ui32Base, uint32_t ui32IntChannel)
Unregisters an interrupt handler for the uDMA controller.
Definition: udma.h:1021
void uDMAChannelScatterGatherSet(uint32_t ui32Base, uint32_t ui32ChannelNum, uint32_t ui32TaskCount, void *pvTaskList, uint32_t ui32IsPeriphSG)
Configures a uDMA channel for scatter-gather mode.
Definition: udma.c:391
#define UDMA_PRIORITY_LOW
Definition: udma.h:214
static uint32_t uDMAGetStatus(uint32_t ui32Base)
Return the status of the uDMA module.
Definition: udma.h:1172
static void uDMAEnable(uint32_t ui32Base)
Enables the uDMA controller for use.
Definition: udma.h:364
static void uDMAErrorStatusClear(uint32_t ui32Base)
Clears the uDMA error interrupt.
Definition: udma.h:443
static void * uDMAControlBaseGet(uint32_t ui32Base)
Gets the base address for the channel control table.
Definition: udma.h:610
static void uDMAChannelEnable(uint32_t ui32Base, uint32_t ui32ChannelNum)
Enables a uDMA channel for operation.
Definition: udma.h:475
void uDMAChannelAttributeDisable(uint32_t ui32Base, uint32_t ui32ChannelNum, uint32_t ui32Attr)
Disables attributes of an uDMA channel.
Definition: udma.c:123
void uDMAChannelAttributeEnable(uint32_t ui32Base, uint32_t ui32ChannelNum, uint32_t ui32Attr)
Enables attributes of a uDMA channel.
Definition: udma.c:72
void uDMAChannelControlSet(uint32_t ui32Base, uint32_t ui32ChannelStructIndex, uint32_t ui32Control)
Sets the control parameters for a uDMA channel control structure.
Definition: udma.c:228
volatile uint32_t ui32Spare
An unused location.
Definition: udma.h:108
static void uDMAChannelDisable(uint32_t ui32Base, uint32_t ui32ChannelNum)
Disables a uDMA channel for operation.
Definition: udma.h:504
#define ASSERT(expr)
Definition: debug.h:74
volatile uint32_t ui32Control
The channel control mode.
Definition: udma.h:107
volatile void * pvDstEndAddr
The ending destination address of the data transfer.
Definition: udma.h:106
static void uDMAIntSwEventDisable(uint32_t ui32Base, uint32_t ui32IntChannel)
Disable interrupt on software event driven uDMA transfers.
Definition: udma.h:1146
static uint32_t uDMAIntStatus(uint32_t ui32Base)
Get the uDMA interrupt status.
Definition: udma.h:1083
static void uDMAIntClear(uint32_t ui32Base, uint32_t ui32ChanMask)
Clears uDMA interrupt done status.
Definition: udma.h:1056
void IntUnregister(uint32_t ui32Interrupt)
Unregisters the function to be called when an interrupt occurs.
Definition: interrupt.c:203
void uDMAChannelTransferSet(uint32_t ui32Base, uint32_t ui32ChannelStructIndex, uint32_t ui32Mode, void *pvSrcAddr, void *pvDstAddr, uint32_t ui32TransferSize)
Sets the transfer parameters for a uDMA channel control structure.
Definition: udma.c:265
static uint32_t uDMAErrorStatusGet(uint32_t ui32Base)
Gets the uDMA error status.
Definition: udma.h:417
static void uDMAChannelPrioritySet(uint32_t ui32Base, uint32_t ui32ChannelNum)
Set the priority of a uDMA channel.
Definition: udma.h:1199
static bool uDMAChannelIsEnabled(uint32_t ui32Base, uint32_t ui32ChannelNum)
Checks if a uDMA channel is enabled for operation.
Definition: udma.h:535
static void uDMAChannelPriorityClear(uint32_t ui32Base, uint32_t ui32ChannelNum)
Clear the priority of a uDMA channel.
Definition: udma.h:1255
A structure that defines an entry in the channel control table.
Definition: udma.h:103
uint32_t uDMAChannelAttributeGet(uint32_t ui32Base, uint32_t ui32ChannelNum)
Gets the enabled attributes of a uDMA channel.
Definition: udma.c:174
static void uDMAIntRegister(uint32_t ui32Base, uint32_t ui32IntChannel, void(*pfnHandler)(void))
Registers an interrupt handler for the uDMA controller.
Definition: udma.h:979
static void uDMAControlBaseSet(uint32_t ui32Base, void *pControlTable)
Sets the base address for the channel control table.
Definition: udma.h:580
uint32_t uDMAChannelSizeGet(uint32_t ui32Base, uint32_t ui32ChannelStructIndex)
Gets the current transfer size for a uDMA channel control structure.
Definition: udma.c:462
static void * uDMAControlAlternateBaseGet(uint32_t ui32Base)
Gets the base address for the channel control table alternate structures.
Definition: udma.h:638
#define UDMA_PRIORITY_HIGH
Definition: udma.h:215
static void uDMAIntSwEventEnable(uint32_t ui32Base, uint32_t ui32IntChannel)
Enable interrupt on software event driven uDMA transfers.
Definition: udma.h:1115
static void uDMADisable(uint32_t ui32Base)
Disables the uDMA controller for use.
Definition: udma.h:390
void IntDisable(uint32_t ui32Interrupt)
Disables an interrupt.
Definition: interrupt.c:381
void IntRegister(uint32_t ui32Interrupt, void(*pfnHandler)(void))
Registers a function to be called when an interrupt occurs.
Definition: interrupt.c:155
static bool uDMAChannelPriorityGet(uint32_t ui32Base, uint32_t ui32ChannelNum)
Get the priority of a uDMA channel.
Definition: udma.h:1226
void IntEnable(uint32_t ui32Interrupt)
Enables an interrupt.
Definition: interrupt.c:321
static void uDMAChannelRequest(uint32_t ui32Base, uint32_t ui32ChannelNum)
Requests a uDMA channel to start a transfer.
Definition: udma.h:674