CC26xx Driver Library
sys_ctrl.h File Reference
#include <stdbool.h>
#include <stdint.h>
#include <inc/hw_types.h>
#include <inc/hw_memmap.h>
#include <inc/hw_ints.h>
#include <inc/hw_sysctl.h>
#include <inc/hw_prcm.h>
#include <inc/hw_nvic.h>
#include <inc/hw_aon_wuc.h>
#include <inc/hw_aux_wuc.h>
#include <inc/hw_aon_ioc.h>
#include <inc/hw_ddi_0_osc.h>
#include <inc/hw_rfc_pwr.h>
#include <inc/hw_adi_3_refsys.h>
#include <inc/hw_aon_sysctl.h>
#include <inc/hw_aon_rtc.h>
#include <inc/hw_fcfg1.h>
#include <driverlib/interrupt.h>
#include <driverlib/debug.h>
#include <driverlib/pwr_ctrl.h>
#include <driverlib/osc.h>
#include <driverlib/prcm.h>
#include <driverlib/aux_wuc.h>
#include <driverlib/aon_wuc.h>
#include <driverlib/adi.h>
#include <driverlib/ddi.h>
#include <driverlib/cpu.h>
#include <driverlib/vims.h>

Go to the source code of this file.

Macros

#define SYSCTRL_SYSBUS_ON   0x00000001
 
#define SYSCTRL_SYSBUS_OFF   0x00000000
 
#define CPU_RUN   0x00000000
 
#define CPU_SLEEP   0x00000001
 
#define CPU_DEEP_SLEEP   0x00000002
 
#define XOSC_IN_HIGH_POWER_MODE   0
 
#define XOSC_IN_LOW_POWER_MODE   1
 
#define XoscInHighPowerMode   ( XOSC_IN_HIGH_POWER_MODE )
 
#define XoscInLowPowerMode   ( XOSC_IN_LOW_POWER_MODE )
 
#define RSTSRC_PWR_ON   (( AON_SYSCTL_RESETCTL_RESET_SRC_PWR_ON >> AON_SYSCTL_RESETCTL_RESET_SRC_S ))
 
#define RSTSRC_PIN_RESET   (( AON_SYSCTL_RESETCTL_RESET_SRC_PIN_RESET >> AON_SYSCTL_RESETCTL_RESET_SRC_S ))
 
#define RSTSRC_VDDS_LOSS   (( AON_SYSCTL_RESETCTL_RESET_SRC_VDDS_LOSS >> AON_SYSCTL_RESETCTL_RESET_SRC_S ))
 
#define RSTSRC_VDD_LOSS   (( AON_SYSCTL_RESETCTL_RESET_SRC_VDD_LOSS >> AON_SYSCTL_RESETCTL_RESET_SRC_S ))
 
#define RSTSRC_VDDR_LOSS   (( AON_SYSCTL_RESETCTL_RESET_SRC_VDDR_LOSS >> AON_SYSCTL_RESETCTL_RESET_SRC_S ))
 
#define RSTSRC_CLK_LOSS   (( AON_SYSCTL_RESETCTL_RESET_SRC_CLK_LOSS >> AON_SYSCTL_RESETCTL_RESET_SRC_S ))
 
#define RSTSRC_SYSRESET   (( AON_SYSCTL_RESETCTL_RESET_SRC_SYSRESET >> AON_SYSCTL_RESETCTL_RESET_SRC_S ))
 
#define RSTSRC_WARMRESET   (( AON_SYSCTL_RESETCTL_RESET_SRC_WARMRESET >> AON_SYSCTL_RESETCTL_RESET_SRC_S ))
 
#define RSTSRC_WAKEUP_FROM_SHUTDOWN   (( AON_SYSCTL_RESETCTL_RESET_SRC_M >> AON_SYSCTL_RESETCTL_RESET_SRC_S ) + 1 )
 

Functions

void SysCtrlPowerEverything (void)
 Power up everything. More...
 
void SysCtrlStandby (void)
 Force the system into standby mode. More...
 
void SysCtrlPowerdown (void)
 Force the system into power down. More...
 
void SysCtrlShutdown (void)
 Force the system into shutdown. More...
 
static uint32_t SysCtrlClockGet (void)
 Get the CPU core clock frequency. More...
 
static void SysCtrlAonSync (void)
 Sync all accesses to the AON register interface. More...
 
static void SysCtrlAonUpdate (void)
 Update all interfaces to AON. More...
 
void SysCtrlSetRechargeBeforePowerDown (uint32_t xoscPowerMode)
 Set Recharge values before entering Power Down. More...
 
void SysCtrlAdjustRechargeAfterPowerDown (void)
 Adjust Recharge calculations to be used next. More...
 
void SysCtrl_DCDC_VoltageConditionalControl (void)
 Turns DCDC on or off depending of what is considered to be optimal usage. More...
 
uint32_t SysCtrlResetSourceGet (void)
 Returns last reset source (including "wakeup from shutdown"). More...
 
static void SysCtrlSystemReset (void)
 Perform a full system reset. More...