CC13xx Driver Library
rfc_CMD_TX_TEST_s Struct Reference

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0808. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips if the rule involves skipping. More...
 
condition
 
struct {
   uint8_t   bUseCw:1
 0: Send modulated signal
1: Send continuous wave More...
 
   uint8_t   bFsOff:1
 0: Keep frequency synth on after command
1: Turn frequency synth off after command More...
 
   uint8_t   whitenMode:2
 0: No whitening
1: Default whitening
2: PRBS-15
3: PRBS-32 More...
 
config
 
uint8_t __dummy0
 
uint16_t txWord
 Value to send to the modem before whitening. More...
 
uint8_t __dummy1
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
endTrigger
 Trigger classifier for ending the operation. More...
 
uint32_t syncWord
 Sync word to use for transmitter. More...
 
ratmr_t endTime
 Time to end the operation. More...
 

Detailed Description

Definition at line 445 of file rf_common_cmd.h.

Field Documentation

uint8_t rfc_CMD_TX_TEST_s::__dummy0

Definition at line 474 of file rf_common_cmd.h.

uint8_t rfc_CMD_TX_TEST_s::__dummy1

Definition at line 476 of file rf_common_cmd.h.

uint8_t rfc_CMD_TX_TEST_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

Definition at line 454 of file rf_common_cmd.h.

uint8_t rfc_CMD_TX_TEST_s::bFsOff

0: Keep frequency synth on after command
1: Turn frequency synth off after command

Definition at line 467 of file rf_common_cmd.h.

uint8_t rfc_CMD_TX_TEST_s::bUseCw

0: Send modulated signal
1: Send continuous wave

Definition at line 465 of file rf_common_cmd.h.

uint16_t rfc_CMD_TX_TEST_s::commandNo

The command ID number 0x0808.

Definition at line 446 of file rf_common_cmd.h.

struct { ... } rfc_CMD_TX_TEST_s::condition
struct { ... } rfc_CMD_TX_TEST_s::config
ratmr_t rfc_CMD_TX_TEST_s::endTime

Time to end the operation.

Definition at line 486 of file rf_common_cmd.h.

struct { ... } rfc_CMD_TX_TEST_s::endTrigger

Trigger classifier for ending the operation.

uint8_t rfc_CMD_TX_TEST_s::nSkip

Number of skips if the rule involves skipping.

Definition at line 462 of file rf_common_cmd.h.

uint8_t rfc_CMD_TX_TEST_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

Definition at line 457 of file rf_common_cmd.h.

rfc_radioOp_t* rfc_CMD_TX_TEST_s::pNextOp

Pointer to the next operation to run after this operation is done.

Definition at line 450 of file rf_common_cmd.h.

uint8_t rfc_CMD_TX_TEST_s::rule

Condition for running next command: Rule for how to proceed.

Definition at line 461 of file rf_common_cmd.h.

ratmr_t rfc_CMD_TX_TEST_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

Definition at line 451 of file rf_common_cmd.h.

struct { ... } rfc_CMD_TX_TEST_s::startTrigger

Identification of the trigger that starts the operation.

uint16_t rfc_CMD_TX_TEST_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

Definition at line 447 of file rf_common_cmd.h.

uint32_t rfc_CMD_TX_TEST_s::syncWord

Sync word to use for transmitter.

Definition at line 485 of file rf_common_cmd.h.

uint8_t rfc_CMD_TX_TEST_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

Definition at line 456 of file rf_common_cmd.h.

uint8_t rfc_CMD_TX_TEST_s::triggerType

The type of trigger.

Definition at line 453 of file rf_common_cmd.h.

uint16_t rfc_CMD_TX_TEST_s::txWord

Value to send to the modem before whitening.

Definition at line 475 of file rf_common_cmd.h.

uint8_t rfc_CMD_TX_TEST_s::whitenMode

0: No whitening
1: Default whitening
2: PRBS-15
3: PRBS-32

Definition at line 469 of file rf_common_cmd.h.