CC13xx Driver Library
rfc_CMD_TX_POWER_BOOST_s Struct Reference

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0816. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips if the rule involves skipping. More...
 
condition
 
uint8_t vddrLevel
 VDDR level to set
0xFD: Trim VDDR voltage to normal level (VDDR_TRIM), nominally 1.68 V
0xFE: Trim VDDR voltage to high level (VDDR_TRIM_H), nominally 1.85 V
0xFF: Trim VDDR voltage to higher level (VDDR_TRIM_HH), nominally 1.95 V
Other: reserved. More...
 
uint8_t paTrimValue
 Optional power amplifier trim setting manipulation
0x00-0x1F: Value to write in ADI_0_RF:PACTL0.TRIM register field
0xFE: Set PACTL0.TRIM to its default value from FCFG1
0xFF: Do not write PACTL0.TRIM, use the setting that is already applied
More...
 

Detailed Description

Definition at line 738 of file rf_common_cmd.h.

Field Documentation

uint8_t rfc_CMD_TX_POWER_BOOST_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

Definition at line 747 of file rf_common_cmd.h.

uint16_t rfc_CMD_TX_POWER_BOOST_s::commandNo

The command ID number 0x0816.

Definition at line 739 of file rf_common_cmd.h.

struct { ... } rfc_CMD_TX_POWER_BOOST_s::condition
uint8_t rfc_CMD_TX_POWER_BOOST_s::nSkip

Number of skips if the rule involves skipping.

Definition at line 755 of file rf_common_cmd.h.

uint8_t rfc_CMD_TX_POWER_BOOST_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

Definition at line 750 of file rf_common_cmd.h.

uint8_t rfc_CMD_TX_POWER_BOOST_s::paTrimValue

Optional power amplifier trim setting manipulation
0x00-0x1F: Value to write in ADI_0_RF:PACTL0.TRIM register field
0xFE: Set PACTL0.TRIM to its default value from FCFG1
0xFF: Do not write PACTL0.TRIM, use the setting that is already applied

Definition at line 762 of file rf_common_cmd.h.

rfc_radioOp_t* rfc_CMD_TX_POWER_BOOST_s::pNextOp

Pointer to the next operation to run after this operation is done.

Definition at line 743 of file rf_common_cmd.h.

uint8_t rfc_CMD_TX_POWER_BOOST_s::rule

Condition for running next command: Rule for how to proceed.

Definition at line 754 of file rf_common_cmd.h.

ratmr_t rfc_CMD_TX_POWER_BOOST_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

Definition at line 744 of file rf_common_cmd.h.

struct { ... } rfc_CMD_TX_POWER_BOOST_s::startTrigger

Identification of the trigger that starts the operation.

uint16_t rfc_CMD_TX_POWER_BOOST_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

Definition at line 740 of file rf_common_cmd.h.

uint8_t rfc_CMD_TX_POWER_BOOST_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

Definition at line 749 of file rf_common_cmd.h.

uint8_t rfc_CMD_TX_POWER_BOOST_s::triggerType

The type of trigger.

Definition at line 746 of file rf_common_cmd.h.

uint8_t rfc_CMD_TX_POWER_BOOST_s::vddrLevel

VDDR level to set
0xFD: Trim VDDR voltage to normal level (VDDR_TRIM), nominally 1.68 V
0xFE: Trim VDDR voltage to high level (VDDR_TRIM_H), nominally 1.85 V
0xFF: Trim VDDR voltage to higher level (VDDR_TRIM_HH), nominally 1.95 V
Other: reserved.

Definition at line 757 of file rf_common_cmd.h.