CC13xx Driver Library
rfc_CMD_RADIO_SETUP_s Struct Reference

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0802. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips if the rule involves skipping. More...
 
condition
 
uint8_t mode
 The main mode to use
0x00: BLE
0x01: IEEE 802.15.4
0x02: 2 Mbps GFSK
0x05: 5 Mbps coded 8-FSK
0x06: ANT
0xFF: Keep existing mode; update overrides only
Others: Reserved More...
 
uint8_t loDivider
 LO divider setting to use. Supported values: 0 (equivalent to 2), 2, 5, 6, 10, 12, 15, and 30.
Value of 0 or 2 only supported for devices that support 2.4 GHz operation. More...
 
struct {
   uint16_t   frontEndMode:3
 0x00: Differential mode
0x01: Single-ended mode RFP
0x02: Single-ended mode RFN
0x05 Single-ended mode RFP with external frontend control on RF pins (RFN and RXTX)
0x06 Single-ended mode RFN with external frontend control on RF pins (RFP and RXTX)
Others: Reserved More...
 
   uint16_t   biasMode:1
 0: Internal bias
1: External bias More...
 
   uint16_t   __pad0__:6
 
   uint16_t   bNoFsPowerUp:1
 0: Power up frequency synth
1: Do not power up frequency synth More...
 
config
 Configuration options. More...
 
struct {
   uint16_t   IB:6
 Value to write to the PA power control field at 25 °C. More...
 
   uint16_t   GC:2
 Value to write to the gain control of the 1st stage of the PA. More...
 
   uint16_t   boost:1
 Value of boost bit in synth. More...
 
   uint16_t   tempCoeff:7
 Temperature coefficient for IB. 0: No temperature compensation. More...
 
txPower
 Transmit power. More...
 
uint32_t * pRegOverride
 Pointer to a list of hardware and configuration registers to override. If NULL, no override is used. More...
 

Detailed Description

Definition at line 165 of file rf_common_cmd.h.

Field Documentation

uint16_t rfc_CMD_RADIO_SETUP_s::__pad0__

Definition at line 204 of file rf_common_cmd.h.

uint8_t rfc_CMD_RADIO_SETUP_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

Definition at line 174 of file rf_common_cmd.h.

uint16_t rfc_CMD_RADIO_SETUP_s::biasMode

0: Internal bias
1: External bias

Definition at line 202 of file rf_common_cmd.h.

uint16_t rfc_CMD_RADIO_SETUP_s::bNoFsPowerUp

0: Power up frequency synth
1: Do not power up frequency synth

Definition at line 205 of file rf_common_cmd.h.

uint16_t rfc_CMD_RADIO_SETUP_s::boost

Value of boost bit in synth.

Definition at line 211 of file rf_common_cmd.h.

uint16_t rfc_CMD_RADIO_SETUP_s::commandNo

The command ID number 0x0802.

Definition at line 166 of file rf_common_cmd.h.

struct { ... } rfc_CMD_RADIO_SETUP_s::condition
struct { ... } rfc_CMD_RADIO_SETUP_s::config

Configuration options.

uint16_t rfc_CMD_RADIO_SETUP_s::frontEndMode

0x00: Differential mode
0x01: Single-ended mode RFP
0x02: Single-ended mode RFN
0x05 Single-ended mode RFP with external frontend control on RF pins (RFN and RXTX)
0x06 Single-ended mode RFN with external frontend control on RF pins (RFP and RXTX)
Others: Reserved

Definition at line 196 of file rf_common_cmd.h.

uint16_t rfc_CMD_RADIO_SETUP_s::GC

Value to write to the gain control of the 1st stage of the PA.

Definition at line 210 of file rf_common_cmd.h.

uint16_t rfc_CMD_RADIO_SETUP_s::IB

Value to write to the PA power control field at 25 °C.

Definition at line 209 of file rf_common_cmd.h.

uint8_t rfc_CMD_RADIO_SETUP_s::loDivider

LO divider setting to use. Supported values: 0 (equivalent to 2), 2, 5, 6, 10, 12, 15, and 30.
Value of 0 or 2 only supported for devices that support 2.4 GHz operation.

Definition at line 192 of file rf_common_cmd.h.

uint8_t rfc_CMD_RADIO_SETUP_s::mode

The main mode to use
0x00: BLE
0x01: IEEE 802.15.4
0x02: 2 Mbps GFSK
0x05: 5 Mbps coded 8-FSK
0x06: ANT
0xFF: Keep existing mode; update overrides only
Others: Reserved

Definition at line 184 of file rf_common_cmd.h.

uint8_t rfc_CMD_RADIO_SETUP_s::nSkip

Number of skips if the rule involves skipping.

Definition at line 182 of file rf_common_cmd.h.

uint8_t rfc_CMD_RADIO_SETUP_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

Definition at line 177 of file rf_common_cmd.h.

rfc_radioOp_t* rfc_CMD_RADIO_SETUP_s::pNextOp

Pointer to the next operation to run after this operation is done.

Definition at line 170 of file rf_common_cmd.h.

uint32_t* rfc_CMD_RADIO_SETUP_s::pRegOverride

Pointer to a list of hardware and configuration registers to override. If NULL, no override is used.

Definition at line 214 of file rf_common_cmd.h.

uint8_t rfc_CMD_RADIO_SETUP_s::rule

Condition for running next command: Rule for how to proceed.

Definition at line 181 of file rf_common_cmd.h.

ratmr_t rfc_CMD_RADIO_SETUP_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

Definition at line 171 of file rf_common_cmd.h.

struct { ... } rfc_CMD_RADIO_SETUP_s::startTrigger

Identification of the trigger that starts the operation.

uint16_t rfc_CMD_RADIO_SETUP_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

Definition at line 167 of file rf_common_cmd.h.

uint16_t rfc_CMD_RADIO_SETUP_s::tempCoeff

Temperature coefficient for IB. 0: No temperature compensation.

Definition at line 212 of file rf_common_cmd.h.

uint8_t rfc_CMD_RADIO_SETUP_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

Definition at line 176 of file rf_common_cmd.h.

uint8_t rfc_CMD_RADIO_SETUP_s::triggerType

The type of trigger.

Definition at line 173 of file rf_common_cmd.h.

struct { ... } rfc_CMD_RADIO_SETUP_s::txPower

Transmit power.