CC13xx Driver Library
rfc_CMD_PROP_RX_ADV_s Struct Reference

#include <rf_prop_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x3804. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips if the rule involves skipping. More...
 
condition
 
struct {
   uint8_t   bFsOff:1
 0: Keep frequency synth on after command
1: Turn frequency synth off after command More...
 
   uint8_t   bRepeatOk:1
 0: End operation after receiving a packet correctly
1: Go back to sync search after receiving a packet correctly More...
 
   uint8_t   bRepeatNok:1
 0: End operation after receiving a packet with CRC error
1: Go back to sync search after receiving a packet with CRC error More...
 
   uint8_t   bUseCrc:1
 0: Do not check CRC
1: Check CRC More...
 
   uint8_t   bCrcIncSw:1
 0: Do not include sync word in CRC calculation
1: Include sync word in CRC calculation More...
 
   uint8_t   bCrcIncHdr:1
 0: Do not include header in CRC calculation
1: Include header in CRC calculation More...
 
   uint8_t   endType:1
 0: Packet is received to the end if end trigger happens after sync is obtained
1: Packet reception is stopped if end trigger happens More...
 
   uint8_t   filterOp:1
 0: Stop receiver and restart sync search on address mismatch
1: Receive packet and mark it as ignored on address mismatch More...
 
pktConf
 
struct {
   uint8_t   bAutoFlushIgnored:1
 If 1, automatically discard ignored packets from Rx queue. More...
 
   uint8_t   bAutoFlushCrcErr:1
 If 1, automatically discard packets with CRC error from Rx queue. More...
 
   uint8_t   __pad0__:1
 
   uint8_t   bIncludeHdr:1
 If 1, include the received header or length byte in the stored packet; otherwise discard it. More...
 
   uint8_t   bIncludeCrc:1
 If 1, include the received CRC field in the stored packet; otherwise discard it. More...
 
   uint8_t   bAppendRssi:1
 If 1, append an RSSI byte to the packet in the Rx queue. More...
 
   uint8_t   bAppendTimestamp:1
 If 1, append a timestamp to the packet in the Rx queue. More...
 
   uint8_t   bAppendStatus:1
 If 1, append a status byte to the packet in the Rx queue. More...
 
rxConf
 Rx configuration. More...
 
uint32_t syncWord0
 Sync word to listen for. More...
 
uint32_t syncWord1
 Alternative sync word if non-zero. More...
 
uint16_t maxPktLen
 Packet length for fixed length, maximum packet length for variable length
0: Unlimited or unknown length. More...
 
struct {
   uint16_t   numHdrBits:6
 Number of bits in header (0–32) More...
 
   uint16_t   lenPos:5
 Position of length field in header (0–31) More...
 
   uint16_t   numLenBits:5
 Number of bits in length field (0–16) More...
 
hdrConf
 
struct {
   uint16_t   addrType:1
 0: Address after header
1: Address in header More...
 
   uint16_t   addrSize:5
 If addrType = 0: Address size in bytes
If addrType = 1: Address size in bits. More...
 
   uint16_t   addrPos:5
 If addrType = 1: Bit position of address in header
If addrType = 0: Non-zero to extend address with sync word identifier. More...
 
   uint16_t   numAddr:5
 Number of addresses in address list. More...
 
addrConf
 
int8_t lenOffset
 Signed value to add to length field. More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
endTrigger
 Trigger classifier for ending the operation. More...
 
ratmr_t endTime
 Time used together with endTrigger for ending the operation. More...
 
uint8_t * pAddr
 Pointer to address list. More...
 
dataQueue_tpQueue
 Pointer to receive queue. More...
 
uint8_t * pOutput
 Pointer to output structure. More...
 

Detailed Description

Definition at line 288 of file rf_prop_cmd.h.

Field Documentation

uint8_t rfc_CMD_PROP_RX_ADV_s::__pad0__

Definition at line 328 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_RX_ADV_s::addrConf
uint16_t rfc_CMD_PROP_RX_ADV_s::addrPos

If addrType = 1: Bit position of address in header
If addrType = 0: Non-zero to extend address with sync word identifier.

Definition at line 349 of file rf_prop_cmd.h.

uint16_t rfc_CMD_PROP_RX_ADV_s::addrSize

If addrType = 0: Address size in bytes
If addrType = 1: Address size in bits.

Definition at line 347 of file rf_prop_cmd.h.

uint16_t rfc_CMD_PROP_RX_ADV_s::addrType

0: Address after header
1: Address in header

Definition at line 345 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::bAppendRssi

If 1, append an RSSI byte to the packet in the Rx queue.

Definition at line 331 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::bAppendStatus

If 1, append a status byte to the packet in the Rx queue.

Definition at line 333 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::bAppendTimestamp

If 1, append a timestamp to the packet in the Rx queue.

Definition at line 332 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::bAutoFlushCrcErr

If 1, automatically discard packets with CRC error from Rx queue.

Definition at line 327 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::bAutoFlushIgnored

If 1, automatically discard ignored packets from Rx queue.

Definition at line 326 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::bCrcIncHdr

0: Do not include header in CRC calculation
1: Include header in CRC calculation

Definition at line 318 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::bCrcIncSw

0: Do not include sync word in CRC calculation
1: Include sync word in CRC calculation

Definition at line 316 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

Definition at line 297 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::bFsOff

0: Keep frequency synth on after command
1: Turn frequency synth off after command

Definition at line 308 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::bIncludeCrc

If 1, include the received CRC field in the stored packet; otherwise discard it.

Definition at line 330 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::bIncludeHdr

If 1, include the received header or length byte in the stored packet; otherwise discard it.

Definition at line 329 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::bRepeatNok

0: End operation after receiving a packet with CRC error
1: Go back to sync search after receiving a packet with CRC error

Definition at line 312 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::bRepeatOk

0: End operation after receiving a packet correctly
1: Go back to sync search after receiving a packet correctly

Definition at line 310 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::bUseCrc

0: Do not check CRC
1: Check CRC

Definition at line 314 of file rf_prop_cmd.h.

uint16_t rfc_CMD_PROP_RX_ADV_s::commandNo

The command ID number 0x3804.

Definition at line 289 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_RX_ADV_s::condition
ratmr_t rfc_CMD_PROP_RX_ADV_s::endTime

Time used together with endTrigger for ending the operation.

Definition at line 362 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_RX_ADV_s::endTrigger

Trigger classifier for ending the operation.

uint8_t rfc_CMD_PROP_RX_ADV_s::endType

0: Packet is received to the end if end trigger happens after sync is obtained
1: Packet reception is stopped if end trigger happens

Definition at line 320 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::filterOp

0: Stop receiver and restart sync search on address mismatch
1: Receive packet and mark it as ignored on address mismatch

Definition at line 322 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_RX_ADV_s::hdrConf
int8_t rfc_CMD_PROP_RX_ADV_s::lenOffset

Signed value to add to length field.

Definition at line 353 of file rf_prop_cmd.h.

uint16_t rfc_CMD_PROP_RX_ADV_s::lenPos

Position of length field in header (0–31)

Definition at line 341 of file rf_prop_cmd.h.

uint16_t rfc_CMD_PROP_RX_ADV_s::maxPktLen

Packet length for fixed length, maximum packet length for variable length
0: Unlimited or unknown length.

Definition at line 337 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::nSkip

Number of skips if the rule involves skipping.

Definition at line 305 of file rf_prop_cmd.h.

uint16_t rfc_CMD_PROP_RX_ADV_s::numAddr

Number of addresses in address list.

Definition at line 351 of file rf_prop_cmd.h.

uint16_t rfc_CMD_PROP_RX_ADV_s::numHdrBits

Number of bits in header (0–32)

Definition at line 340 of file rf_prop_cmd.h.

uint16_t rfc_CMD_PROP_RX_ADV_s::numLenBits

Number of bits in length field (0–16)

Definition at line 342 of file rf_prop_cmd.h.

uint8_t* rfc_CMD_PROP_RX_ADV_s::pAddr

Pointer to address list.

Definition at line 363 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

Definition at line 300 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_RX_ADV_s::pktConf
rfc_radioOp_t* rfc_CMD_PROP_RX_ADV_s::pNextOp

Pointer to the next operation to run after this operation is done.

Definition at line 293 of file rf_prop_cmd.h.

uint8_t* rfc_CMD_PROP_RX_ADV_s::pOutput

Pointer to output structure.

Definition at line 365 of file rf_prop_cmd.h.

dataQueue_t* rfc_CMD_PROP_RX_ADV_s::pQueue

Pointer to receive queue.

Definition at line 364 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::rule

Condition for running next command: Rule for how to proceed.

Definition at line 304 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_RX_ADV_s::rxConf

Rx configuration.

ratmr_t rfc_CMD_PROP_RX_ADV_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

Definition at line 294 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_RX_ADV_s::startTrigger

Identification of the trigger that starts the operation.

uint16_t rfc_CMD_PROP_RX_ADV_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

Definition at line 290 of file rf_prop_cmd.h.

uint32_t rfc_CMD_PROP_RX_ADV_s::syncWord0

Sync word to listen for.

Definition at line 335 of file rf_prop_cmd.h.

uint32_t rfc_CMD_PROP_RX_ADV_s::syncWord1

Alternative sync word if non-zero.

Definition at line 336 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

Definition at line 299 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_ADV_s::triggerType

The type of trigger.

Definition at line 296 of file rf_prop_cmd.h.