CC13xx Driver Library
rfc_CMD_PATTERN_CHECK_s Struct Reference

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0813. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips if the rule involves skipping. More...
 
condition
 
struct {
   uint16_t   operation:2
 Operation to perform
0: True if value == compareVal
1: True if value < compareVal
2: True if value > compareVal
3: Reserved More...
 
   uint16_t   bByteRev:1
 If 1, interchange the four bytes of the value, so that they are read most-significant-byte-first. More...
 
   uint16_t   bBitRev:1
 If 1, perform bit reversal of the value. More...
 
   uint16_t   signExtend:5
 0: Treat value and compareVal as unsigned
1–31: Treat value and compareVal as signed, where the value gives the number of the most significant bit in the signed number. More...
 
   uint16_t   bRxVal:1
 0: Use pValue as a pointer
1: Use pValue as a signed offset to the start of the last committed Rx entry element More...
 
patternOpt
 Options for comparison. More...
 
rfc_radioOp_tpNextOpIfOk
 Pointer to next operation if comparison result was true. More...
 
uint8_t * pValue
 Pointer to read from, or offset from last Rx entry if patternOpt.bRxVal == 1. More...
 
uint32_t mask
 Bit mask to apply before comparison. More...
 
uint32_t compareVal
 Value to compare to. More...
 

Detailed Description

Definition at line 692 of file rf_common_cmd.h.

Field Documentation

uint16_t rfc_CMD_PATTERN_CHECK_s::bBitRev

If 1, perform bit reversal of the value.

Definition at line 719 of file rf_common_cmd.h.

uint16_t rfc_CMD_PATTERN_CHECK_s::bByteRev

If 1, interchange the four bytes of the value, so that they are read most-significant-byte-first.

Definition at line 717 of file rf_common_cmd.h.

uint8_t rfc_CMD_PATTERN_CHECK_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

Definition at line 701 of file rf_common_cmd.h.

uint16_t rfc_CMD_PATTERN_CHECK_s::bRxVal

0: Use pValue as a pointer
1: Use pValue as a signed offset to the start of the last committed Rx entry element

Definition at line 723 of file rf_common_cmd.h.

uint16_t rfc_CMD_PATTERN_CHECK_s::commandNo

The command ID number 0x0813.

Definition at line 693 of file rf_common_cmd.h.

uint32_t rfc_CMD_PATTERN_CHECK_s::compareVal

Value to compare to.

Definition at line 730 of file rf_common_cmd.h.

struct { ... } rfc_CMD_PATTERN_CHECK_s::condition
uint32_t rfc_CMD_PATTERN_CHECK_s::mask

Bit mask to apply before comparison.

Definition at line 729 of file rf_common_cmd.h.

uint8_t rfc_CMD_PATTERN_CHECK_s::nSkip

Number of skips if the rule involves skipping.

Definition at line 709 of file rf_common_cmd.h.

uint16_t rfc_CMD_PATTERN_CHECK_s::operation

Operation to perform
0: True if value == compareVal
1: True if value < compareVal
2: True if value > compareVal
3: Reserved

Definition at line 712 of file rf_common_cmd.h.

uint8_t rfc_CMD_PATTERN_CHECK_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

Definition at line 704 of file rf_common_cmd.h.

struct { ... } rfc_CMD_PATTERN_CHECK_s::patternOpt

Options for comparison.

rfc_radioOp_t* rfc_CMD_PATTERN_CHECK_s::pNextOp

Pointer to the next operation to run after this operation is done.

Definition at line 697 of file rf_common_cmd.h.

rfc_radioOp_t* rfc_CMD_PATTERN_CHECK_s::pNextOpIfOk

Pointer to next operation if comparison result was true.

Definition at line 727 of file rf_common_cmd.h.

uint8_t* rfc_CMD_PATTERN_CHECK_s::pValue

Pointer to read from, or offset from last Rx entry if patternOpt.bRxVal == 1.

Definition at line 728 of file rf_common_cmd.h.

uint8_t rfc_CMD_PATTERN_CHECK_s::rule

Condition for running next command: Rule for how to proceed.

Definition at line 708 of file rf_common_cmd.h.

uint16_t rfc_CMD_PATTERN_CHECK_s::signExtend

0: Treat value and compareVal as unsigned
1–31: Treat value and compareVal as signed, where the value gives the number of the most significant bit in the signed number.

Definition at line 720 of file rf_common_cmd.h.

ratmr_t rfc_CMD_PATTERN_CHECK_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

Definition at line 698 of file rf_common_cmd.h.

struct { ... } rfc_CMD_PATTERN_CHECK_s::startTrigger

Identification of the trigger that starts the operation.

uint16_t rfc_CMD_PATTERN_CHECK_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

Definition at line 694 of file rf_common_cmd.h.

uint8_t rfc_CMD_PATTERN_CHECK_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

Definition at line 703 of file rf_common_cmd.h.

uint8_t rfc_CMD_PATTERN_CHECK_s::triggerType

The type of trigger.

Definition at line 700 of file rf_common_cmd.h.