#include <rf_common_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x0008. More... | |
uint16_t | __dummy0 |
dataQueue_t * | pQueue |
Pointer to the queue structure to be cleared. More... | |
Definition at line 888 of file rf_common_cmd.h.
uint16_t rfc_CMD_CLEAR_RX_s::__dummy0 |
Definition at line 890 of file rf_common_cmd.h.
uint16_t rfc_CMD_CLEAR_RX_s::commandNo |
The command ID number 0x0008.
Definition at line 889 of file rf_common_cmd.h.
dataQueue_t* rfc_CMD_CLEAR_RX_s::pQueue |
Pointer to the queue structure to be cleared.
Definition at line 891 of file rf_common_cmd.h.