module ti.sysbios.family.arm.arm9.Mmu

Memory Management Unit Manager

This module allows the ARM processor to map a virtual address to a different physical address and enable/disable the MMU. It does this through a translation table in memory. The translation table is 16KB and manages only the first level descriptor table. Each entry in the table defines the properties of memory areas of size 1MB. These properties include memory access permissions, cacheability, bufferability, and domain access. [ more ... ]
C synopsis target-domain sourced in ti/sysbios/family/arm/arm9/Mmu.xdc
DETAILS
This module allows the ARM processor to map a virtual address to a different physical address and enable/disable the MMU. It does this through a translation table in memory. The translation table is 16KB and manages only the first level descriptor table. Each entry in the table defines the properties of memory areas of size 1MB. These properties include memory access permissions, cacheability, bufferability, and domain access.
By default, the MMU translation table contains cache-enabled entries for every memory segment from the platform. Cache-disabled entries are added the peripheral addresses used by SYS/BIOS (i.e. Timers, Interrupt controller). The translation table is placed in an output section called "ti.sysbios.family.arm.arm9.mmuTableSection". This section is placed into the platform's default dataMemory and in order to minimize object file size, specified to not be initialized via the "NOINIT" type. If cacheable is true and bufferable is true, L1 data cache operates as a write-back cache. If cacheable is true but bufferable is false, L1 data cache operates as a write-through cache.
This module does not manage the second level descriptor tables. A 'SECTION' mapped access requires only a first level fetch. In this case, there is no need for a second level descriptor table. A 'COARSE' or 'FINE' mapped access requires a second level descriptor table which can be supplied by the user.
Note: There are size and alignment requirements on the second level descriptor tables depending on the page size. See the ARM Architecture Reference Manual for more info.
The following is an example of how to place the MMU table and how to enable L1 data caching for the address range 0xC3000000-0xC4000000 in the *.cfg file:
    var Cache = xdc.useModule('ti.sysbios.family.arm.arm9.Cache');
    var Mmu = xdc.useModule('ti.sysbios.family.arm.arm9.Mmu');

    // Enable the cache
    Cache.enableCache = true;

    // Enable the MMU (Required for L1 data caching)
    Mmu.enableMMU = true;

    // descriptor attribute structure
    var attrs = {
        type: Mmu.FirstLevelDesc_SECTION,  // SECTION descriptor
        bufferable: true,                  // bufferable
        cacheable: true,                   // cacheable
        imp: 1,                            // implementation defined
        domain: 0,                         // domain between 0-15
        accPerm: 3,                        // read/write permission
    };

    // Set the descriptor for each entry in the address range
    for (var i=0xC3000000; i < 0xC4000000; i = i + 0x00100000) {
        // Each 'SECTION' descriptor entry spans a 1MB address range
        Mmu.setFirstLevelDescMeta(i, i, attrs);
    }

    var memmap = Program.cpu.memoryMap;
    var DDR = null;

    // Find DDR in memory map
    for (var i=0; i < memmap.length; i++) {
        if (memmap[i].name == "DDR") {
            DDR = memmap[i];
        }
    }

    // Place the MMU table in the DDR memory segment if it exists
    if (DDR != null) {
        var sectionName = "ti.sysbios.family.arm.arm9.mmuTableSection";
        Program.sectMap[sectionName] = new Program.SectionSpec();
        Program.sectMap[sectionName].type = "NOINIT";
        Program.sectMap[sectionName].loadSegment = "DDR";
    }
    else {
        print("No DDR memory segment was found");
    }

The following is an example of using a second level descriptor to specify a 4KB block of memory. The first level descriptor is specified as a COARSE page table. The second level descriptors are specified as a small page, cacheable, and bufferable for the addresses 0xFFFEE000-0xFFFF0000. This code is be placed in main() in the *.c file. The MMU should not be enabled prior to initializing the second level descriptors.
    #define MMU_LEVEL2DESC_SMALLPAGE    0x2
    #define MMU_LEVEL2DESC_BUFFERABLE   0x4
    #define MMU_LEVEL2DESC_CACHEABLE    0x8

    #pragma DATA_ALIGN(mmuL2Table, 4096);    // align to 4KB

    UInt32 mmuL2Table[256];   // each level 2 descriptor specifies a 4KB block

    Void main(Int argc, Char * argv[])
    {
        Mmu_FirstLevelDescAttrs attrs;
        Int i;

        // initialize the second level descriptors
        for (i=0; i < 256; i++) {
             mmuL2Table[i] = 0;
        }

        // change the address starting at 0xFFFEE000 to be a small page
        mmuL2Table[0xEE] = 0xFFFEE000 | // set the physical address
            MMU_LEVEL2DESC_SMALLPAGE |  // set descriptor to small page (4KB)
            0xFF0;                      // set Access Permission bits to 1

        // change the address starting at 0xFFFEF000 to be a small page
        mmuL2Table[0xEF] = 0xFFFEF000 | // set the physical address
            MMU_LEVEL2DESC_SMALLPAGE |  // set descriptor to small page (4KB)
            0xFF0;                      // set Access Permission bits to 1

        // change the address starting at 0xFFFF0000 to be a small page
        mmuL2Table[0xF0] = 0xFFFF0000 | // set the physical address
            MMU_LEVEL2DESC_SMALLPAGE |  // set descriptor to small page (4KB)
            MMU_LEVEL2DESC_CACHEABLE |  // set cacheable bit to true
            MMU_LEVEL2DESC_BUFFERABLE | // set bufferable bit to true
            0xFF0;                      // set Access Permission bits to 1

        // first level descriptor properties
        attrs.type = Mmu_FirstLevelDesc_COARSE; // set to a coarse descriptor
        attrs.imp = 1;                          // defined to be 1 for ARM9
        attrs.domain = 0;                       // set domain to 0

        // Set the first level descriptor for the virtual address 0xFFFF0000.
        Mmu_setFirstLevelDesc((Ptr)0xFFFF0000, &mmuL2Table, &attrs);

        // enable MMU
        Mmu_enable();

        BIOS_start();
    }

 
enum Mmu_FirstLevelDesc

First Level descriptors

C synopsis target-domain
typedef enum Mmu_FirstLevelDesc {
    Mmu_FirstLevelDesc_FAULT,
    // Virtual address is unmapped
    Mmu_FirstLevelDesc_COARSE,
    // Coarse page table descriptor
    Mmu_FirstLevelDesc_SECTION,
    // Section descriptor
    Mmu_FirstLevelDesc_FINE
    // Fine page table descriptor
} Mmu_FirstLevelDesc;
 
 
struct Mmu_FirstLevelDescAttrs

Structure for setting first level descriptor entries

C synopsis target-domain
typedef struct Mmu_FirstLevelDescAttrs {
    Mmu_FirstLevelDesc type;
    // first level descriptor type
    Bool bufferable;
    // is memory section bufferable
    Bool cacheable;
    // is memory section cacheable
    UInt8 imp;
    // implementation defined
    UInt8 domain;
    // domain access control value 0-15
    UInt8 accPerm;
    // access permission bits value 0-3
} Mmu_FirstLevelDescAttrs;
 
DETAILS
See the 'Translation Tables' section of the ARM Architecture Reference Manual for details
 
config Mmu_A_nullPointer  // module-wide

Assert raised when a pointer is null

C synopsis target-domain
extern const Assert_Id Mmu_A_nullPointer;
 
 
config Mmu_A_unknownDescType  // module-wide

Assert raised when the descriptor type is not recognized

C synopsis target-domain
extern const Assert_Id Mmu_A_unknownDescType;
 
 
config Mmu_defaultAttrs  // module-wide

default descriptor attributes structure

C synopsis target-domain
extern const Mmu_FirstLevelDescAttrs Mmu_defaultAttrs;
 
 
config Mmu_enableMMU  // module-wide

Configuration parameter to enable MMU

C synopsis target-domain
extern const Bool Mmu_enableMMU;
 
 
Mmu_disable()  // module-wide

Disables the MMU

C synopsis target-domain
Void Mmu_disable();
 
DETAILS
If the MMU is already disabled, then simply return. Otherwise this function does the following: If the L1 data cache is enabled, write back invalidate all of L1 data cache. If the L1 program cache is enabled, invalidate all of L1 program cache. This function does not change the cache L1 data/program settings.
 
Mmu_enable()  // module-wide

Enables the MMU

C synopsis target-domain
Void Mmu_enable();
 
DETAILS
If the MMU is already enabled, then simply return. Otherwise this function does the following: If the L1 program cache is enabled, invalidate all of L1 program cache. This function does not change the L1 data/program cache settings.
 
Mmu_initDescAttrs()  // module-wide

Initializes the first level descriptor attribute structure

C synopsis target-domain
Void Mmu_initDescAttrs(Mmu_FirstLevelDescAttrs *attrs);
 
ARGUMENTS
attrs — Pointer to first level descriptor attribute struct
 
Mmu_isEnabled()  // module-wide

Determines if the MMU is enabled

C synopsis target-domain
Bool Mmu_isEnabled();
 
 
Mmu_setFirstLevelDesc()  // module-wide

Sets the descriptor for the virtual address

C synopsis target-domain
Void Mmu_setFirstLevelDesc(Ptr virtualAddr, Ptr phyAddr, Mmu_FirstLevelDescAttrs *attrs);
 
ARGUMENTS
virtualAddr — The modified virtual address
phyAddr — The physical address
attrs — Pointer to first level descriptor attribute struct
DETAILS
The first level table entry for the virtual address is mapped to the physical address with the attributes specified. The descriptor table is effective when the MMU is enabled.
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId Mmu_Module_id();
// Get this module's unique id
 
Bool Mmu_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle Mmu_Module_heap();
// The heap from which this module allocates memory
 
Bool Mmu_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 Mmu_Module_getMask();
// Returns the diagnostics mask for this module
 
Void Mmu_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/sysbios/family/arm/arm9/Mmu.xdc
var Mmu = xdc.useModule('ti.sysbios.family.arm.arm9.Mmu');
module-wide constants & types
 
        obj.bufferable// is memory section bufferable = Bool  ...
        obj.cacheable// is memory section cacheable = Bool  ...
        obj.imp// implementation defined = UInt8  ...
        obj.domain// domain access control value 0-15 = UInt8  ...
        obj.accPerm// access permission bits value 0-3 = UInt8  ...
module-wide config parameters
        msg: "A_nullPointer: Pointer is null"
    };
        msg: "A_unknownDescType: Descriptor type is not recognized"
    };
        type: Mmu.FirstLevelDesc_SECTION,
        bufferable: false,
        cacheable: false,
        imp: 1,
        domain: 0,
        accPerm: 3
    };
 
module-wide functions
 
 
enum Mmu.FirstLevelDesc

First Level descriptors

Configuration settings
values of type Mmu.FirstLevelDesc
    const Mmu.FirstLevelDesc_FAULT;
    // Virtual address is unmapped
    const Mmu.FirstLevelDesc_COARSE;
    // Coarse page table descriptor
    const Mmu.FirstLevelDesc_SECTION;
    // Section descriptor
    const Mmu.FirstLevelDesc_FINE;
    // Fine page table descriptor
 
C SYNOPSIS
 
struct Mmu.FirstLevelDescAttrs

Structure for setting first level descriptor entries

Configuration settings
var obj = new Mmu.FirstLevelDescAttrs;
 
    obj.type = Mmu.FirstLevelDesc  ...
    // first level descriptor type
    obj.bufferable = Bool  ...
    // is memory section bufferable
    obj.cacheable = Bool  ...
    // is memory section cacheable
    obj.imp = UInt8  ...
    // implementation defined
    obj.domain = UInt8  ...
    // domain access control value 0-15
    obj.accPerm = UInt8  ...
    // access permission bits value 0-3
 
DETAILS
See the 'Translation Tables' section of the ARM Architecture Reference Manual for details
C SYNOPSIS
 
config Mmu.A_nullPointer  // module-wide

Assert raised when a pointer is null

Configuration settings
Mmu.A_nullPointer = Assert.Desc {
    msg: "A_nullPointer: Pointer is null"
};
 
C SYNOPSIS
 
config Mmu.A_unknownDescType  // module-wide

Assert raised when the descriptor type is not recognized

Configuration settings
Mmu.A_unknownDescType = Assert.Desc {
    msg: "A_unknownDescType: Descriptor type is not recognized"
};
 
C SYNOPSIS
 
config Mmu.defaultAttrs  // module-wide

default descriptor attributes structure

Configuration settings
Mmu.defaultAttrs = Mmu.FirstLevelDescAttrs {
    bufferable: false,
    cacheable: false,
    imp: 1,
    domain: 0,
    accPerm: 3
};
 
C SYNOPSIS
 
config Mmu.enableMMU  // module-wide

Configuration parameter to enable MMU

Configuration settings
Mmu.enableMMU = Bool true;
 
C SYNOPSIS
 
metaonly config Mmu.cachePlatformMemory  // module-wide

Flag to automatically mark platform's code/data/stack memory as cacheable in MMU descriptor table

Configuration settings
Mmu.cachePlatformMemory = Bool true;
 
DETAILS
By default, all memory regions defined in the platform an application is built with are marked as cacheable.
If manual configuration of memory regions is required, set this config parameter to 'false'.
SEE
 
metaonly config Mmu.common$  // module-wide

Common module configuration parameters

Configuration settings
Mmu.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
metaonly config Mmu.rovViewInfo  // module-wide
Configuration settings
Mmu.rovViewInfo = ViewInfo.Instance ViewInfo.create;
 
 
metaonly Mmu.setFirstLevelDescMeta()  // module-wide

Statically sets the descriptor for the virtual address

Configuration settings
Mmu.setFirstLevelDescMeta(Ptr virtualAddr, Ptr phyAddr, Mmu.FirstLevelDescAttrs attrs) returns Void
 
ARGUMENTS
virtualAddr — The modified virtual address
phyAddr — The physical address
attrs — Pointer to first level descriptor attribute struct
DETAILS
The first level table entry for the virtual address is mapped to the physical address with the attributes specified. The descriptor table is effective when the MMU is enabled.
generated on Tue, 18 Aug 2015 20:38:40 GMT