![]() |
![]() |
TI-RTOS for SimpleLink Wireless MCUs
2.14.02.22
|
SDSPIMSP432 Hardware attributes. More...
#include <SDSPIMSP432.h>
Data Fields | |
uint32_t | baseAddr |
uint8_t | clockSource |
uint8_t | portSCK |
uint16_t | pinSCK |
uint8_t | sckMode |
uint8_t | portMISO |
uint16_t | pinMISO |
uint8_t | misoMode |
uint8_t | portMOSI |
uint16_t | pinMOSI |
uint8_t | mosiMode |
uint8_t | portCS |
uint16_t | pinCS |
SDSPIMSP432 Hardware attributes.
The SDSPIMSP432 HWAttrs configuration structure contains SPI peripheral and GPIO Pin details required by the SDSPIMSP432 driver implementation.
The SDSPIMSP432 driver uses this information to:
These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For TivaWare these definitions are found in:
An example configuration structure could look as the following:
uint32_t SDSPIMSP432_HWAttrs::baseAddr |
SPI Peripheral's base address
uint8_t SDSPIMSP432_HWAttrs::clockSource |
SPIUSCI Clock source
uint8_t SDSPIMSP432_HWAttrs::portSCK |
SPI port for the SCK pin
uint16_t SDSPIMSP432_HWAttrs::pinSCK |
SPI SCK pin
uint8_t SDSPIMSP432_HWAttrs::sckMode |
GPIO mode to enable SCK pin
uint8_t SDSPIMSP432_HWAttrs::portMISO |
SPI port for the MISO pin
uint16_t SDSPIMSP432_HWAttrs::pinMISO |
SPI MISO pin
uint8_t SDSPIMSP432_HWAttrs::misoMode |
GPIO mode to enable MISO pin
uint8_t SDSPIMSP432_HWAttrs::portMOSI |
SPI port for the MOSI pin
uint16_t SDSPIMSP432_HWAttrs::pinMOSI |
SPI MOSI pin
uint8_t SDSPIMSP432_HWAttrs::mosiMode |
GPIO mode to enable MOSI pin
uint8_t SDSPIMSP432_HWAttrs::portCS |
GPIO Port used for the chip select
uint16_t SDSPIMSP432_HWAttrs::pinCS |
GPIO Pin used for the chip select