IPC API  3.30.01.12
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Data Fields
RcmServer_ThreadPoolDesc Struct Reference

Worker pool descriptor. More...

#include <RcmServer.h>

Collaboration diagram for RcmServer_ThreadPoolDesc:
Collaboration graph

Data Fields

String name
 The name of the worker pool. More...
 
UInt count
 The number of worker threads in the pool. More...
 
Thread_Priority priority
 The priority of all threads in the worker pool. More...
 
Int osPriority
 The priority (OS-specific) of all threads in the worker pool. More...
 
SizeT stackSize
 The stack size in bytes of a worker thread. More...
 
String stackSeg
 The worker thread stack placement. More...
 

Detailed Description

Worker pool descriptor.

Use this data structure to define a worker pool to be created either at the server create time or dynamically at runtime.

Field Documentation

String RcmServer_ThreadPoolDesc::name

The name of the worker pool.

UInt RcmServer_ThreadPoolDesc::count

The number of worker threads in the pool.

Thread_Priority RcmServer_ThreadPoolDesc::priority

The priority of all threads in the worker pool.

This value is Operating System independent. It determines the execution priority of all the worker threads in the pool.

Int RcmServer_ThreadPoolDesc::osPriority

The priority (OS-specific) of all threads in the worker pool.

This value is Operating System specific. It determines the execution priority of all the worker threads in the pool. If this property is set, it takes precedence over the priority property above.

SizeT RcmServer_ThreadPoolDesc::stackSize

The stack size in bytes of a worker thread.

String RcmServer_ThreadPoolDesc::stackSeg

The worker thread stack placement.


The documentation for this struct was generated from the following file:
Copyright 2014, Texas Instruments Incorporated