IPC API  3.30.01.12
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Data Fields
RcmClient_Message Struct Reference

Remote Command Message structure. More...

#include <RcmClient.h>

Collaboration diagram for RcmClient_Message:
Collaboration graph

Data Fields

UInt16 poolId
 The worker pool id that will process this message. More...
 
UInt16 jobId
 The job id associated with this message. More...
 
UInt32 fxnIdx
 The index of the remote function to execute. More...
 
Int32 result
 The return value of the remote message function. More...
 
UInt32 dataSize
 The size of the data buffer (in chars). More...
 
UInt32 data [1]
 The data buffer containing the message payload. More...
 

Detailed Description

Remote Command Message structure.

An RcmClient needs to fill in this message before sending it to the RcmServer for execution.

Field Documentation

UInt16 RcmClient_Message::poolId

The worker pool id that will process this message.

The message will be processed by a worker thread from the worker pool specified in this field. The default value is the default pool id.

UInt16 RcmClient_Message::jobId

The job id associated with this message.

All messages beloging to a job id must have this field set to that id. Use the value RcmClient_DISCRETEJOBID if the message does not belong to any job.

UInt32 RcmClient_Message::fxnIdx

The index of the remote function to execute.

Int32 RcmClient_Message::result

The return value of the remote message function.

UInt32 RcmClient_Message::dataSize

The size of the data buffer (in chars).

This field should be considered as read-only. It is set by the call to the RcmClient_alloc() function.

UInt32 RcmClient_Message::data[1]

The data buffer containing the message payload.

The size of this field is dataSize chars. The space is allocated by the call to the RcmClient_alloc() function.


The documentation for this struct was generated from the following file:
Copyright 2014, Texas Instruments Incorporated