#include <rf_common_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x0816. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips if the rule involves skipping. More... | |
} | condition |
uint8_t | vddrLevel |
VDDR level to set 0xFD: Trim VDDR voltage to normal level (VDDR_TRIM), nominally 1.68 V 0xFE: Trim VDDR voltage to high level (VDDR_TRIM_H), nominally 1.85 V 0xFF: Trim VDDR voltage to higher level (VDDR_TRIM_HH), nominally 1.95 V Other: reserved. More... | |
uint8_t | paTrimValue |
Optional power amplifier trim setting manipulation 0x00-0x1F: Value to write in ADI_0_RF:PACTL0.TRIM register field 0xFE: Set PACTL0.TRIM to its default value from FCFG1 0xFF: Do not write PACTL0.TRIM, use the setting that is already applied More... | |
Definition at line 738 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_POWER_BOOST_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 747 of file rf_common_cmd.h.
uint16_t rfc_CMD_TX_POWER_BOOST_s::commandNo |
The command ID number 0x0816.
Definition at line 739 of file rf_common_cmd.h.
struct { ... } rfc_CMD_TX_POWER_BOOST_s::condition |
uint8_t rfc_CMD_TX_POWER_BOOST_s::nSkip |
Number of skips if the rule involves skipping.
Definition at line 755 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_POWER_BOOST_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 750 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_POWER_BOOST_s::paTrimValue |
Optional power amplifier trim setting manipulation
0x00-0x1F: Value to write in ADI_0_RF:PACTL0.TRIM register field
0xFE: Set PACTL0.TRIM to its default value from FCFG1
0xFF: Do not write PACTL0.TRIM, use the setting that is already applied
Definition at line 762 of file rf_common_cmd.h.
rfc_radioOp_t* rfc_CMD_TX_POWER_BOOST_s::pNextOp |
Pointer to the next operation to run after this operation is done.
Definition at line 743 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_POWER_BOOST_s::rule |
Condition for running next command: Rule for how to proceed.
Definition at line 754 of file rf_common_cmd.h.
ratmr_t rfc_CMD_TX_POWER_BOOST_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
Definition at line 744 of file rf_common_cmd.h.
struct { ... } rfc_CMD_TX_POWER_BOOST_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_CMD_TX_POWER_BOOST_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
Definition at line 740 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_POWER_BOOST_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 749 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_POWER_BOOST_s::triggerType |
The type of trigger.
Definition at line 746 of file rf_common_cmd.h.
uint8_t rfc_CMD_TX_POWER_BOOST_s::vddrLevel |
VDDR level to set
0xFD: Trim VDDR voltage to normal level (VDDR_TRIM), nominally 1.68 V
0xFE: Trim VDDR voltage to high level (VDDR_TRIM_H), nominally 1.85 V
0xFF: Trim VDDR voltage to higher level (VDDR_TRIM_HH), nominally 1.95 V
Other: reserved.
Definition at line 757 of file rf_common_cmd.h.