#include <rf_prop_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x3802. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips if the rule involves skipping. More... | |
} | condition |
struct { | |
uint8_t bFsOff:1 | |
0: Keep frequency synth on after command 1: Turn frequency synth off after command More... | |
uint8_t bRepeatOk:1 | |
0: End operation after receiving a packet correctly 1: Go back to sync search after receiving a packet correctly More... | |
uint8_t bRepeatNok:1 | |
0: End operation after receiving a packet with CRC error 1: Go back to sync search after receiving a packet with CRC error More... | |
uint8_t bUseCrc:1 | |
0: Do not check CRC 1: Check CRC More... | |
uint8_t bVarLen:1 | |
0: Fixed length 1: Receive length as first byte More... | |
uint8_t bChkAddress:1 | |
0: No address check 1: Check address More... | |
uint8_t endType:1 | |
0: Packet is received to the end if end trigger happens after sync is obtained 1: Packet reception is stopped if end trigger happens More... | |
uint8_t filterOp:1 | |
0: Stop receiver and restart sync search on address mismatch 1: Receive packet and mark it as ignored on address mismatch More... | |
} | pktConf |
struct { | |
uint8_t bAutoFlushIgnored:1 | |
If 1, automatically discard ignored packets from Rx queue. More... | |
uint8_t bAutoFlushCrcErr:1 | |
If 1, automatically discard packets with CRC error from Rx queue. More... | |
uint8_t __pad0__:1 | |
uint8_t bIncludeHdr:1 | |
If 1, include the received header or length byte in the stored packet; otherwise discard it. More... | |
uint8_t bIncludeCrc:1 | |
If 1, include the received CRC field in the stored packet; otherwise discard it. More... | |
uint8_t bAppendRssi:1 | |
If 1, append an RSSI byte to the packet in the Rx queue. More... | |
uint8_t bAppendTimestamp:1 | |
If 1, append a timestamp to the packet in the Rx queue. More... | |
uint8_t bAppendStatus:1 | |
If 1, append a status byte to the packet in the Rx queue. More... | |
} | rxConf |
Rx configuration. More... | |
uint32_t | syncWord |
Sync word to listen for. More... | |
uint8_t | maxPktLen |
Packet length for fixed length, maximum packet length for variable length 0: Unlimited or unknown length. More... | |
uint8_t | address0 |
Address. More... | |
uint8_t | address1 |
Address (set equal to address0 to accept only one address. If 0xFF, accept 0x00 as well) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | endTrigger |
Trigger classifier for ending the operation. More... | |
ratmr_t | endTime |
Time used together with endTrigger for ending the operation. More... | |
dataQueue_t * | pQueue |
Pointer to receive queue. More... | |
uint8_t * | pOutput |
Pointer to output structure. More... | |
Definition at line 154 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::__pad0__ |
Definition at line 194 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::address0 |
Address.
Definition at line 204 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::address1 |
Address (set equal to address0
to accept only one address. If 0xFF, accept 0x00 as well)
Definition at line 205 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::bAppendRssi |
If 1, append an RSSI byte to the packet in the Rx queue.
Definition at line 197 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::bAppendStatus |
If 1, append a status byte to the packet in the Rx queue.
Definition at line 199 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::bAppendTimestamp |
If 1, append a timestamp to the packet in the Rx queue.
Definition at line 198 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::bAutoFlushCrcErr |
If 1, automatically discard packets with CRC error from Rx queue.
Definition at line 193 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::bAutoFlushIgnored |
If 1, automatically discard ignored packets from Rx queue.
Definition at line 192 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::bChkAddress |
0: No address check
1: Check address
Definition at line 184 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 163 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::bFsOff |
0: Keep frequency synth on after command
1: Turn frequency synth off after command
Definition at line 174 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::bIncludeCrc |
If 1, include the received CRC field in the stored packet; otherwise discard it.
Definition at line 196 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::bIncludeHdr |
If 1, include the received header or length byte in the stored packet; otherwise discard it.
Definition at line 195 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::bRepeatNok |
0: End operation after receiving a packet with CRC error
1: Go back to sync search after receiving a packet with CRC error
Definition at line 178 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::bRepeatOk |
0: End operation after receiving a packet correctly
1: Go back to sync search after receiving a packet correctly
Definition at line 176 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::bUseCrc |
0: Do not check CRC
1: Check CRC
Definition at line 180 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::bVarLen |
0: Fixed length
1: Receive length as first byte
Definition at line 182 of file rf_prop_cmd.h.
uint16_t rfc_CMD_PROP_RX_s::commandNo |
The command ID number 0x3802.
Definition at line 155 of file rf_prop_cmd.h.
struct { ... } rfc_CMD_PROP_RX_s::condition |
ratmr_t rfc_CMD_PROP_RX_s::endTime |
Time used together with endTrigger
for ending the operation.
Definition at line 215 of file rf_prop_cmd.h.
struct { ... } rfc_CMD_PROP_RX_s::endTrigger |
Trigger classifier for ending the operation.
uint8_t rfc_CMD_PROP_RX_s::endType |
0: Packet is received to the end if end trigger happens after sync is obtained
1: Packet reception is stopped if end trigger happens
Definition at line 186 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::filterOp |
0: Stop receiver and restart sync search on address mismatch
1: Receive packet and mark it as ignored on address mismatch
Definition at line 188 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::maxPktLen |
Packet length for fixed length, maximum packet length for variable length
0: Unlimited or unknown length.
Definition at line 202 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::nSkip |
Number of skips if the rule involves skipping.
Definition at line 171 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 166 of file rf_prop_cmd.h.
struct { ... } rfc_CMD_PROP_RX_s::pktConf |
rfc_radioOp_t* rfc_CMD_PROP_RX_s::pNextOp |
Pointer to the next operation to run after this operation is done.
Definition at line 159 of file rf_prop_cmd.h.
uint8_t* rfc_CMD_PROP_RX_s::pOutput |
Pointer to output structure.
Definition at line 217 of file rf_prop_cmd.h.
dataQueue_t* rfc_CMD_PROP_RX_s::pQueue |
Pointer to receive queue.
Definition at line 216 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::rule |
Condition for running next command: Rule for how to proceed.
Definition at line 170 of file rf_prop_cmd.h.
struct { ... } rfc_CMD_PROP_RX_s::rxConf |
Rx configuration.
ratmr_t rfc_CMD_PROP_RX_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
Definition at line 160 of file rf_prop_cmd.h.
struct { ... } rfc_CMD_PROP_RX_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_CMD_PROP_RX_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
Definition at line 156 of file rf_prop_cmd.h.
uint32_t rfc_CMD_PROP_RX_s::syncWord |
Sync word to listen for.
Definition at line 201 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 165 of file rf_prop_cmd.h.
uint8_t rfc_CMD_PROP_RX_s::triggerType |
The type of trigger.
Definition at line 162 of file rf_prop_cmd.h.